2009-08-06 07:44:05     How can I attach both spi mmc and another spi adc in 08r1.5?

2009-08-06 07:44:05     How can I attach both spi mmc and another spi adc in 08r1.5?

Wei Jiang (CHINA)

Message: 78420   

Dear all,

     My hardware is bf561, kernel is 08r1.5

     As SPI support is dropped while spi_mmc enabled, how can I  control the ADC via SPI interface?

     Can I write Blackfin SPI bus directly at the same time?

    Thanks .

    Wei Jiang

QuoteReplyEditDelete

2009-08-06 22:12:10     Re: How can I attach both spi mmc and another spi adc in 08r1.5?

Yi Li (CHINA)

Message: 78433   

Is it possible that you move to 2009R1? The original spi_mmc driver has been replaced by mainline mmc_spi driver. And you can use the "spi_lock_bus()" functions if mmc_spi cannot share spi bus with you ADC properly.

If you insist on using 2008R1.5, you may set spi_mmc driver to use spi frame work (do not use spi bus directly).

-Yi

QuoteReplyEditDelete

2009-08-06 22:37:45     Re: How can I attach both spi mmc and another spi adc in 08r1.5?

Wei Jiang (CHINA)

Message: 78434   

Dear Li,

         Thanks for your kindly reply.

         I can move to 2009R1. How can I get the toolchains for 09R1? And can you tell me when the 09R1 will be formally released?

             Wei Jiang

QuoteReplyEditDelete

2009-08-07 02:26:10     Re: How can I attach both spi mmc and another spi adc in 08r1.5?

Yi Li (CHINA)

Message: 78476   

Please download and use 2009R1-RC10 toolchain:   blackfin.uclinux.org/gf/project/toolchain/frs/?action=FrsReleaseBrowse&frs_package_id=74

2009R1 will be release in one or two week. You can use 2009r1 release candidates. There are just bug fix - no major changes.

-Yi

QuoteReplyEditDelete

2009-08-07 04:14:36     Re: How can I attach both spi mmc and another spi adc in 08r1.5?

Wei Jiang (CHINA)

Message: 78482   

Li,

    Ok, I\'ll try. Thanks a lot for your help.

      Wei Jiang

  • Created
Was this helpful?

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.