2009-07-22 07:30:01     HDD Mount

2009-07-22 07:30:01     HDD Mount

sree karan (INDIA)

Message: 77862   

Hi,

##############################################################################

ide: Assuming 50MHz system bus speed for PIO modes; override with idebus=xx

ide0: Blackfin generic IDE interface

Probing IDE interface ide0...

hda: probing with STATUS(0x50) instead of ALTSTATUS(0xaa)

hda: HTS541040G9AT00, ATA DISK drive

hdb: probing with STATUS(0x50) instead of ALTSTATUS(0xaa)

hdb: probing with STATUS(0x51) instead of ALTSTATUS(0xaa)

ide0 at 0x20100000-0x20100007,0x20118004 on irq 33

hda: max request size: 512KiB

hda: Host Protected Area detected.

        current capacity is 78140160 sectors (40007 MB)

        default  capacity is 185074430006016 sectors (94758108163 MB)

hda: task_no_data_intr: status=0x51 { DriveReady SeekComplete Error }

hda: task_no_data_intr: error=0x04 { DriveStatusError }

ide: failed opcode was: 0x37

hda: 78140160 sectors (40007 MB) w/7539KiB Cache, CHS=16383/255/63

hda: cache flushes supported

hda: hda1 hda2

##############################################################################

I am trying to enable HDD driver in uClinux-dist-2008R1.5-RC3 kernel for the BF533 custom hardware.

Though I can mount, read from and write to the hard disk, I get some errors (highlighted in the above log).

What should be done to overcome those errors?

Kindly help.

Thanks in advance

Regards,

Karan

QuoteReplyEditDelete

2010-04-17 23:07:32     Re: HDD Mount

steven O (AFGHANISTAN)

Message: 88549   

Hi ,

    I have the same problem . had you solved it ? and how to solve it ?

QuoteReplyEditDelete

2010-04-21 11:44:39     Re: HDD Mount

Robin Getz (UNITED STATES)

Message: 88727   

Steven:

Start a new thread.

-robin

  • Created
Was this helpful?

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.