2009-07-20 15:41:26     When I add gdbserver to my configuration make fails - Please Help

2009-07-20 15:41:26     When I add gdbserver to my configuration make fails - Please Help

Marshall Seaborn (UNITED STATES)

Message: 77763   

I'm trying to use gdbserver to debug a userland application.  When I add the "Miscellaneous

Application 'gdbserver' and run make I get the following error,

make[3]: Entering directory `/home/seaborn/Projects/blackfin-uClinux/uClinux-dist-2008R1.5-RC3/user/gdb'                                          

rm -rf build                                                                                                                                      

mkdir build                                                                                                                                       

(cd build; sh ../gdb/gdbserver/configure --build=i686-pc-linux-gnu --host=bfin-linux-uclibc --build=i686-pc-linux-gnu --prefix=/usr --sysconfdir=/etc --datadir=/usr/share --mandir=/usr/share/man --infodir=/usr/share/info --localstatedir=/var/lib --with-readline --disable-nls)                  

creating cache ./config.cache                                                                                                                     

checking for gcc... bfin-linux-uclibc-gcc                                                                                                         

checking whether the C compiler (bfin-linux-uclibc-gcc -pipe -Wall -g3 -O0      -mcpu=bf548-0.1         -mcpu=bf548-0.1) works... yes             

checking whether the C compiler (bfin-linux-uclibc-gcc -pipe -Wall -g3 -O0      -mcpu=bf548-0.1         -mcpu=bf548-0.1) is a cross-compiler... yes

checking whether we are using GNU C... yes

checking whether bfin-linux-uclibc-gcc accepts -g... yes

checking host system type... bfin-unknown-linux-uclibc

checking target system type... bfin-unknown-linux-uclibc

checking build system type... i686-pc-linux-gnu

checking for a BSD compatible install... /usr/bin/install -c

checking how to run the C preprocessor... bfin-linux-uclibc-gcc -E

checking for ANSI C header files... yes

checking for sgtty.h... yes

checking for termio.h... yes

checking for termios.h... yes

checking for sys/reg.h... yes

checking for string.h... yes

checking for proc_service.h... no

checking for sys/procfs.h... yes

checking for thread_db.h... yes

checking for linux/elf.h... yes

checking for stdlib.h... yes

checking for unistd.h... yes

checking whether strerror must be declared... no

Error: target not supported by gdbserver.

make[3]: *** [build/build] Error 1

make[3]: Leaving directory `/home/seaborn/Projects/blackfin-uClinux/uClinux-dist-2008R1.5-RC3/user/gdb'

make[2]: *** [gdb] Error 2

make[2]: Leaving directory `/home/seaborn/Projects/blackfin-uClinux/uClinux-dist-2008R1.5-RC3/user'

make[1]: *** [all] Error 2

make[1]: Leaving directory `/home/seaborn/Projects/blackfin-uClinux/uClinux-dist-2008R1.5-RC3/user'

make: *** [subdirs] Error 1

make[3]: Entering directory `/home/seaborn/Projects/blackfin-uClinux/uClinux-dist-2008R1.5-RC3/user/gdb'                                          

rm -rf build                                                                                                                                      

mkdir build                                                                                                                                       

(cd build; sh ../gdb/gdbserver/configure --build=i686-pc-linux-gnu --host=bfin-linux-uclibc --build=i686-pc-linux-gnu --prefix=/usr --sysconfdir=/etc --datadir=/usr/share --mandir=/usr/share/man --infodir=/usr/share/info --localstatedir=/var/lib --with-readline --disable-nls)                  

creating cache ./config.cache                                                                                                                     

checking for gcc... bfin-linux-uclibc-gcc                                                                                                         

checking whether the C compiler (bfin-linux-uclibc-gcc -pipe -Wall -g3 -O0      -mcpu=bf548-0.1         -mcpu=bf548-0.1) works... yes             

checking whether the C compiler (bfin-linux-uclibc-gcc -pipe -Wall -g3 -O0      -mcpu=bf548-0.1         -mcpu=bf548-0.1) is a cross-compiler... yes

checking whether we are using GNU C... yes

checking whether bfin-linux-uclibc-gcc accepts -g... yes

checking host system type... bfin-unknown-linux-uclibc

checking target system type... bfin-unknown-linux-uclibc

checking build system type... i686-pc-linux-gnu

checking for a BSD compatible install... /usr/bin/install -c

checking how to run the C preprocessor... bfin-linux-uclibc-gcc -E

checking for ANSI C header files... yes

checking for sgtty.h... yes

checking for termio.h... yes

checking for termios.h... yes

checking for sys/reg.h... yes

checking for string.h... yes

checking for proc_service.h... no

checking for sys/procfs.h... yes

checking for thread_db.h... yes

checking for linux/elf.h... yes

checking for stdlib.h... yes

checking for unistd.h... yes

checking whether strerror must be declared... no

Error: target not supported by gdbserver.

make[3]: *** [build/build] Error 1

make[3]: Leaving directory `/home/seaborn/Projects/blackfin-uClinux/uClinux-dist-2008R1.5-RC3/user/gdb'

make[2]: *** [gdb] Error 2

make[2]: Leaving directory `/home/seaborn/Projects/blackfin-uClinux/uClinux-dist-2008R1.5-RC3/user'

make[1]: *** [all] Error 2

make[1]: Leaving directory `/home/seaborn/Projects/blackfin-uClinux/uClinux-dist-2008R1.5-RC3/user'

make: *** [subdirs] Error 1

My target is a BF548-EZKIT derivative.  What does this error mean.  If I use gdbserver(old) the make

succeeds.

Also,

The kernel configuration option

for the "Miscellaneous Application" says I must ENABLE PTHREADS_DEBUG_SUPPORT in uClibc config.

How/Where do I enable this option?

Thanks,

Marshall Seaborn

QuoteReplyEditDelete

2009-07-20 15:43:24     Re: When I add gdbserver to my configuration make fails - Please Help

Mike Frysinger (UNITED STATES)

Message: 77764   

you picked the wrong one.  enable the one that's enabled in the default config -- the one labeled "old".

QuoteReplyEditDelete

2009-07-20 16:11:36     Re: When I add gdbserver to my configuration make fails - Please Help

Marshall Seaborn (UNITED STATES)

Message: 77765   

Mike,

thanks for the fast response.

Marshall

  • Created
Was this helpful?

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.