2009-06-01 03:10:42     Building USB Mass storage in BF527(silicon 0.1) failure?

2009-06-01 03:10:42     Building USB Mass storage in BF527(silicon 0.1) failure?

浩 何 (CHINA)

Message: 74892   

Hi,

my trunk is uClinux-dist-2008R1.5-RC3,and by board is BF527(Version 0.1), after according to the following config:

USB driver:

  x x

  x x                 <*> Support for Host-side USB                                                           x x

  x x                 [ ]   USB verbose debug messages                                                        x x

  x x                 ---   Miscellaneous USB options                                                         x x

  x x                 [*]   USB device filesystem                                                             x x

  x x                 [*]   USB device class-devices (DEPRECATED)                                             x x

  x x                 [ ]   Dynamic USB minor allocation (EXPERIMENTAL)                                       x x

  x x                 [ ]   USB selective suspend/resume and wakeup (EXPERIMENTAL)                            x x

  x x                 [ ]   Rely on OTG Targeted Peripherals List                                             x x

  x x                 [ ]   Disable external hubs                                                             x x

  x x                 ---   USB Host Controller Drivers                                                       x x

  x x                 < >   ISP116X HCD support                                                               x x

  x x                 < >   ISP1362 HCD support                                                               x x

  x x                 < >   ISP1760 HCD support                                                               x x

  x x                 < >   SL811HS HCD support                                                               x x

  x x                 <*> Inventra Highspeed Dual Role Controller (TI, ADI, ...)                              x x

  x x                 ---   Blackfin BF54x, BF525 and BF527 high speed USB support                            x x

  x x                       Driver Mode (USB Host)  --->                                                      x x

  x x                 [*]   Disable DMA (always use PIO)                                                      x x

  x x                 [*]     Using DMA polling in MUSB PIO mode                                              x x

  x x                 (0)   Logging Level (0 - none / 3 - annoying / ... )                                    x x

  x x                 --- USB Device Class drivers                                                            x x

  x x                 < > USB Modem (CDC ACM) support                                                         x x

  x x                 < > USB Printer support                                                                 x x

  x x                 --- NOTE: USB_STORAGE enables SCSI, and 'SCSI disk support'                             x x

  x x                 --- may also be needed; see USB_STORAGE Help for more information                       x x

  x x                 <*> USB Mass Storage support                                                            x x

  x x                 [ ]   USB Mass Storage verbose debug

SCSI support:

  x x                 < > RAID Transport Class                                                                x x

  x x                 <*> SCSI device support                                                                 x x

  x x                 < >   SCSI target support                                                               x x

  x x                 [ ] legacy /proc/scsi/ support                                                          x x

  x x                 --- SCSI support type (disk, tape, CD-ROM)                                              x x

  x x                 <*> SCSI disk support                                                                   x x

  x x                 < > SCSI tape support                                                                   x x

  x x                 < > SCSI OnStream SC-x0 tape support                                                    x x

  x x                 < > SCSI CDROM support                                                                  x x

  x x                 < > SCSI generic support                                                                x x

  x x                 < > SCSI media changer support                                                          x x

  x x                 --- Some SCSI devices (e.g. CD jukebox) support multiple LUNs                           x x

  x x                 [*] Probe all LUNs on each SCSI device                                                  x x

  x x                 [ ] Verbose SCSI error reporting (kernel size +=12K)                                    x x

  x x                 [ ] SCSI logging facility                                                               x x

  x x                 [ ] Asynchronous SCSI scanning                                                          x x

  x x                     SCSI Transports  --->                                                               x x

  x x                     SCSI low-level drivers  --->  

AND add language and DOS/VFAT filesystems support.

after build the kernel:

I plug in the u-disk(sony 128M,and other u-disk 2G)

there is no message on the console:

dmesg:

Linux version 2.6.22.19-ADI-2008R1.5-svn2487 (hehao@svnhost.imagintech.cn) (gcc version 4.1.2 (ADI svn)) #1197 Mon Jun 1 14:58:50 CST 2009

early printk enabled on early_BFuart0

Hardware Trace Active and Enabled

Reset caused by Software reset

Blackfin support (C) 2004-2007 Analog Devices, Inc.

Compiled for ADSP-BF527 Rev any

Warning: Unsupported Chip Revision ADSP-BF527 Rev 0.1 detected

Blackfin Linux support by http://blackfin.uclinux.org/

Processor Speed: 600 MHz core clock and 120 MHz System Clock

Board Memory: 32MB

Kernel Managed Memory: 32MB

Memory map:

  text      = 0x00100000-0x00232290

  rodata    = 0x00233000-0x0028e724

  data      = 0x0028f000-0x002a4000

    stack   = 0x00290000-0x00292000

  init      = 0x002a4000-0x00556000

  bss       = 0x00556000-0x00569fe4

  available = 0x00569fe4-0x01dff000

  DMA Zone  = 0x01e00000-0x02000000

On node 0 totalpages: 7679

  DMA zone: 59 pages used for memmap

  DMA zone: 0 pages reserved

  DMA zone: 7620 pages, LIFO batch:0

  Normal zone: 0 pages used for memmap

NOMPU: setting up cplb tables for global access

Instruction Cache Enabled

Data Cache Enabled (write-through)

Built 1 zonelists.  Total pages: 7620

Kernel command line: root=/dev/mtdblock0 rw earlyprintk=serial,uart0,57600 console=ttyBF0,57600

Configuring Blackfin Priority Driven Interrupts

PID hash table entries: 128 (order: 7, 512 bytes)

bfin-rtc: invalid date; resetting

console handover: boot [early_BFuart0] -> real [ttyBF0]

Dentry cache hash table entries: 4096 (order: 2, 16384 bytes)

Inode-cache hash table entries: 2048 (order: 1, 8192 bytes)

Kernel managed physical pages: 7679

Memory available: 24876k/32768k RAM, (2760k init code, 1224k kernel code, 535k data, 2048k dma, 1324k reserved)

Blackfin Scratchpad data SRAM: 4 KB

Blackfin Data A SRAM: 16 KB (16 KB free)

Blackfin Data B SRAM: 32 KB (32 KB free)

Blackfin Instruction SRAM: 48 KB (43 KB free)

Calibrating delay loop... 1196.03 BogoMIPS (lpj=2392064)

Security Framework v1.0.0 initialized

Mount-cache hash table entries: 512

NET: Registered protocol family 16

Blackfin GPIO Controller

Blackfin DMA Controller

stamp_init(): registering device resources

Generic PHY: Registered new driver

SCSI subsystem initialized

usbcore: registered new interface driver usbfs

usbcore: registered new interface driver hub

usbcore: registered new device driver usb

musb_hdrc: version 6.0/dbg, pio, host, debug=3

musb_hdrc: ConfigData=0x00 (UTMI-8)

musb_hdrc: kernel must blacklist external hubs

ep_config_from_hw 1276: <== static silicon ep config

musb_hdrc: hw_ep 0shared, max 64

musb_hdrc: hw_ep 1tx, max 128

musb_hdrc: hw_ep 1rx, max 128

musb_hdrc: hw_ep 2tx, max 128

musb_hdrc: hw_ep 2rx, max 128

musb_hdrc: hw_ep 3tx, max 128

musb_hdrc: hw_ep 3rx, max 128

musb_hdrc: hw_ep 4tx, max 128

musb_hdrc: hw_ep 4rx, max 128

musb_hdrc: hw_ep 5tx, max 1024

musb_hdrc: hw_ep 5rx, max 1024

musb_hdrc: hw_ep 6tx, max 1024

musb_hdrc: hw_ep 6rx, max 1024

musb_hdrc: hw_ep 7tx, max 1024

musb_hdrc: hw_ep 7rx, max 1024

musb_hdrc: USB Host mode controller at ffc03800 using PIO, IRQ 59

musb_hdrc musb_hdrc.0: MUSB HDRC host driver

musb_hdrc musb_hdrc.0: new USB bus registered, assigned bus number 1

usb usb1: configuration #1 chosen from 1 choice

hub 1-0:1.0: USB hub found

hub 1-0:1.0: 1 port detected

musb_start 874: <== devctl 80

musb_init_controller 2099: HOST mode, status 0, devctl 81 B

Registered /proc/driver/musb_hdrc

NET: Registered protocol family 2

IP route cache hash table entries: 1024 (order: 0, 4096 bytes)

TCP established hash table entries: 1024 (order: 1, 8192 bytes)

TCP bind hash table entries: 1024 (order: 0, 4096 bytes)

TCP: Hash tables configured (established 1024 bind 1024)

TCP reno registered

JFFS2 version 2.2. (NAND) 漏 2001-2006 Red Hat, Inc.

io scheduler noop registered

io scheduler anticipatory registered (default)

io scheduler cfq registered

simple-gpio: now handling 48 GPIOs: 0 - 47

bfin-wdt: initialized: timeout=20 sec (nowayout=0)

Serial: Blackfin serial driver

bfin-uart.1: ttyBF0 at MMIO 0xffc00400 (irq = 29) is a BFIN-UART

RAMDISK driver initialized: 16 RAM disks of 4096K size 1024 blocksize

bf537mac_probe: MAC = 0-12-22-33-12-1a

bfin_mac_mdio: probed

bfin_mac: attached PHY driver [Generic PHY] (mii_bus:phy_addr=0:03, irq=-1, mdc_clk=2500000Hz(mdc_div=23)@sclk=120MHz)

bfin_mac: Version 1.1, Blackfin BF53[67] BF527 on-chip Ethernet MAC driver

bfin-spi bfin-spi.0: Blackfin BF5xx on-chip SPI Contoller Driver, Version 1.0, regs_base@ffc00500, dma channel@7

Initializing USB Mass Storage driver...

usbcore: registered new interface driver usb-storage

USB Mass Storage support registered.

rtc-bfin rtc-bfin: rtc core: registered rtc-bfin as rtc0

TCP cubic registered

NET: Registered protocol family 1

NET: Registered protocol family 17

Setting up Blackfin MMR debugfs

rtc-bfin rtc-bfin: setting the system clock to 2059-01-01 07:21:07 (2808631267)

Freeing unused kernel memory: 2760k freed

dma_alloc_init: dma_page @ 0x01ade000 - 512 pages at 0x01e00000

PHY: 0:03 - Link is Up - 100/Full

root:/>

root:/>

question:

1.Does the BF527 0.1 and the uClinux-dist-2008R1.5-RC3 can support USB Host mass storage ??

2.if can, how can i config the kernel ???

TranslateQuoteReplyEditDelete

2009-06-01 03:13:55     Re: Building USB Mass storage in BF527(silicon 0.1) failure?

Mike Frysinger (UNITED STATES)

Message: 74893   

if you want to use USB on the BF52x, you have to use the 2009R1+ branches in svn.  or wait for the next release.  2008R1.5 wont work.

QuoteReplyEditDelete

2009-06-01 03:31:37     Re: Building USB Mass storage in BF527(silicon 0.1) failure?

浩 何 (CHINA)

Message: 74894   

thank you for you reponse!

but when will the next release version come out?

and we have decide use the release version !!!

i will have a try the svn !

thanks!!!

TranslateQuoteReplyEditDelete

2009-06-03 03:28:43     Re: Building USB Mass storage in BF527(silicon 0.1) failure?

浩 何 (CHINA)

Message: 75049   

hi

I svn the latest trunk (2.6.28.10-ADI-2010R1-pre-svn6523)

according the docs.blackfin.uclinux.org,i make kernel successfully, but when i insert the u-dist,

there is no message printked all the same,

please tell me is the software config  correct:

this is the dmesg:

BusyBox v1.14.1 (2009-06-02 17:33:20 CST) hush - the humble shell

root:/>

root:/> dmesg

Linux version 2.6.28.10-ADI-2010R1-pre-svn6523 (hehao@svnhost.imagintech.cn) (gcc version 4.1.2 (ADI svn)) #65 Wed Jun 3 15:26:11 CST 2009

console [early_BFuart0] enabled

early printk enabled on early_BFuart0

Board Memory: 32MB

Kernel Managed Memory: 32MB

Memory map:

  fixedcode = 0x00000400-0x00000490

  text      = 0x00001000-0x001233d0

  rodata    = 0x001233d0-0x001833e8

  bss       = 0x00184000-0x00194e44

  data      = 0x00194e44-0x001a8000

    stack   = 0x001a6000-0x001a8000

  init      = 0x001a8000-0x003b5000

  available = 0x003b5000-0x01eff000

  DMA Zone  = 0x01f00000-0x02000000

Hardware Trace Active and Enabled

Boot Mode: 1

Blackfin support (C) 2004-2009 Analog Devices, Inc.

Compiled for ADSP-BF527 Rev any

Blackfin Linux support by http://blackfin.uclinux.org/

Processor Speed: 500 MHz core clock and 100 MHz System Clock

boot memmap: 00000000003b5000 - 0000000001eff000 (usable)

On node 0 totalpages: 7935

free_area_init_node: node 0, pgdat 001a4948, node_mem_map 003b7000

  DMA zone: 62 pages used for memmap

  DMA zone: 0 pages reserved

  DMA zone: 7873 pages, LIFO batch:0

  Normal zone: 0 pages used for memmap

  Movable zone: 0 pages used for memmap

NOMPU: setting up cplb tables

Instruction Cache Enabled for CPU0

Data Cache Enabled for CPU0 (write-back)

Built 1 zonelists in Zone order, mobility grouping off.  Total pages: 7873

Kernel command line: root=/dev/mtdblock0 rw earlyprintk=serial,uart0,57600 console=ttyBF0,57600

Configuring Blackfin Priority Driven Interrupts

PID hash table entries: 128 (order: 7, 512 bytes)

console handover: boot [early_BFuart0] -> real [ttyBF0]

Dentry cache hash table entries: 4096 (order: 2, 16384 bytes)

Inode-cache hash table entries: 2048 (order: 1, 8192 bytes)

Kernel managed physical pages: 7935

Memory available: 27656k/32768k RAM, (2100k init code, 1160k kernel code, 532k data, 1024k dma, 292k reserved)

Calibrating delay loop... 997.37 BogoMIPS (lpj=1994752)

Security Framework initialized

Mount-cache hash table entries: 512

Blackfin Scratchpad data SRAM: 4 KB

Blackfin L1 Data A SRAM: 16 KB (15 KB free)

Blackfin L1 Data B SRAM: 16 KB (16 KB free)

Blackfin L1 Instruction SRAM: 48 KB (42 KB free)

net_namespace: 288 bytes

NET: Registered protocol family 16

Blackfin DMA Controller

ezkit_init(): registering device resources

SCSI subsystem initialized

usbcore: registered new interface driver usbfs

usbcore: registered new interface driver hub

usbcore: registered new device driver usb

musb_hdrc: version 6.0, pio, host, debug=0

musb_hdrc: ConfigData=0x00 (UTMI-8)

musb_hdrc: kernel must blacklist external hubs

musb_hdrc: HDRC RTL version 0.0

musb_hdrc: hw_ep 0shared, max 64

musb_hdrc: hw_ep 1tx, max 128

musb_hdrc: hw_ep 1rx, max 128

musb_hdrc: hw_ep 2tx, max 128

musb_hdrc: hw_ep 2rx, max 128

musb_hdrc: hw_ep 3tx, max 128

musb_hdrc: hw_ep 3rx, max 128

musb_hdrc: hw_ep 4tx, max 128

musb_hdrc: hw_ep 4rx, max 128

musb_hdrc: hw_ep 5tx, max 1024

musb_hdrc: hw_ep 5rx, max 1024

musb_hdrc: hw_ep 6tx, max 1024

musb_hdrc: hw_ep 6rx, max 1024

musb_hdrc: hw_ep 7tx, max 1024

musb_hdrc: hw_ep 7rx, max 1024

musb_hdrc: USB Host mode controller at ffc03800 using PIO, IRQ 59

musb_hdrc musb_hdrc.0: MUSB HDRC host driver

musb_hdrc musb_hdrc.0: new USB bus registered, assigned bus number 1

usb usb1: configuration #1 chosen from 1 choice

hub 1-0:1.0: USB hub found

hub 1-0:1.0: 1 port detected

NET: Registered protocol family 2

IP route cache hash table entries: 1024 (order: 0, 4096 bytes)

TCP established hash table entries: 1024 (order: 1, 8192 bytes)

TCP bind hash table entries: 1024 (order: 0, 4096 bytes)

TCP: Hash tables configured (established 1024 bind 1024)

TCP reno registered

NET: Registered protocol family 1

Setting up Blackfin MMR debugfs

msgmni has been set to 54

io scheduler noop registered

io scheduler anticipatory registered (default)

io scheduler cfq registered

bfin-otp: initialized

Serial: Blackfin serial driver

bfin-uart.1: ttyBF0 at MMIO 0xffc00400 (irq = 29) is a BFIN-UART

brd: module loaded

bfin_mii_bus: probed

bfin_mac: attached PHY driver [Generic PHY] (mii_bus:phy_addr=0:03, irq=-1, mdc_clk=2500000Hz(mdc_div=19)@sclk=100MHz)

bfin_mac bfin_mac.0: Blackfin on-chip Ethernet MAC driver, Version 1.1

Driver 'sd' needs updating - please use bus_type methods

Initializing USB Mass Storage driver...

usbcore: registered new interface driver usb-storage

USB Mass Storage support registered.

TCP cubic registered

NET: Registered protocol family 17

Freeing unused kernel memory: 2100k freed

dma_alloc_init: dma_page @ 0x018ae000 - 256 pages at 0x01f00000

root:/>

this problem has puzzled me 3 days,please help me

thank you!!!!

TranslateQuoteReplyEditDelete

2009-06-03 03:52:02     Re: Building USB Mass storage in BF527(silicon 0.1) failure?

Mike Frysinger (UNITED STATES)

Message: 75051   

did you use the right usb connector ?  most people pick the wrong one out of the little bag.

QuoteReplyEditDelete

2009-06-03 05:11:54     Re: Building USB Mass storage in BF527(silicon 0.1) failure?

浩 何 (CHINA)

Message: 75081   

thank you for you reply

I think i use the connector correct,

do you confirm my config is correct? and the silicon of 0.1 can support usb mass storage?

thanks!!!

TranslateQuoteReplyEditDelete

2009-06-03 08:41:41     Re: Building USB Mass storage in BF527(silicon 0.1) failure?

浩 何 (CHINA)

Message: 75128   

Thank you for you response!

According  the the BF527 manual,  If we don't use the usb OTG mode, and i just want to use usb Host mode to support the

mass storage, shoud I pull down or pull up the USB_ID PIN and USB_RSET PIN?

Should I pull down or pull up the USB_DM and USB_DP PIN?

In other words, how can i deal with the following pins?

USB_ID

USB_RSET

USB_DM

USB_DP

thanks!!!!

TranslateQuoteReplyEditDelete

2009-06-03 22:30:41     Re: Building USB Mass storage in BF527(silicon 0.1) failure?

浩 何 (CHINA)

Message: 75138   

There is no person answer my question?

Anyone who has complete the Usb host(Hardware) can help me?

thanks again!

TranslateQuoteReplyEditDelete

2009-06-04 03:32:48     Re: Building USB Mass storage in BF527(silicon 0.1) failure?

Sonic Zhang (CHINA)

Message: 75143   

What board do you use? If it is bf527-ezkit, you won't need to pull down and up any PIN.

QuoteReplyEditDelete

  • Created
Was this helpful?

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.