2009-05-27 09:56:36     Device node creation problem

2009-05-27 09:56:36     Device node creation problem

Hari Prasad (INDIA)

Message: 74650   

Hi,

When I plug my USB, sometimes device node gets created while sometimes its not created. Following is a log showing such a non-creation scenario:

root: /> usb 1-1: new high speed USB device using musb_hdrc and address 4

usb 1-1: configuration #1 chosen from 1 choice

scsi2 : SCSI emulation for USB Mass Storage devices

scsi 2:0:0:0: Direct-Access     Memorex  TD Classic 003B  PMAP PQ: 0 ANSI: 0 CCS

sd 2:0:0:0: [sda] 4016128 512-byte hardware sectors: (2.05 GB/1.91 GiB)

sd 2:0:0:0: [sda] Write Protect is off

sd 2:0:0:0: [sda] Assuming drive cache: write through

sd 2:0:0:0: [sda] 4016128 512-byte hardware sectors: (2.05 GB/1.91 GiB)

sd 2:0:0:0: [sda] Write Protect is off

sd 2:0:0:0: [sda] Assuming drive cache: write through

sda:<7>usb-storage: queuecommand called

sda1

sd 2:0:0:0: [sda] Attached SCSI removable disk

root: />

root: /> ls /dev/

bfin-otp            ram6                tty27               tty51

console             ram7                tty28               tty52

cpu_dma_latency     ram8                tty29               tty53

fb0                 ram9                tty3                tty54

full                random              tty30               tty55

kmsg                rtc0                tty31               tty56

log                 tty                 tty32               tty57

mem                 tty0                tty33               tty58

mtdblock0           tty1                tty34               tty59

mtdblock1           tty10               tty35               tty6

network_latency     tty11               tty36               tty60

network_throughput  tty12               tty37               tty61

null                tty13               tty38               tty62

ptmx                tty14               tty39               tty63

pts                 tty15               tty4                tty7

ram0                tty16               tty40               tty8

ram1                tty17               tty41               tty9

ram10               tty18               tty42               ttyBF0

ram11               tty19               tty43               urandom

ram12               tty2                tty44               usbdev1.1

ram13               tty20               tty45               usbdev1.1_ep00

ram14               tty21               tty46               usbdev1.1_ep81

ram15               tty22               tty47               vcs

ram2                tty23               tty48               vcsa

ram3                tty24               tty49               watchdog

ram4                tty25               tty5                zero

ram5                tty26               tty50

While the USB connect output shows the entry  sda1, there is no such entry in /dev. What could be the problem?

QuoteReplyEditDelete

2009-05-27 14:30:32     Re: Device node creation problem

Mike Frysinger (UNITED STATES)

Message: 74658   

try running `mdev -s`

QuoteReplyEditDelete

  • Created
Was this helpful?

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.