2009-05-27 08:54:31     how to access i2c as a slave in BF537

2009-05-27 08:54:31     how to access i2c as a slave in BF537

Adam W (POLAND)

Message: 74646   

I want to communicate via i2c (it can be smbus), but BF537 must be a SLAVE device.

I looked at documentation, examples, sources of drivers, bo I cannot find anything usefull (all is

So questions:

1. how to open driver as a ic2 slave ? (slave device doesnt drive a SCK line)

2. how to setup my own i2c hardware address ? Master device doesnt need it, but in slave device it should be changable.

3. how to detect that master wants to read or write data to me ?

4. is it posiible to use smbus protocol ?

with best regards,

xadamus

QuoteReplyEditDelete

2009-05-27 14:06:09     Re: how to access i2c as a slave in BF537

Mike Frysinger (UNITED STATES)

Message: 74655   

there is no support for using the I2C as a slave.  you'll have to write your own device driver from scratch.

QuoteReplyEditDelete

2009-05-27 16:41:12     Re: how to access i2c as a slave in BF537

Adam W (POLAND)

Message: 74671   

eeh, my own device driver.. ? it doesnt sound easy..

so where can i find source of oryginal device driver for BF537 ?

> there is no support for using the I2C as a slave.  you'll have to write your own device driver from scratch.

---

QuoteReplyEditDelete

2009-05-27 17:05:18     Re: how to access i2c as a slave in BF537

Robin Getz (UNITED STATES)

Message: 74673   

Adam:

The source - is part of the linux kernel -- linux-2.6.x/drivers/i2c/busses/i2c-bfin-twi.c

-Robin

QuoteReplyEditDelete

2009-11-06 21:32:49     Re: how to access i2c as a slave in BF537

Adrien Cottenceau (CANADA)

Message: 82141   

Adam,

Did you find a way to use the BF537 as an i2c salve?

thanks.

Adrien.

QuoteReplyEditDelete

2009-11-06 21:42:34     Re: how to access i2c as a slave in BF537

Adrien Cottenceau (CANADA)

Message: 82142   

Adam,

Did you find a way to use the BF537 as an i2c salve?

Or is it possible to use it with the SMBUS mode? ( i.e. no SCK control)

thanks.

Adrien.

---

QuoteReplyEditDelete

2009-11-10 14:48:26     Re: how to access i2c as a slave in BF537

Oussema Harbi (TUNISIA)

Message: 82257   

Adam ,Adrian

Did you found any way to access the BF537 as an i2c slave ?

Am interrested if any of you started developping a new drive.

I don't have a bf537 available now ,so am ready to make the development if one of you accepts to test it for me.

I have exams this week ,but i ll try to make it next week if you re interrested.

Regards ,

Oussema.

QuoteReplyEditDelete

2009-11-11 21:58:09     Re: how to access i2c as a slave in BF537

Adrien Cottenceau (CANADA)

Message: 82279   

Oussema,

i didn't start developping a new driver.

But i have a bf537 board ready, so i can test your driver if you want.

Adrien.

QuoteReplyEditDelete

2010-01-15 07:14:57     Re: how to access i2c as a slave in BF537

Adrien Cottenceau (CANADA)

Message: 84652   

Any news?

  • Created
Was this helpful?

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.