2009-05-05 13:52:20     request to add libmodbus to trunk

2009-05-05 13:52:20 request to add libmodbus to trunk

Kyle Schlansker (UNITED STATES)

Message: 73682  

Is it possible to add the latest release (2.0.3) of libmodbus to trunk before the 2009R1 branch?  You can get the sources here:  launchpad.net/libmodbus/+download

Thanks.

QuoteReplyEditDelete

2009-05-05 15:53:58 Re: request to add libmodbus to trunk

Robin Getz (UNITED STATES)

Message: 73696  

Kyle:

I would say no problem - but this is the first one that I'm aware of that would include any GPL/LGPL v3 into something that runs on the target. (Unless Mike can correct me, and something else slipped in).

Do you need v2.0.3 or is libmodbus v1.2.5 (which is still under LGPL 2) OK?

-Robin

QuoteReplyEditDelete

2009-05-05 16:51:38 Re: request to add libmodbus to trunk

Mike Frysinger (UNITED STATES)

Message: 73704  

readline is GPL-3.  whether the library is GPL-2 or GPL-3 doesnt matter that much ... any library that isnt LGPL means any project linking against it needs to be GPL.  licensing problems are the end user's problem though ;).

ive added libmodbus-2.0.3 to the tree.

QuoteReplyEditDelete

2009-05-06 11:06:32 Re: request to add libmodbus to trunk

Kyle Schlansker (UNITED STATES)

Message: 73767 I don't think the licensing issues will be a problem, but just to check my understanding: I'm working under the assumption that if program X links against libmodbus then program X needs to be GPL. If that's not a good assumption then let me know

QuoteReplyEditDelete

2009-05-06 11:36:40 Re: request to add libmodbus to trunk

Robin Getz (UNITED STATES)

Message: 73773  

Kyle:

The best place to get legal/licensing advice from is not us.

https://docs.blackfin.uclinux.org/doku.php?id=copyright_information#software_license

Also check out the FSF faq:

  www.gnu.org/licenses/gpl-faq.html

specifically -

  www.gnu.org/licenses/gpl-faq.html#AllCompatibility

I just didn't think there were any other GPL v3 applications in the dist - Mike corrected me - so yeah, I don't have a problem with it (Mike added the latest yesterday) - it is up to you on how you combine things, and meet the requirements of each license.

-Robin

QuoteReplyEditDelete

2009-05-06 11:53:27 Re: request to add libmodbus to trunk

Kyle Schlansker (UNITED STATES)

Message: 73775  

Thanks for the links Robin, and thank you for adding it to the tree Mike.

  • Created
Was this helpful?

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.