2009-04-21 07:12:38     zeroconf

2009-04-21 07:12:38     zeroconf

Daniele Pagani (ITALY)

Message: 72938   

Dear sirs,

could somebody suggest me an application in order to run zeroconf protocol, or Bonjour or something similar in order to have the network autoconfiguration?

I've found the zcip under the BusyBox menu. Does exist something more?

This application needs to run on Blackfin BF537 and on Pc Windows machine (of course not the same application, but the same protocol).

Best regards,

Daniele.

TranslateQuoteReplyEditDelete

2009-04-21 07:33:42     Re: zeroconf

Robin Getz (UNITED STATES)

Message: 72972   

Daniele:

Have a look at avahi. It is already in the uClinux-dist. (./lib/avahi/)

-Robin

QuoteReplyEditDelete

2009-04-21 08:55:21     Re: zeroconf

Daniele Pagani (ITALY)

Message: 72988   

Dear Robin,

I'm using live distribution rev 7972.

I've find avahi in lib. If I compile, than I've:

libavahi-common.so.3 and libavahi-core.so.5 in /usr/lib directory, but I don't find any avahi application.

Do I write my application using this library? or is there a ready application?

Regards,

Daniele.

TranslateQuoteReplyEditDelete

2009-04-21 11:50:56     Re: zeroconf

Robin Getz (UNITED STATES)

Message: 73002   

Daniele:

Have a look at the docs:

  avahi.org/

Normally - people use their own - but I think there are likely some things in ./staging that aren't installed into the romfs.

  avahi.org/wiki/Avah4users#Documentation

-Robin

  • Created
Was this helpful?

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.