2009-04-01 22:15:45     need help with PPI

2009-04-01 22:15:45     need help with PPI

raghu mulagada (UNITED STATES)

Message: 71989   

Hello all

I am working to setup a parallel data tranmission using PPI on the blackfin

i am using blackfin 537, my kernel version is linux 2.6.21.19 and user-dist is release 2008R1.5

i modified the kernel to include ppi device as directed in the ppi wiki

i used the following piece of code to call the ppi device and use it :

fd = open("/dev/ppi0", O_RDWR);

        if (fd < 0) {

              printf("Could not open ppi device : %d \n",errno);

        exit(1);

    }

  

    else {

        printf("fd(%d) = open(/dev/ppi) \n", fd );

    }

i can see  the ppi in the dev folder of the blackfin when do an 'ls' in the serial port terminal

but when i try to run the appication 'ppitest', it gives me the following error:

could not open ppi device : 2

do any of you guys having experience with using PPI can help me resolve this problem?

thanks

-raghu

QuoteReplyEditDelete

2009-04-01 23:17:41     Re: need help with PPI

Mike Frysinger (UNITED STATES)

Message: 71990   

the output already shows you the problem

errno = 2 (ENOENT)

so /dev/ppi does not exist

make sure the device node is in /dev/ and if it isnt, make sure you enabled the driver properly

  • Created
Was this helpful?

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.