2009-03-22 20:03:03     tslib woes

2009-03-22 20:03:03     tslib woes

Gregory Hassett (UNITED STATES)

Message: 71353   

Hello,

I have been struggling for a few days now to get a version of uClinux to build for the blackfin that includes Qt.  In an ideal world, I would build Qt as shared libraries.

Currently I am battling tslib.  I am using the toolchain and the distribution directly from the subversion trunks (because Qt is not integrated into any released version of uClinux/Blackfin yet).

To get to a clean start state, I use "make menuconfig" to restore all defaults.  Then I check to make sure that I am building for the BF 533, and I do "make clean" followed by "make".

This builds the kernel successfully!

I then go back into "make menuconfig" and enable one additional option -- the "build tslib" option in the Library Configuration.  At this point, "make" fails while building ncurses (which I assume is included in the default settings).  I then go back into "make menuconfig" and de-select the ncurses library, leaving tslib selected.  Now, when I make, it fails during the build of tslib, with the errors attached at the end of this post.

Any suggestions or pointers would be HUGELY appreciated --

Thanks,

Greg

make[5]: Leaving directory `/home/ghassett/bfin/uclinux-dist/lib/tslib-1.0/etc'

Making all in src

make[5]: Entering directory `/home/ghassett/bfin/uclinux-dist/lib/tslib-1.0/src'

if /bin/sh ../libtool --tag=CC --mode=compile bfin-uclinux-gcc -DHAVE_CONFIG_H -I. -I. -I..    -DPLUGIN_DIR=\"/usr/bfin/lib/ts/\" -DTS_CONF=\"/usr/bfin/etc/ts.conf\"  -DTSLIB_INTERNAL -fvisibility=hidden -DGCC_HASCLASSVISIBILITY -O2 -Wall -W -MT ts_load_module.lo -MD -MP -MF ".deps/ts_load_module.Tpo" -c -o ts_load_module.lo ts_load_module.c; \

        then mv -f ".deps/ts_load_module.Tpo" ".deps/ts_load_module.Plo"; else rm -f ".deps/ts_load_module.Tpo"; exit 1; fi

Making install in lzo

make[6]: Entering directory `/home/ghassett/bfin/uclinux-dist/lib/lzo/build-lzo-2.02/include/lzo'

make[7]: Entering directory `/home/ghassett/bfin/uclinux-dist/lib/lzo/build-lzo-2.02/include/lzo'

make[7]: Nothing to be done for `install-exec-am'.

test -z "/usr/include/lzo" || mkdir -p -- "/home/ghassett/bfin/uclinux-dist/staging/usr/include/lzo"

/usr/bin/install -c -m 644 '../../../lzo-2.02/include/lzo/lzoconf.h' '/home/ghassett/bfin/uclinux-dist/staging/usr/include/lzo/lzoconf.h'

/usr/bin/install -c -m 644 '../../../lzo-2.02/include/lzo/lzodefs.h' '/home/ghassett/bfin/uclinux-dist/staging/usr/include/lzo/lzodefs.h'

/usr/bin/install -c -m 644 '../../../lzo-2.02/include/lzo/lzoutil.h' '/home/ghassett/bfin/uclinux-dist/staging/usr/include/lzo/lzoutil.h'

/usr/bin/install -c -m 644 '../../../lzo-2.02/include/lzo/lzo_asm.h' '/home/ghassett/bfin/uclinux-dist/staging/usr/include/lzo/lzo_asm.h'

/usr/bin/install -c -m 644 '../../../lzo-2.02/include/lzo/lzo1.h' '/home/ghassett/bfin/uclinux-dist/staging/usr/include/lzo/lzo1.h'

/usr/bin/install -c -m 644 '../../../lzo-2.02/include/lzo/lzo1a.h' '/home/ghassett/bfin/uclinux-dist/staging/usr/include/lzo/lzo1a.h'

/usr/bin/install -c -m 644 '../../../lzo-2.02/include/lzo/lzo1b.h' '/home/ghassett/bfin/uclinux-dist/staging/usr/include/lzo/lzo1b.h'

/usr/bin/install -c -m 644 '../../../lzo-2.02/include/lzo/lzo1c.h' '/home/ghassett/bfin/uclinux-dist/staging/usr/include/lzo/lzo1c.h'

/usr/bin/install -c -m 644 '../../../lzo-2.02/include/lzo/lzo1f.h' '/home/ghassett/bfin/uclinux-dist/staging/usr/include/lzo/lzo1f.h'

/usr/bin/install -c -m 644 '../../../lzo-2.02/include/lzo/lzo1x.h' '/home/ghassett/bfin/uclinux-dist/staging/usr/include/lzo/lzo1x.h'

/usr/bin/install -c -m 644 '../../../lzo-2.02/include/lzo/lzo1y.h' '/home/ghassett/bfin/uclinux-dist/staging/usr/include/lzo/lzo1y.h'

/usr/bin/install -c -m 644 '../../../lzo-2.02/include/lzo/lzo1z.h' '/home/ghassett/bfin/uclinux-dist/staging/usr/include/lzo/lzo1z.h'

bfin-uclinux-gcc -DHAVE_CONFIG_H -I. -I. -I.. -DPLUGIN_DIR=\"/usr/bfin/lib/ts/\" -DTS_CONF=\"/usr/bfin/etc/ts.conf\" -DTSLIB_INTERNAL -fvisibility=hidden -DGCC_HASCLASSVISIBILITY -O2 -Wall -W -MT ts_load_module.lo -MD -MP -MF .deps/ts_load_module.Tpo -c ts_load_module.c  -fPIC -DPIC -o .libs/ts_load_module.o

ts_load_module.c:20:19: error: dlfcn.h: No such file or directory

ts_load_module.c: In function '__ts_load_module':

ts_load_module.c:48: warning: implicit declaration of function 'dlopen'

ts_load_module.c:48: error: 'RTLD_NOW' undeclared (first use in this function)

ts_load_module.c:48: error: (Each undeclared identifier is reported only once

ts_load_module.c:48: error: for each function it appears in.)

ts_load_module.c:48: warning: assignment makes pointer from integer without a cast

ts_load_module.c:52: warning: implicit declaration of function 'dlsym'

ts_load_module.c:52: warning: assignment makes pointer from integer without a cast

ts_load_module.c:54: warning: implicit declaration of function 'dlclose'

make[5]: *** [ts_load_module.lo] Error 1

make[5]: Leaving directory `/home/ghassett/bfin/uclinux-dist/lib/tslib-1.0/src'

make[4]: *** [all-recursive] Error 1

make[4]: Leaving directory `/home/ghassett/bfin/uclinux-dist/lib/tslib-1.0'

make[3]: *** [all] Error 2

make[3]: Leaving directory `/home/ghassett/bfin/uclinux-dist/lib/tslib-1.0'

make[2]: *** [tslib-1.0] Error 2

make[2]: *** Waiting for unfinished jobs....

/usr/bin/install -c -m 644 '../../../lzo-2.02/include/lzo/lzo2a.h' '/home/ghassett/bfin/uclinux-dist/staging/usr/include/lzo/lzo2a.h'

make[7]: Leaving directory `/home/ghassett/bfin/uclinux-dist/lib/lzo/build-lzo-2.02/include/lzo'

make[6]: Leaving directory `/home/ghassett/bfin/uclinux-dist/lib/lzo/build-lzo-2.02/include/lzo'

make[6]: Entering directory `/home/ghassett/bfin/uclinux-dist/lib/lzo/build-lzo-2.02/include'

make[7]: Entering directory `/home/ghassett/bfin/uclinux-dist/lib/lzo/build-lzo-2.02/include'

make[7]: Nothing to be done for `install-exec-am'.

make[7]: Nothing to be done for `install-data-am'.

make[7]: Leaving directory `/home/ghassett/bfin/uclinux-dist/lib/lzo/build-lzo-2.02/include'

make[6]: Leaving directory `/home/ghassett/bfin/uclinux-dist/lib/lzo/build-lzo-2.02/include'

make[5]: Leaving directory `/home/ghassett/bfin/uclinux-dist/lib/lzo/build-lzo-2.02/include'

Making install in src

make[5]: Entering directory `/home/ghassett/bfin/uclinux-dist/lib/lzo/build-lzo-2.02/src'

make[6]: Entering directory `/home/ghassett/bfin/uclinux-dist/lib/lzo/build-lzo-2.02/src'

test -z "/usr/lib" || mkdir -p -- "/home/ghassett/bfin/uclinux-dist/staging/usr/lib"

make[6]: Nothing to be done for `install-data-am'.

/bin/sh ../libtool --mode=install /usr/bin/install -c  'liblzo2.la' '/home/ghassett/bfin/uclinux-dist/staging/usr/lib/liblzo2.la'

/usr/bin/install -c .libs/liblzo2.lai /home/ghassett/bfin/uclinux-dist/staging/usr/lib/liblzo2.la

/usr/bin/install -c .libs/liblzo2.a /home/ghassett/bfin/uclinux-dist/staging/usr/lib/liblzo2.a

bfin-uclinux-ranlib /home/ghassett/bfin/uclinux-dist/staging/usr/lib/liblzo2.a

chmod 644 /home/ghassett/bfin/uclinux-dist/staging/usr/lib/liblzo2.a

libtool: install: warning: remember to run `libtool --finish /usr/lib'

make[6]: Leaving directory `/home/ghassett/bfin/uclinux-dist/lib/lzo/build-lzo-2.02/src'

make[5]: Leaving directory `/home/ghassett/bfin/uclinux-dist/lib/lzo/build-lzo-2.02/src'

Making install in lzotest

make[5]: Entering directory `/home/ghassett/bfin/uclinux-dist/lib/lzo/build-lzo-2.02/lzotest'

make[6]: Entering directory `/home/ghassett/bfin/uclinux-dist/lib/lzo/build-lzo-2.02/lzotest'

make[6]: Nothing to be done for `install-exec-am'.

make[6]: Nothing to be done for `install-data-am'.

make[6]: Leaving directory `/home/ghassett/bfin/uclinux-dist/lib/lzo/build-lzo-2.02/lzotest'

make[5]: Leaving directory `/home/ghassett/bfin/uclinux-dist/lib/lzo/build-lzo-2.02/lzotest'

Making install in examples

make[5]: Entering directory `/home/ghassett/bfin/uclinux-dist/lib/lzo/build-lzo-2.02/examples'

make[6]: Entering directory `/home/ghassett/bfin/uclinux-dist/lib/lzo/build-lzo-2.02/examples'

make[6]: Nothing to be done for `install-exec-am'.

make[6]: Nothing to be done for `install-data-am'.

make[6]: Leaving directory `/home/ghassett/bfin/uclinux-dist/lib/lzo/build-lzo-2.02/examples'

make[5]: Leaving directory `/home/ghassett/bfin/uclinux-dist/lib/lzo/build-lzo-2.02/examples'

Making install in tests

make[5]: Entering directory `/home/ghassett/bfin/uclinux-dist/lib/lzo/build-lzo-2.02/tests'

make[6]: Entering directory `/home/ghassett/bfin/uclinux-dist/lib/lzo/build-lzo-2.02/tests'

make[6]: Nothing to be done for `install-exec-am'.

make[6]: Nothing to be done for `install-data-am'.

make[6]: Leaving directory `/home/ghassett/bfin/uclinux-dist/lib/lzo/build-lzo-2.02/tests'

make[5]: Leaving directory `/home/ghassett/bfin/uclinux-dist/lib/lzo/build-lzo-2.02/tests'

Making install in minilzo

make[5]: Entering directory `/home/ghassett/bfin/uclinux-dist/lib/lzo/build-lzo-2.02/minilzo'

make[6]: Entering directory `/home/ghassett/bfin/uclinux-dist/lib/lzo/build-lzo-2.02/minilzo'

make[6]: Nothing to be done for `install-exec-am'.

make[6]: Nothing to be done for `install-data-am'.

make[6]: Leaving directory `/home/ghassett/bfin/uclinux-dist/lib/lzo/build-lzo-2.02/minilzo'

make[5]: Leaving directory `/home/ghassett/bfin/uclinux-dist/lib/lzo/build-lzo-2.02/minilzo'

make[5]: Entering directory `/home/ghassett/bfin/uclinux-dist/lib/lzo/build-lzo-2.02'

make[6]: Entering directory `/home/ghassett/bfin/uclinux-dist/lib/lzo/build-lzo-2.02'

make[6]: Nothing to be done for `install-exec-am'.

make[6]: Nothing to be done for `install-data-am'.

make[6]: Leaving directory `/home/ghassett/bfin/uclinux-dist/lib/lzo/build-lzo-2.02'

make[5]: Leaving directory `/home/ghassett/bfin/uclinux-dist/lib/lzo/build-lzo-2.02'

make[4]: Leaving directory `/home/ghassett/bfin/uclinux-dist/lib/lzo/build-lzo-2.02'

make post-build

make[4]: Entering directory `/home/ghassett/bfin/uclinux-dist/lib/lzo'

make[4]: Nothing to be done for `post-build'.

make[4]: Leaving directory `/home/ghassett/bfin/uclinux-dist/lib/lzo'

/home/ghassett/bfin/uclinux-dist/tools/cross-fix-root

make[3]: Leaving directory `/home/ghassett/bfin/uclinux-dist/lib/lzo'

make[2]: Leaving directory `/home/ghassett/bfin/uclinux-dist/lib'

make[1]: *** [all] Error 2

make[1]: Leaving directory `/home/ghassett/bfin/uclinux-dist/lib'

make: *** [subdirs] Error 1

[ghassett@localhost uclinux-dist]$

QuoteReplyEditDelete

2009-03-23 03:59:47     Re: tslib woes

Mike Frysinger (UNITED STATES)

Message: 71361   

tslib will only work when built as FDPIC

QuoteReplyEditDelete

2009-03-23 09:11:16     Re: tslib woes

Gregory Hassett (UNITED STATES)

Message: 71368   

Hi Mike...

Does this mean that I need to use "make makeconfig" to change "Blackfin build options --> Binary Format" to FDPIC and rebuild the entire kernel this way, or is is possible to build tslib in FDPIC format while leaving the rest of the build in the default (FLAT) format?

Thanks

Greg

QuoteReplyEditDelete

2009-03-23 14:05:04     Re: tslib woes

Mike Frysinger (UNITED STATES)

Message: 71381   

you can mix FLAT and FDPIC applications, but the dist doesnt support that kind of granularity.  you'll have to build the whole dist as FDPIC.

  • Created
Was this helpful?

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.