2009-03-11 01:26:36     adding new field to event subsystem

2009-03-11 01:26:36     adding new field to event subsystem

abhrajit datta (INDIA)

Message: 70735   

Hi,

I want to add a new event type to the input subsystem. My accelerometer reports events such as tap and activity, for which there are no suitable fields in the input subsystem. Can i customize the input.c file. In which files should i have to add code if i want to do something similiar?

Thanks

Abhri

QuoteReplyEditDelete

2009-03-11 04:03:36     Re: adding new field to event subsystem

Mike Frysinger (UNITED STATES)

Message: 70738   

you should send your question to linux-input@vger.kernel.org as they should know ...

  • Created
Was this helpful?

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.