2009-03-09 03:38:27     uclinux-dist can't start with the uboot

2009-03-09 03:38:27     uclinux-dist can't start with the uboot

wenchao zhou (CHINA)

Message: 70574   

Hi   Mike,

     I   have download the uclinux-dist-2007R1-RC3,and i have make the uclinux-dist successfully. Then  i  download the

uboot1.1.1 to the ADI BF533 board.the uboot1.1.1 is provided by the adi factory which send me the board .And the uboot

has been ported right, i used to use the uboot1.1.1 and the uclinux-dist provided by the factory ,and i could use NFS to start the uclinux-dist with the uboot1.1.1,the process is like this:

BOOT> tftp 0x100000 linux.bin

TFTP from server 59.77.17.105; our IP address is 59.77.17.1

Filename 'linux.bin'.

Load address: 0x100000

Loading: *#################################################################

         #################################################################

         #################################################################

         #######

done

Bytes transferred = 1030848 (fbac0 hex)

BOOT> go 0x100000

## Starting application at 0x00100000 ...

Linux version 2.6.8.1 (Administrator@cmdstudi-8ed6ad) (gcc version 3.4.4) #73 Mon Dec 29 17:20:11 2008

Blackfin support (C) 2004 Analog Devices, Inc.

ADSP-BF533 Rev. 0.5

uClinux/BF533

Blackfin uClinux support by blackfin.uclinux.org

Processor Speed: 216 MHz core clock and 54 Mhz System Clock

Board Memory: 32MB

Memory map:

  text = 0x100000-0x1df584

  data = 0x1ec1a0-0x1fbac0

  bss  = 0x1fbac0-0x20eb4c

  rootfs = 0x20eb4c-0x20f000

  stack = 0x300000-0x500000

Command line: 'root=/dev/nfs rw nfsroot=59.77.17.105:/home/eflag-bfin/uClinux-dist/romfs ip=59.77.17.1:59.77.17.105:59.77.17.1:255.0.0.0 mem=32M console=ttyS0,57600'

DCPLB pos 24

Instruction Cache Enabled

Data Cache Enabled (write-through)

Built 1 zonelists

Kernel command line: root=/dev/nfs rw nfsroot=59.77.17.105:/home/eflag-bfin/uClinux-dist/romfs ip=59.77.17.1:59.77.17.105:59.77.17.1:255.0.0.0 mem=32M console=ttyS0,57600

Whoops

Configuring Blackfin Priority Driven Interrupts

PID hash table entries: 16 (order 4: 128 bytes)

Dentry cache hash table entries: 4096 (order: 2, 16384 bytes)

Inode-cache hash table entries: 2048 (order: 1, 8192 bytes)

Physical pages: 1f00

Memory available: 27276k/30799k RAM, (48k init code, 893k kernel code, 138k data, 1024k dma)

Blackfin Scratchpad data SRAM: 4 KB

Blackfin DATA_A SRAM: 16 KB

Blackfin DATA_B SRAM: 16 KB

Calibrating delay loop... 39.21 BogoMIPS

Mount-cache hash table entries: 512 (order: 0, 4096 bytes)

Freeing initrd memory: 512k freed

NET: Registered protocol family 16

evm02_init(): registering device resources

fbmem init is called

fbmen init is done

devfs: 2004-01-31 Richard Gooch (rgooch@atnf.csiro.au)

devfs: boot_options: 0x1

spi0: INIT

BlackFin BF533 serial driver version 2.00 With DMA Support

ttyS0 at irq = 21 is a builtin BlackFin BF533 UART

Enabling Serial UART Interrupts

RAMDISK driver initialized: 16 RAM disks of 10240K size 1024 blocksize

Using anticipatory io scheduler

nbd: registered device at major 43

eth0: cs8900 rev K found at 0x203d4600

cs89x0: Extended EEPROM checksum bad and no Cirrus EEPROM, relying on command line

cs89x0 media RJ-45, IRQ 34, programmed I/O, MAC 61:00:00:1d:2d:02

temp_video_init is called

***** video_setup called

mice: PS/2 mouse device common for all mice

NET: Registered protocol family 2

IP: routing cache hash table of 512 buckets, 4Kbytes

TCP: Hash tables configured (established 2048 bind 4096)

NET: Registered protocol family 1

NET: Registered protocol family 17

eth0: using half-duplex 10Base-T (RJ-45)

IP-Config: Complete:

      device=eth0, addr=59.77.17.1, mask=255.0.0.0, gw=59.77.17.1,

     host=59.77.17.1, domain=, nis-domain=(none),

     bootserver=59.77.17.105, rootserver=59.77.17.105, rootpath=

RAMDISK: Couldn't find valid RAM disk image starting at 0.

Looking up port of RPC 100003/2 on 59.77.17.105

Looking up port of RPC 100005/1 on 59.77.17.105

VFS: Mounted root (nfs filesystem).

Mounted devfs on /dev

Freeing unused kernel memory: 48k freed (0x1e0000 - 0x1eb000)

Shell invoked to run file: /etc/rc

Reading command line: Input/output error

Execution Finished, Exiting

Sash command shell (version 1.1.1)

/>

i use the address :tftp 0x100000 linux.bin  ,the address is follow the factory's instruction about the board.

But now i use the uclinux-dist 2007R1-RC3(because i want to use the linphone in it ,the old uclinux-dist provide by the factory don't include the linphone),but i can't start the new uclinux-dist with the uboot1.1.1 now.  the new process is like this:

BOOT>tftp 0x1000000 linux                                            (the linux is copyed from the /uClinux-dist/images)

BOOT>bootelf 0x1000000                                         

Loading  .text @0x00001000 (1097896 bytes)

Loading  .init @0x0010d0a8 (1097896 bytes)

Loading  .text_l1 @0xffa00000 (8496 bytes)

Loading  .data @ 0x0011e76c (218240 bytes)

Clearing .bss @ 0x00153bf0 (56096 bytes)

##Starting application at 0x00001000

And the process stop here.i use the new address 0x1000000 which is advised by your website.In the past,i use the address 0x100000.

Mike,i asked the problem yesterday and somebody tell me that i should use the uclinux-dist-2008R1.5 or later release.

but i think the 2007R1-RC3 is enough for me. I saw the note of 2007r1 release ,and it remind we should use the uboot1.1.6 for the uclinux-2007R1-RC3.Is it because i use the uboot too old.?  I  also discover that the uclinux-dist start

address is different between  the two proccess i paste upon.If i can solve the problem by alter the start address ,i will save

a lot of time for me .Or do you think i should port the uboot1.1.6 myself for the new uclinux-dist.

Thanks for all of your help,it is very useful!

Regards

Zhou 

QuoteReplyEditDelete

2009-03-09 03:40:32     Re: uclinux-dist can't start with the uboot

Mike Frysinger (UNITED STATES)

Message: 70575   

you were already told that the software you're using is old.  use 2008R1.5.

QuoteReplyEditDelete

2009-03-09 04:50:49     Re: uclinux-dist can't start with the uboot

wenchao zhou (CHINA)

Message: 70593   

Hi,Mike!

I have followed your advice ,now i use the  linux-bf533-ezkit-2008R1.5-RC3 download from your website and the uboot is

the uboot1.1.1,but the system still can't start.Tht process is like this:

BOOT> tftp 0x1000000 linux-bf533-ezkit-2008R1.5-RC3

TFTP from server 59.77.17.245; our IP address is 59.77.17.1

Filename 'linux-bf533-ezkit-2008R1.5-RC3'.

Load address: 0x1000000

Loading: #################################################################

         #################################################################

         #################################################################

         #################################################################

         #################################################################

         #################################################################

         #################################################################

         #################################################################

         #################################################################

         #################################################################

         #################################################################

         #################################################################

         #################################################################

         ###################################

done

Bytes transferred = 4502466 (44b3c2 hex)

BOOT> bootelf 0x1000000

Loading .text @ 0x00001000 (977312 bytes)

Loading .rodata @ 0x000f0000 (213456 bytes)

Loading __ksymtab @ 0x001241d0 (13992 bytes)

Loading __ksymtab_gpl @ 0x00127878 (3840 bytes)

Loading __ksymtab_strings @ 0x00128778 (42576 bytes)

Loading __param @ 0x00132dc8 (320 bytes)

Loading .data @ 0x00133000 (69632 bytes)

Loading .init.text @ 0x00144000 (80460 bytes)

Loading .init.data @ 0x00157a4c (3240 bytes)

Loading .init.setup @ 0x001586f4 (588 bytes)

Loading .initcall.init @ 0x00158940 (412 bytes)

Loading .con_initcall.init @ 0x00158adc (4 bytes)

Loading .init.ramfs @ 0x00158ae0 (2555040 bytes)

Loading .text_l1 @ 0xffa00000 (8248 bytes)

Loading .data_l1 @ 0xff800000 (192 bytes)

Clearing .bss @ 0x003cb000 (59120 bytes)

## Starting application at 0x00144000 ...�

It stops here.

Does it because the uboot cannot match the uclinux-dist?Should i upgrade the uboot to uboot1.1.6 and port the new uboot

to my board?

Thanks for your  patient and help!

Regards

Zhou

QuoteReplyEditDelete

2009-03-09 04:55:34     Re: uclinux-dist can't start with the uboot

Mike Frysinger (UNITED STATES)

Message: 70595   

update everything, not just the kernel

QuoteReplyEditDelete

2009-03-09 05:10:29     Re: uclinux-dist can't start with the uboot

wenchao zhou (CHINA)

Message: 70597   

OK,i would try to port. Thanks Mike!

QuoteReplyEditDelete

2009-03-09 06:08:06     Re: uclinux-dist can't start with the uboot

Mike Frysinger (UNITED STATES)

Message: 70598   

there is no porting for you to do.  we've already done all the porting work for the BF533-EZKIT platform.

  • Created
Was this helpful?

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.