2009-02-09 17:00:03     PPI BF527 won't compile

2009-02-09 17:00:03     PPI BF527 won't compile

Adam Dershowitz (UNITED STATES)

Message: 69149   

I am trying to use the Blackfin BF5xx Driver with uClinux-dist-2008R1.5-RC3.  If I try to compile it for the BF527 I get an error:

Undefined Reference to "bfin_clear_PPI_STATUS"

I foudn that all of the related things are defined in:  include/asm-blackfin/machbf527/cdefBF52x_base.h

And that it is defined in machbf-537/cdefbf534.h this way:

#define bfin_clear_PPI_STATUS()              bfin_write_PPI_STATUS(0xFFFF)

So I copied that definition into the cdefbfBF52x_base.h and now it does compile.  But I want to make sure that is the correct definition for the 527.  The bug tracker #2562 shows that there was a problem with this, but that it was fixed.

So, my  questions are 1)  Why isn't this defined for the 527?  Just an accidental oversight or something else to be aware of?

2) Who should I report this to, so that it can be fixed in the future?

3)  Is bfin_write_PPI_STATUS(0xFFFF) the correct way to clear the PPI status on a BF527?

Thanks,

--Adam

QuoteReplyEditDelete

2009-02-09 17:28:51     Re: PPI BF527 won't compile

Mike Frysinger (UNITED STATES)

Message: 69151   

the PPI driver in the release really only works for BF533 and BF537.  it has been rewritten in svn trunk and should work on all platforms now (including the BF52x).

QuoteReplyEditDelete

2009-02-09 20:52:47     Re: PPI BF527 won't compile

Adam Dershowitz (UNITED STATES)

Message: 69160   

OK.

I just downloaded char/bfin_ppi.c and char/bfin_ppi.h.  When I try to build I get build errors.

In function 'disable_ppi_dma'

bfin_ppi.c:150  error:  'ANOMALY_0500278' undeclared.

Are there other files that I need to get this new version to work?  Do I need a full svn snapshot of the whole linux-2.6.x kernel?  Or are there just a few other changes that perhaps you can point me to?

Thank you for the help.

--Adam

QuoteReplyEditDelete

2009-02-09 20:59:30     Re: PPI BF527 won't compile

Robin Getz (UNITED STATES)

Message: 69162   

Adam:

You need the whole things - trunk toolchain, trunk U-Boot, trunk linux kernel, trunk uClinux Dist - the whole shooting match.

If you wonder why - check out the faq.

http://docs.blackfin.uclinux.org/doku.php?id=faq

-Robin

QuoteReplyEditDelete

2009-02-09 20:59:34     Re: PPI BF527 won't compile

Mike Frysinger (UNITED STATES)

Message: 69163   

you can try to backport the changes yourself or just grab the latest code from svn/git

QuoteReplyEditDelete

2009-02-10 03:56:03     Re: PPI BF527 won't compile

Michael Hennerich (GERMANY)

Message: 69176   

Mike,

ANOMALY_05000278 is not defined for BF51x, BF54x and BF52x can you please add these.

Adam,

As a temp. solution - Simply add following line into the driver

#define ANOMALY_05000278 0 /* in case you compile for BF52x */

-Michael

QuoteReplyEditDelete

2009-02-10 04:10:46     Re: PPI BF527 won't compile

Mike Frysinger (UNITED STATES)

Message: 69177   

should be all set now in trunk

QuoteReplyEditDelete

2009-02-10 13:07:47     Re: PPI BF527 won't compile

Adam Dershowitz (UNITED STATES)

Message: 69212   

Robin,

that FAQ doesn't really address my question.  Because we are not yet talking about a release.  I  have the latest release, and now we are just talking about a patch to that.  I assume that stuff in SVN repository has not yet gone through the full set of testing (or it would be a release)

So, depending on what has been changed I could imagine that the release code could be more stable, and just using the new ppi could work with it  fine.  Or, it could be that it needs features in the newer version of the rest of the code, so that a full update, from the release to trunk, is necesssary, or at least more stable.

I will try just the fixed version of the ppi code initially, and see what happens.

--Adam

QuoteReplyEditDelete

2009-02-10 20:19:03     Re: PPI BF527 won't compile

Robin Getz (UNITED STATES)

Message: 69225   

Adam:

The FAQ does address the point I was making -- The question "Why do I need to use the same version of toolchain/kernel/uClibc/U-boot/uClinux-dist?"

I'm not as hopeful as Mike - and don't normally suggest people backport things from trunk to the last release. If you want to use a feature from trunk - use trunk - and that means upgrade everything - as the FAQ states.

-Robin

QuoteReplyEditDelete

2009-02-11 13:18:12     Re: PPI BF527 won't compile

Adam Dershowitz (UNITED STATES)

Message: 69273   

I tried just changing those two files, and now it does compile.  But when I run it, I don't see anything new in /dev/

And, during my boot I see:

ppi: can't         get major 252

Is this a known problem?  Any suggestions?  Perhaps the answer is that this relates to me not doing a full update, as Robin had suggested, and I need the trunk versions?

Thanks,

--Adam

QuoteReplyEditDelete

2009-02-11 13:23:21     Re: PPI BF527 won't compile

Mike Frysinger (UNITED STATES)

Message: 69274   

major numbers are unique.  only one driver can have it at a time.  look at /proc/devices.

QuoteReplyEditDelete

2009-02-11 15:00:43     Re: PPI BF527 won't compile

Adam Dershowitz (UNITED STATES)

Message: 69279   

Thanks.

opt was using 252, so I disabled that and rebuilt.  Now I get a kernel panic on boot from ppi_init_module.

I am trying to download and build the SVN version to see if that helps.

QuoteReplyEditDelete

2009-02-11 15:32:02     Re: PPI BF527 won't compile

Michael Hennerich (GERMANY)

Message: 69282   

Can you post the kernel panic messages?

QuoteReplyEditDelete

2009-02-11 16:15:45     Re: PPI BF527 won't compile

Adam Dershowitz (UNITED STATES)

Message: 69284   

io scheduler noop registered

io scheduler anticipatory registered (default)

io scheduler cfq registered

NULL pointer access (probably)

Kernel OOPS in progress

Defered Exception context

CURRENT PROCESS:

COMM=swapper PID=1

invalid mm

return address: [0x0008b4fa]; contents of:

0x0008b4d0:  05e3  e800  0008  0c81  e630  0011  3021  e632

0x0008b4e0:  0013  e537  0014  1402  2209  3209  e530  0011

0x0008b4f0:  5ac8  0a58  14dc  e531  0013 [9949] 4308  0c00

0x0008b500:  19bd  e535  0011  612a  0810  181c  0a6b  1c04

SEQUENCER STATUS:        Not tainted

SEQSTAT: 00000027  IPEND: 8030  SYSCFG: 0006

  HWERRCAUSE: 0x0

  EXCAUSE   : 0x27

  physical IVG15 asserted : <0xffa00dac> { _evt_system_call + 0x0 }

  logical irq   6 mapped  : <0xffa00250> { _timer_interrupt + 0x0 }

  logical irq  59 mapped  : <0x000c361c> { _blackfin_interrupt + 0x0 }

RETE: <0x00000000> /* Maybe null pointer? */

RETN: <0x03eebef0> /* unknown address */

RETX: <0x0008b4fa> { _vsnprintf + 0x2a }

RETS: <0x0009c0c6> { _device_create + 0x66 }

PC  : <0x0008b4fa> { _vsnprintf + 0x2a }

DCPLB_FAULT_ADDR: <0x00000000> /* Maybe null pointer? */

ICPLB_FAULT_ADDR: <0x0008b4fa> { _vsnprintf + 0x2a }

PROCESSOR STATE:

R0 : 00d3a2a4    R1 : 00000014    R2 : 00000000    R3 : 00d3a400

R4 : 00000014    R5 : 00000000    R6 : 0fc00000    R7 : 00d38ca0

P0 : 00d3a2a4    P1 : 00000000    P2 : 00d3a400    P3 : 00d3a2b8

P4 : 009e9cfc    P5 : 00d3a200    FP : 03eebf6c    SP : 03eebe14

LB0: 0008bd5c    LT0: 0008bd5c    LC0: 00000000

LB1: 0008b7c8    LT1: 0008b7be    LC1: 00000000

B0 : 00000000    L0 : 00000000    M0 : 00000000    I0 : 0018b390

B1 : 00000000    L1 : 00000000    M1 : 00000000    I1 : 00000000

B2 : 00000000    L2 : 00000000    M2 : 00000000    I2 : fffedbb0

B3 : 00000000    L3 : 00000000    M3 : 00000000    I3 : 00000000

A0.w: 00000044   A0.x: 00000000   A1.w: 00000044   A1.x: 00000000

USP : 00000000  ASTAT: 00003024

Hardware Trace:

   0 Target : <0x0000494c> { _trap_c + 0x0 }

     Source : <0xffa006ec> { _exception_to_level5 + 0xb4 }

   1 Target : <0xffa00638> { _exception_to_level5 + 0x0 }

     Source : <0xffa00590> { _ex_trap_c + 0x5c }

   2 Target : <0xffa00534> { _ex_trap_c + 0x0 }

     Source : <0xffa0078c> { _trap + 0x28 }

   3 Target : <0xffa00764> { _trap + 0x0 }

     Source : <0x0008b4f6> { _vsnprintf + 0x26 }

   4 Target : <0x0008b4ea> { _vsnprintf + 0x1a }

     Source : <0x0008b4e6> { _vsnprintf + 0x16 }

   5 Target : <0x0008b4d0> { _vsnprintf + 0x0 }

     Source : <0x0009c0c2> { _device_create + 0x62 }

   6 Target : <0x0009c08c> { _device_create + 0x2c }

     Source : <0x000343bc> { _kmem_cache_zalloc + 0x54 }

   7 Target : <0x000343b4> { _kmem_cache_zalloc + 0x4c }

     Source : <0x0008bd62> { _memset + 0x2e }

   8 Target : <0x0008bd34> { _memset + 0x0 }

     Source : <0x000343b0> { _kmem_cache_zalloc + 0x48 }

   9 Target : <0x00034378> { _kmem_cache_zalloc + 0x10 }

     Source : <0x000343c2> { _kmem_cache_zalloc + 0x5a }

  10 Target : <0x000343c2> { _kmem_cache_zalloc + 0x5a }

     Source : <0x0012572e> { _cond_resched + 0x1a }

  11 Target : <0x00125714> { _cond_resched + 0x0 }

     Source : <0x000343be> { _kmem_cache_zalloc + 0x56 }

  12 Target : <0x000343be> { _kmem_cache_zalloc + 0x56 }

     Source : <0x00034374> { _kmem_cache_zalloc + 0xc }

  13 Target : <0x00034368> { _kmem_cache_zalloc + 0x0 }

     Source : <0x0009c088> { _device_create + 0x28 }

  14 Target : <0x0009c060> { _device_create + 0x0 }

     Source : <0x001a66ac> { _ppi_init_module + 0x8c }

  15 Target : <0x001a6690> { _ppi_init_module + 0x70 }

     Source : <0x00065d56> { _sysfs_add_file + 0x4a }

Stack from 03eebdf4:

        4ea93000 ffa006f0 00184568 00184568 00184564 03ef0478 00044c22 009e8654

        0008b4fa 00008030 00000027 00000000 03eebef0 0008b4fa 0008b4fa 0009c0c6

        00d3a2a4 00003024 0008b7c8 0008bd5c 0008b7be 0008bd5c 00000000 00000000

        00000044 00000000 00000044 00000000 00000000 00000000 00000000 00000000

        00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000

        00000000 fffedbb0 00000000 0018b390 00000000 03eebf6c 00d3a200 009e9cfc

Call Trace:

[<00008124>] _l1_data_B_sram_alloc+0x14/0x34

[<0009e7cc>] _class_register+0x104/0x110

[<0006682e>] _sysfs_make_dirent+0x1e/0x38

[<0009c0c6>] _device_create+0x66/0x90

[<001a66b0>] _ppi_init_module+0x90/0x188

[<00009600>] _in_sched_functions+0x18/0x38

[<001a6398>] _tty_init+0x128/0x158

[<00194654>] _kernel_init+0x88/0x234

[<001945cc>] _kernel_init+0x0/0x234

[<00001666>] _kernel_thread_helper+0x6/0xc

Modules linked in:

Kernel panic - not syncing: Kernel exception

QuoteReplyEditDelete

2009-02-11 16:53:52     Re: PPI BF527 won't compile

Michael Hennerich (GERMANY)

Message: 69287   

I haven't tried the driver on BF52x yet.

Tomorrow - I see if I can recreate the issue on my side.

-Michael

QuoteReplyEditDelete

2009-02-12 06:39:11     Re: PPI BF527 won't compile

Michael Hennerich (GERMANY)

Message: 69340   

Module insertion as well as driver build into the kernel works ok for me on BF527

root:/dev> modprobe bfin_ppi ppi_major=62

root:/dev> modprobe -r bfin_ppi

root:/dev> version

kernel: Linux release 2.6.28.4-ADI-2009R1-pre-svn6093, build #10090 Thu Feb 12 12:33:02 CET 2009

toolchain: bfin-uclinux-gcc release gcc version 4.1.2 (ADI svn)

user-dist: release svn-7707, build #3431 Thu Feb 12 12:32:18 CET 2009

root:/dev>

root:/dev> cat /proc/cpuinfo

processor : 0

vendor_id : Analog Devices

cpu family : 0x27e0

model name : ADSP-BF527 525(MHz CCLK) 131(MHz SCLK) (mpu off)

stepping : 0

cpu MHz : 525.000/131.250000

bogomips : 1044.48

Calibration : 522240000 loops

cache size : 16 KB(L1 icache) 32 KB(L1 dcache-wt) 0 KB(L2 cache)

dbank-A/B : cache/cache

icache setup : 4 Sub-banks/4 Ways, 32 Lines/Way

dcache setup : 2 Super-banks/4 Sub-banks/2 Ways, 64 Lines/Way

board name : ADI BF527-EZKIT

board memory : 65536 kB (0x00000000 -> 0x04000000)

kernel memory : 64504 kB (0x00001000 -> 0x03eff000)

root:/dev>

QuoteReplyEditDelete

2009-02-12 13:15:10     Re: PPI BF527 won't compile

Adam Dershowitz (UNITED STATES)

Message: 69354   

Thanks.

I upgraded to the SVN snapshot of linux and now it does seem to be working.

I think that just upgrading those couple of files was not enough, with the 20081.5RC3, for it to work.  There is something else that was missing or different.

QuoteReplyEditDelete

2009-02-20 20:00:27     Re: PPI BF527 won't compile

Adam Dershowitz (UNITED STATES)

Message: 69708   

I have been trying to track down a problem related to this ppi driver.  I was working from ppitest.c that is included.

What I realized is that ppitest tries to set both

CMD_PPI_PORT_DIRECTION and CMD_PPI_PACKING.  Neither of these appear to be valid to the driver.  So, when ppitest is run, I get

device ioctl error:  Invalid argument.

I tried commenting out those two things commands from the setup.  Now my code works, sometimes.  But it seems to depend on the version of u-boot that is being used.  I assume that is because of some other parameter being set, or not set by u-boot, and then not being conifigured properly in the setup.

Any ideas?

QuoteReplyEditDelete

2009-02-20 20:04:53     Re: PPI BF527 won't compile

Mike Frysinger (UNITED STATES)

Message: 69709   

if you're using the bf527-ezkit, then u-boot will configure the ppi for the lcd to display the splash screen

QuoteReplyEditDelete

2009-06-05 06:17:09     Re: PPI BF527 won't compile

Stefan Wanja (GERMANY)

Message: 75249   

Hello,

I am trying to get the adv7183b extension board with the bf527 ezkit working. I just checked out the svn trunk and tried to build, but I still get an error about a missing definition of  bfin_clear_PPI_STATUS. Shouldn't this be added into 'arch/blackfin/mach-bf527/include/mach/cdefBF52x_base.h'  ?

QuoteReplyEditDelete

  • Created
Was this helpful?

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.