2009-01-13 09:17:22     Qt application build

2009-01-13 09:17:22     Qt application build

Nikolay Chokoev (IRELAND)

Message: 67879   

Hi,

How can I build a custom Qt application? How to setup tools? Is there any documentation?

Best regards,

Nikolay

QuoteReplyEditDelete

2009-01-13 10:05:38     Re: Qt application build

Mike Frysinger (UNITED STATES)

Message: 67884   

http://www.qtsoftware.com/products

QuoteReplyEditDelete

2009-01-14 04:34:59     Re: Qt application build

Nikolay Chokoev (IRELAND)

Message: 67926   

Hi Mike,

I'm asking in terms of ucLinux distribution for blackfin....

...there are "tools/bfin-linux-uclibc-qmake" I suppose I have to use instead 'qmake'. Is it true? What else?

Regards,

Nikolay

QuoteReplyEditDelete

2009-01-14 06:07:00     Re: Qt application build

Mike Frysinger (UNITED STATES)

Message: 67934   

that is a wrapper for the normal qmake binary that you can use when generating a cross-Makefile

QuoteReplyEditDelete

2009-01-14 07:01:51     Re: Qt application build

Nikolay Chokoev (IRELAND)

Message: 67940   

I'm trying to cross-build a Qt application which is in separate from the ucLinux folder. I'm running the qmake-wrapper, which makes Makefile. That's OK, but when I run 'make' on this folder I have a lot of errors, probably because of wrong environment variable values.

Usualy when I build Qt application 'qmake' and 'make' on the Qt application folder do the job, but in this cross-compile situation doesn't.

How to proceed? Is there any script ....or something to set the needed variables/environment for me?

...some variables I've set:

STAGEDIR=/usr/dlnx764/svn/uclinux-dist/staging

QTDIR=/usr/dlnx764/svn/uclinux-dist/lib/qt-embedded/qt-embedded-linux-opensource-src-4.4.3

QuoteReplyEditDelete

2009-01-14 13:06:11     Re: Qt application build

Mike Frysinger (UNITED STATES)

Message: 67946   

cant really guess without seeing the actual build/errors

  • Created
Was this helpful?

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.