2009-01-03 08:47:43     Where can I find the implement of Blackfin GCC Built-in Functions

2009-01-03 08:47:43     Where can I find the implement of Blackfin GCC Built-in Functions

haiping zeng (CHINA)

Message: 67318   

Hi.

as show in the  title of this thread:

Where can I find the implement of Blackfin GCC Built-in Functions.

as follow:

__builtin_bfin_mult_fr1x32

__builtin_bfin_add_fr1x32

__builtin_bfin_add_fr1x16

-------------------------------------------------------------------------------------------

Word16 round(Word32 L_var1)

{

    Word16 var_out;

    Word32 L_arrondi;

    L_arrondi = L_add(L_var1, (Word32)0x00008000L);

    var_out = extract_h(L_arrondi);

    return(var_out);

}

-------------------------------------------------------------------------------------------

Becuase i want to study how to code the Blackfin GCC Built-in Function and  add the round function to become the Blackfin GCC Built-in Function.could someone give me some helps?thanks.

QuoteReplyEditDelete

2009-01-03 08:59:48     Re: Where can I find the implement of Blackfin GCC Built-in Functions

Mike Frysinger (UNITED STATES)

Message: 67319   

all of the builtins come from gcc itself, so look in the gcc source directory.  gcc-*/gcc/config/bfin/ ...

QuoteReplyEditDelete

2009-01-13 03:56:53     Re: Where can I find the implement of Blackfin GCC Built-in Functions

haiping zeng (CHINA)

Message: 67843   

Hi

i want to find the implement of Blackfin GCC Built-in Functions from the Index of /trunk/gcc-4.1/gcc/config/bfin/...(links as :http://blackfin.uclinux.org/gf/project/toolchain/scmsvn/?action=browse&path=%2Ftrunk%2Fgcc-4.1%2Fgcc%2Fconfig%2Fbfin%2F),but i cannt find some codes about that implement.

QuoteReplyEditDelete

2009-01-13 06:18:29     Re: Where can I find the implement of Blackfin GCC Built-in Functions

Mike Frysinger (UNITED STATES)

Message: 67862   

you'll need to be specific as to what function exactly you're looking for ... all the Blackfin specific builtins are in there

QuoteReplyEditDelete

2009-01-13 07:09:06     Re: Where can I find the implement of Blackfin GCC Built-in Functions

haiping zeng (CHINA)

Message: 67869   

such as :__builtin_bfin_mult_fr1x32();

in bfin.c file ,what we can find is only like this :  

def_builtin ("__builtin_bfin_mult_fr1x32", int_ftype_short_short,

  BFIN_BUILTIN_MULT_1X32);

  def_builtin ("__builtin_bfin_mult_fr1x32x32", int_ftype_int_int,

  BFIN_BUILTIN_MULT_1X32X32);

  def_builtin ("__builtin_bfin_mult_fr1x32x32NS", int_ftype_int_int,

  BFIN_BUILTIN_MULT_1X32X32NS);

{ CODE_FOR_flag_mulhisi, "__builtin_bfin_mult_fr1x32", BFIN_BUILTIN_MULT_1X32, MACFLAG_NONE }

but i can not find the implement of this function? Could  you tell me which files i can find that?

QuoteReplyEditDelete

2009-01-13 07:26:36     Re: Where can I find the implement of Blackfin GCC Built-in Functions

Mike Frysinger (UNITED STATES)

Message: 67870   

that's because it isnt an external symbol.  it expands into assembly.  the bfin.c file contains that information as well (look for the associated constant BFIN_BUILTIN_MULT_1X32).

QuoteReplyEditDelete

2009-01-13 08:31:25     Re: Where can I find the implement of Blackfin GCC Built-in Functions

haiping zeng (CHINA)

Message: 67876   

Hi ,Mike ,

yes ,i find the symbol BFIN_BUILTIN_MULT_1X32 in a emum{...};

enum bfin_builtins

3859: {

3860: BFIN_BUILTIN_CSYNC,

3861: BFIN_BUILTIN_SSYNC,

3862: BFIN_BUILTIN_COMPOSE_2X16,

3863: BFIN_BUILTIN_EXTRACTLO,

3864: BFIN_BUILTIN_EXTRACTHI,

3865:

3866: BFIN_BUILTIN_SSADD_2X16,

3867: BFIN_BUILTIN_SSSUB_2X16,

3868: BFIN_BUILTIN_SSADDSUB_2X16,

3869: BFIN_BUILTIN_SSSUBADD_2X16,

3870: BFIN_BUILTIN_MULT_2X16,

3871: BFIN_BUILTIN_MULTR_2X16,

3872: BFIN_BUILTIN_NEG_2X16,

3873: BFIN_BUILTIN_ABS_2X16,

3874: BFIN_BUILTIN_MIN_2X16,

3875: BFIN_BUILTIN_MAX_2X16,

3876:

3877: BFIN_BUILTIN_SSADD_1X16,

3878: BFIN_BUILTIN_SSSUB_1X16,

3879: BFIN_BUILTIN_MULT_1X16,

3880: BFIN_BUILTIN_MULTR_1X16,

3881: BFIN_BUILTIN_NORM_1X16,

3882: BFIN_BUILTIN_NEG_1X16,

3883: BFIN_BUILTIN_ABS_1X16,

3884: BFIN_BUILTIN_MIN_1X16,

3885: BFIN_BUILTIN_MAX_1X16,

3886:

3887: BFIN_BUILTIN_DIFFHL_2X16,

3888: BFIN_BUILTIN_DIFFLH_2X16,

3889:

3890: BFIN_BUILTIN_SSADD_1X32,

3891: BFIN_BUILTIN_SSSUB_1X32,

3892: BFIN_BUILTIN_NORM_1X32,

3893: BFIN_BUILTIN_NEG_1X32,

3894: BFIN_BUILTIN_MIN_1X32,

3895: BFIN_BUILTIN_MAX_1X32,

3896: BFIN_BUILTIN_MULT_1X32,

3897:

3898: BFIN_BUILTIN_MULHISILL,

3899: BFIN_BUILTIN_MULHISILH,

3900: BFIN_BUILTIN_MULHISIHL,

3901: BFIN_BUILTIN_MULHISIHH,

3902:

3903: BFIN_BUILTIN_LSHIFT_1X16,

3904: BFIN_BUILTIN_LSHIFT_2X16,

3905: BFIN_BUILTIN_SSASHIFT_1X16,

3906: BFIN_BUILTIN_SSASHIFT_2X16,

3907:

3908: BFIN_BUILTIN_CPLX_MUL_16,

3909: BFIN_BUILTIN_CPLX_MAC_16,

3910: BFIN_BUILTIN_CPLX_MSU_16,

3911:

3912: BFIN_BUILTIN_MAX

3913: };

do you mean that the symbol "BFIN_BUILTIN_MULT_1X32" tell the gcc to expand this function( __builtin_bfin_mult_fr1x32()) into assembly code by some optimizations,but  in fact ,this is no the implement of this function is gcc codes ?

QuoteReplyEditDelete

2009-01-14 05:49:22     Re: Where can I find the implement of Blackfin GCC Built-in Functions

haiping zeng (CHINA)

Message: 67931   

Hi,there is no body know it?

it don't matter, Any advices is welcome.

QuoteReplyEditDelete

2009-01-14 06:07:44     Re: Where can I find the implement of Blackfin GCC Built-in Functions

Mike Frysinger (UNITED STATES)

Message: 67935   

what exactly is your question ?  you wanted to know where the builtin came from and you were told where it can be found.

QuoteReplyEditDelete

2009-01-14 07:28:52     Re: Where can I find the implement of Blackfin GCC Built-in Functions

haiping zeng (CHINA)

Message: 67941   

oh,sorry!

i don't express my question exactly,

what i mean is that i wanted to know where the builtin came from!

QuoteReplyEditDelete

2009-01-14 11:44:24     Re: Where can I find the implement of Blackfin GCC Built-in Functions

Mike Frysinger (UNITED STATES)

Message: 67943   

and you were told where it came from, so is that the only question you had ?

QuoteReplyEditDelete

2009-01-14 21:40:13     Re: Where can I find the implement of Blackfin GCC Built-in Functions

haiping zeng (CHINA)

Message: 67952   

oh,yes !

where it come from?

For example,i want to find it like this:

__builtin_bfin_add_fr1x32 {

...some codes....

}

or somethings like!

QuoteReplyEditDelete

2009-01-14 21:53:43     Re: Where can I find the implement of Blackfin GCC Built-in Functions

haiping zeng (CHINA)

Message: 67953   

another example:

23 #define __builtin_bfin_max(a,b) ((a)>=(b)?(a):(b))

24 #define __builtin_bfin_min(a,b) ((a)<=(b)?(a):(b))

25 #define __builtin_bfin_lmax(a,b) ((a)>=(b)?(a):(b))

26 #define __builtin_bfin_lmin(a,b) ((a)<=(b)?(a):(b))

27 #define __builtin_bfin_max_fr1x32(a,b) ((a)>=(b)?(a):(b))

28 #define __builtin_bfin_min_fr1x32(a,b) ((a)<=(b)?(a):(b))

QuoteReplyEditDelete

2009-01-14 22:36:30     Re: Where can I find the implement of Blackfin GCC Built-in Functions

Robin Getz (UNITED STATES)

Message: 67954   

Haiping:

It is all in the souce code for gcc. If you don't know how to read it - or don't understand what it is doing - or how it works - that is a different question that "where is it" - Mike already answered that with " look in the gcc source directory.  gcc-*/gcc/config/bfin/ ..."

grep and a little bit sleuthing can go much faster than asking the same question for 2 weeks.

-Robin

QuoteReplyEditDelete

2009-01-15 03:50:35     Re: Where can I find the implement of Blackfin GCC Built-in Functions

haiping zeng (CHINA)

Message: 67961   

Robin:

Thank

Maybe you are right!i shoud not ask this question so many times and should creat a new thread for another

question !but i have found in gcc-*/gcc/config/bfin/ ...,and i cant find what i need.such as :

__builtin_bfin_add_fr1x32,why i want to find it ?

because i want to know how it works.  Maybe this  is another question!

QuoteReplyEditDelete

2009-01-15 07:54:30     Re: Where can I find the implement of Blackfin GCC Built-in Functions

Robin Getz (UNITED STATES)

Message: 67982   

Haiping:

Everything you need is between the toolchain source, and grep.

A trivial example: - find out where the built-in csync comes from:

rgetz@imhotep:~/blackfin/trunk/toolchain/gcc-4.3/gcc/config/bfin> grep builtin_bfin_csync *

bfin.c:  def_builtin ("__builtin_bfin_csync", void_ftype_void, BFIN_BUILTIN_CSYNC);

rgetz@imhotep:~/blackfin/trunk/toolchain/gcc-4.3/gcc/config/bfin> grep BFIN_BUILTIN_CSYNC *

bfin.c:  BFIN_BUILTIN_CSYNC,

bfin.c:  def_builtin ("__builtin_bfin_csync", void_ftype_void, BFIN_BUILTIN_CSYNC);

bfin.c:    case BFIN_BUILTIN_CSYNC:

bfin_expand_builtin (tree exp, rtx target ATTRIBUTE_UNUSED,

                     rtx subtarget ATTRIBUTE_UNUSED,

                     enum machine_mode mode ATTRIBUTE_UNUSED,

                     int ignore ATTRIBUTE_UNUSED)

{

  switch (fcode)

    {

    case BFIN_BUILTIN_CSYNC:

      emit_insn (gen_csync ());

And there you go -

It is a similar for all.

For many built-ins -- the build in is not written in Blackfin assembly, but in RLT (so the compiler can do a better job in the optimizations.) for example:

    case BFIN_BUILTIN_DIFFHL_2X16:

    case BFIN_BUILTIN_DIFFLH_2X16:

    case BFIN_BUILTIN_SUM_2X16:

      arg0 = CALL_EXPR_ARG (exp, 0);

      op0 = expand_expr (arg0, NULL_RTX, VOIDmode, 0);

      icode = (fcode == BFIN_BUILTIN_DIFFHL_2X16 ? CODE_FOR_subhilov2hi3

               : fcode == BFIN_BUILTIN_DIFFLH_2X16 ? CODE_FOR_sublohiv2hi3

               : CODE_FOR_ssaddhilov2hi3);

      tmode = insn_data[icode].operand[0].mode;

      mode0 = insn_data[icode].operand[1].mode;

      if (! target

          || GET_MODE (target) != tmode

          || ! (*insn_data[icode].operand[0].predicate) (target, tmode))

        target = gen_reg_rtx (tmode);

      if (VECTOR_MODE_P (mode0))

        op0 = safe_vector_operand (op0, mode0);

      if (! (*insn_data[icode].operand[1].predicate) (op0, mode0))

        op0 = copy_to_mode_reg (mode0, op0);

      pat = GEN_FCN (icode) (target, op0, op0);

      if (! pat)

        return 0;

      emit_insn (pat);

      return target;

If you need help figuring that out - then it is time to buy a book on gcc.

-Robin

QuoteReplyEditDelete

2009-01-15 19:53:00     Re: Where can I find the implement of Blackfin GCC Built-in Functions

haiping zeng (CHINA)

Message: 68003   

Robin

Thanks  a lots!

I got it.

"For many built-ins -- the build in is not written in Blackfin assembly, but in RLT (so the compiler can do a better job in the optimizations.)"--this is the answer i need!

becuace i think that the build in was  written in Blackfin assembly at first,so i find anywhere and can not find anything!

  • Created
Was this helpful?

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.