2008-12-30 01:55:33     issue with getting Kernel information

2008-12-30 01:55:33     issue with getting Kernel information

P SENTHIL KUMAR (INDIA)

Message: 67173   

Dear all,

I am using 2008R1.5 release and configured the kernel for BF561. I had done the baud rate configuration as 11520 and used to view the kernel information using the same baud rate in teraterm window.

While booting of uImage, i am not able to get the kernel informations like memory map details and cache information.

Initial part of kernel information are displayed as corrupted one and other portion are displayed properly.

below are information, i am getting while booting of my uimage

ÿà˜†žøžf~f†øæøfžþžøžxø†x†xø†˜ø˜ž˜`†˜æ†˜f†fàžæàææ†x†žøžæ††~øž†æøfxøž`ž†žàžfž`~xf††~æàæà~f†øæøfžþžøžø†††`†˜˜ø†~øž††††˜

`x~˜æžøž`fæàx†˜à˜ø~x˜˜æ˜æ˜fx˜˜€ff†øž††øfžøž`ææ˜††ž†àžfx˜žøž˜†f†øž†æf€†`ff†ø~˜˜€€˜†øx~f†øfxffæàfx˜æà~†žxfx˜€†ž`˜†ž†àžfx怘€~f

€†ø†ž†žøž~†~ž†žæž†ž`fžøž~˜žfxæžþžf~þž˜†€xffx~þžž†øx~f†øfx˜€†žþžæžž†˜æxx˜x怘€žæàææ†x†žøž˜øf~æž~†f†x憘˜†žžþž~`f†~†žfx†˜†ž††æ

€˜€æžæžfžàžfxxþž˜`ffž€†`f˜fxx†˜˜€žæàææ†x†žøž˜†žøžf˜øf~æž~àfž`~†~þ†þ†žæàææ†x†žøžø†fæàž†žøžf††þžæxþ†æ€˜€føæžfxæøæž˜˜fxfx˜˜æ˜˜˜

˜àæžfx˜àžþžææ˜€†ž`˜à˜˜˜˜˜fæø~ffž˜€žþžææf€˜€æž†øx˜fxæžþžf†~`˜†€f€˜€ž˜f†ø†žfž˜f†žæxfx˜fxæžþžf†~`˜†€f€˜€æ˜ffžþžf˜žf†~怘€~f~˜þx

˜žxx†x~x˜˜€øæž`f~˜þ˜x˜ž˜xxf€˜˜€x~˜þ˜x`˜ž˜xfx˜˜€˜ø~æàææ˜þ˜x`˜ž˜x`x˜˜€˜˜†ž†ž`˜þ˜xfx˜ž`˜˜€àæøæø˜þ`˜žfà†àf€˜€˜€†~fžàž†àžf˜þfà†àf

†˜x†xx˜˜€`æ˜žæžøžf˜þ˜xx˜ž˜˜€ø˜þ˜æ˜ff†~˜øfx`~†žøž~˜æ˜àž~†àžfæøxþž˜xàžþžfž˜€æàæàfxæøf€˜€†˜øž~f~~†žþžøž˜€fæàžf˜†ž†àžfx怘€`f~˜€

fæàžf˜†ž†àžfx†~†øfž`fxæ†`žæžfæx€ž††æ€˜€f~†žàž`˜àþæžøžfž†ž~††fþž`fžfæxfæø†~˜à˜æx`˜˜€ž˜f†ø†žfž˜àæžæžæž†ž`ž†žøžf†~øæžþž`f˜†`fxx

æ†æž`xžþžææøæ~˜†f†øž††øfžøž`ææf˜øfxfžžà†ff†ø~†˜à˜æx˜àæžøžæžàžff~`f†€†`†˜à˜æx˜˜€æžøžxfž~f~fžøž~€žæàææ†x†žøžføfžþžfž`f`fžxfxøž

˜†ž`fx†øf~~f€˜€f`žæøž~†àžf˜††ž`†øfžfæø†~xf†þžxf†ø†~†˜àx`àf~fæøf†æh½¹Í½±•handover: boot [early_BFuart0] -> real [ttyBF0]

Dentry cache hash table entries: 8192 (order: 3, 32768 bytes)

Inode-cache hash table entries: 4096 (order: 2, 16384 bytes)

Memory available: 54348k/65536k RAM, (3024k init code, 1021k kernel code, 417k data, 1024k dma, 5704k reserved)

Blackfin Scratchpad data SRAM: 4 KB

Blackfin Data A SRAM: 16 KB (2 KB free)

Blackfin Data B SRAM: 16 KB (16 KB free)

Blackfin Instruction SRAM: 16 KB (5 KB free)

Mount-cache hash table entries: 512

NET: Registered protocol family 16

Blackfin GPIO Controller

if i set the baud rate as 57600, i can able view the initial kernel informations like memory map and cache deatils, but the other portion the information are displayed as corrupted one. Also i cant able get root prompt for further execution of the application.

below are kernel information, i had got while setting the baud rate 57600

Linux version 2.6.22.19-ADI-2008R1.5blackfin-svn (psenthil@mdtv) (gcc v

ersion 4.1.2 (ADI svn)) #327 Mon Dec 29 19:22:56 IST 2008

early printk enabled on early_BFuart0

Hardware Trace Active and Enabled

Warning: limiting memory to 60MB due to hardware anomaly 05000263

Blackfin support (C) 2004-2007 Analog Devices, Inc.

Compiled for ADSP-BF561 Rev 0.3

Blackfin Linux support by http://blackfin.uclinux.org/

Processor Speed: 500 MHz core clock and 100 MHz System Clock

Board Memory: 64MB

Kernel Managed Memory: 64MB

Memory map:

  text      = 0x00200000-0x002ff7d0

  rodata    = 0x00300000-0x0033fe48

  data      = 0x00340000-0x00352000

    stack   = 0x00340000-0x00342000

  init      = 0x00352000-0x00646000

  bss       = 0x00646000-0x0065bb4c

  available = 0x0065bb4c-0x03bff000

  DMA Zone  = 0x03f00000-0x04000000

NOMPU: setting up cplb tables for global access

Instruction Cache Enabled

Data Cache Enabled (write-through)

Built 1 zonelists.  Total pages: 15240

Kernel command line: root=/dev/mtdblock0 rw earlyprintk=serial,uart0,115200 console=ttyBF0,115200

Configuring Blackfin Priority Driven Interrupts

PID hash table entries: 256 (order: 8, 1024 bytes)M–Ý{Xz~œŒØaºú˜ž³

k‹-‹x=Ò=Ø|pÞ<¸L³Í^âa                                              YØïÃÓ&½íߘÎ1Ø|pÎ<¨VóÍ^›5KK

      Ýû7KÊzò%Ï

               o˘yXN›œ>oIɘòÓ[Xh~&ge  IÉPËR

                                             퐸›z:

                                                   ¬œ>KžŸÌÖ     (°"›h˜<ˆþeSÙ€›X

                                                                                mÉͼ›

ÉP¾ÇŽ<9:ª7'6Ÿ“xŸX                                                                    —.{8¸<œX

ÍÚ³üÙyÍ8x¹Ÿ‚Öù“ªü½OÌÚïmÒyÛ>[Xy\l±6;ð

                                       ÃÞ|L›¬Êþµ½í¿Íó¾'óŸ¨ù˜»þ<¸½OÈÒëi[˜|~yžÝLáËßC“

                                                                                        Ÿ¬ÂÒù“¢%ÍRegisteredò%-   oIÜ»|øúg>7k

ÐÂÉžyŸHn

        ¾RegisteredÍ

           /X_jŒóZˆòzxÚ>»JϽMXZNˆîúŸ%“ŸêÊZlŸHêe:[˜jœ¯Hn

                                                           Ÿ¾¿È¼ëâáίݿßÛˆI     ¨Ðt“i   «

                                                                                         iIZØRegistered>ÎûK|ý¿¿

                                                                                                      ;åòÒ±Û{xúzÒËãòsz¹||xÈ

[ú{ŠøÍîòói

                >*û*z˜ÒÛ÷ÛšüÜ]/þå

                                  ñ€qM8º<ZX°<y¾ú\]

œ¯¿hð                                           øçE%s0¾>\[¸?z½úZL±>>z8_}0~~žŸ¾0~\Ú[>'ÅYâ÷ú|p>XXÎóÞx:Z[œ½óŸ½*~òÂ7s~y½

       !‹ó¬Registeredû{‰ŸÒæÒ!yxßœ

                         ½&žÛè?7žˆŸ>g“âÃ>~~8:~Ê!’       ¾¬

                                                          ò·y˜RegisteredJO

žÌ‚{œÞžÚ±{“a;¼.MÈ{‰!µJdJ”ÞH                                      žÞ|X˜‚ށžRegisteredù&ùÓ÷Ëœ[²9'K³¦7ÿ   +I~9>|ν½

Let me know your suggestion to resolve this display issue.

Regards,Senthil

QuoteReplyEditDelete

2008-12-30 04:05:58     Re: issue with getting Kernel information

Mike Frysinger (UNITED STATES)

Message: 67180   

post your exact kernel .config in use as an attachment

QuoteReplyEditDelete

2008-12-30 06:09:40     Re: issue with getting Kernel information

P SENTHIL KUMAR (INDIA)

Message: 67202   

Hi Mike,

Thanks for the reply.

Actually there is no problem with these uImage, since our standalone project are working with this uImage.

The only problem is we cant able to see the kernel details like memory map and cache.

I had attached the .config files build during this uImage.

Regards,Senthil

config

Attachments:
  • Created
Was this helpful?

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.