2008-12-29 22:05:36     about tftp on uclinux

2008-12-29 22:05:36     about tftp on uclinux

chen shevchenko (CHINA)

Message: 67165   

my board net ic is dm9000   cpu is bf548

on uboot ,use tftp download uImage ok, and boot this kernel.

on uclinux,

use " ping hostip "is ok;

but i use "tftp hostip" ,run this command ,

then use

tftp> get uImage

Received 4355087 bytes in 9.2 seconds

but i use "quit ",

tftp> quit

?Invalid command

QuoteReplyEditDelete

2008-12-29 22:17:48     Re: about tftp on uclinux

Mike Frysinger (UNITED STATES)

Message: 67166   

so use a different command like "q" or "exit" or just CTRL+C

QuoteReplyEditDelete

2008-12-29 22:24:48     Re: about tftp on uclinux

chen shevchenko (CHINA)

Message: 67168   

i test other comand ,like exit ,ctrl+c.

find this thing,

when i after run "tftp hostip",i run any comand like "a"or "b" or other availability command .

after  this command is run,

the next you input any comand ,the system print eroor is all "?Invalid command".

QuoteReplyEditDelete

2009-05-08 17:18:41     Re: about tftp on uclinux

Jay Ku (UNITED STATES)

Message: 73902   

I'm also having this problem with tftp... when I run it, the first command is processed normally but then anything else I enter get me a '?Invalid command' response.  Ctrl-C doesn't even work (but Ctrl-D will kill it).  If I run 'tftp' and then just enter a blank line, I get 'NULL pointer access (probably)' and the program crashes.  I'm using the 2008R1.5-RC3 distribution of uClinux.  'tftp 192.168.1.5 file' works, but I think it's doing the transfers in ASCII mode.

I wonder if there's something strange with the I/O on my system... I also have a problem with 'more'... when it pauses after each page, I have to enter space + Enter to get to the next page (not just space like it should be).  My busybox is 1.4.1.

  • Created
Was this helpful?

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.