2008-11-24 23:48:51     Linux Driverm for AD7147 capsense

2008-11-24 23:48:51     Linux Driverm for AD7147 capsense

deepthi kiran (INDIA)

Message: 65771   

HI,

  Iam working on BF526 EZkit with LCD Ezkit extender, I searched for AD7147 driver in uClinux, but I dint found the one, driver is not ther in SVN trunk also, so Iam planning to take AD7142 as the refrence driver and to bring up AD7147 drver, but in AD7142 driver we have code only for push button part, not for  scroll wheel part, we need scrool wheel part also in the driver for our project purpose, So do we have any scroll wheel refernce driver in linux or in VDSP to continue my work.

Thanks and Regards

Deepthi

QuoteReplyEditDelete

2008-11-25 19:46:11     Re: Linux Driverm for AD7147 capsense

Robin Getz (UNITED STATES)

Message: 65806   

Deepthi:

I think someone has a driver close to done - it is just not yet committed.

When do you need it?

-Robin

QuoteReplyEditDelete

2008-11-25 22:49:16     Re: Linux Driverm for AD7147 capsense

deepthi kiran (INDIA)

Message: 65808   

Thanks Robin, Even I did coding for AD7147 by taking 7142 as the referance, but it has only push button part, I need scroll part also by the end of this week end to continue my work

QuoteReplyEditDelete

2008-12-13 08:47:49     Re: Linux Driverm for AD7147 capsense

Peps River (SWEDEN)

Message: 66692   

Robin: Do you now of any updates on AD7147 driver?

I haven't seen any patches anywhere for a driver for that chip...

QuoteReplyEditDelete

2009-07-15 01:01:33     Re: Linux Driverm for AD7147 capsense

Barry Song (CHINA)

Message: 77284   

Yes. AD7142 driver didn't support non-button event yet. And AD7147 is still under-developping.

For how to process non-button events, you can take

AN-925 Sensors for the AD7147 and AD7148 CapTouch Controllers

http://www.analog.com/static/imported-files/application_notes/AN-925.pdf

as refrence.

QuoteReplyEditDelete

2009-07-22 04:22:38     Re: Linux Driverm for AD7147 capsense

Barry Song (CHINA)

Message: 77854   

deepthi,

I have checked in the new ad7147 driver into trunk head of blackfin uclinux kernel project. The driver supports both button and non-button events. You can take it as a refrence.

-Barry

  • Created
Was this helpful?

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.