2008-11-20 07:24:36     How does module relocation work

2008-11-20 07:24:36     How does module relocation work

Michael McTernan (UNITED KINGDOM)

Message: 65591   

I've got a problem with a module which crashes on load.  Hacking around with the stack back tracing got me some nice traces, and I can see it going wrong at a CALL instruction.  This is with MPU protection on, and it seems to reliably fail in a function named ipnet_init:

(gdb) disassemble ipnet_init

Dump of assembler code for function ipnet_init:

0x00c46388 <ipnet_init+0>:      [--SP] = (R7:7, P5:5);

0x00c4638a <ipnet_init+2>:      LINK 0x20;              /* (32) */

0x00c4638e <ipnet_init+6>:      R0 = 0x6704 (X);                /*              R0=0x0x6704 <module_frob_arch_sections+160>(26372) */

0x00c46392 <ipnet_init+10>:     [FP -0x4] = R0;

0x00c46394 <ipnet_init+12>:     P2.H = 0xc9;            /* (201)        P2=0x0xc90000 <_end+7971516> */

0x00c46398 <ipnet_init+16>:     P2.L = 0x1f28;          /* (7976)       P2=0x0xc91f28 <ipnet_conf_max_sockets> */

0x00c4639c <ipnet_init+20>:     R0 = [P2];

0x00c4639e <ipnet_init+22>:     R1 = 0x1 (X);           /*              R1=0x1(  1) */

0x00c463a0 <ipnet_init+24>:     R1 <<= 0x14;

0x00c463a2 <ipnet_init+26>:     CC = R0 <= R1;

0x00c463a4 <ipnet_init+28>:     IF CC JUMP 0x0xc463ae <ipnet_init+38>;

0x00c463a6 <ipnet_init+30>:     R0 = -0x3eb (X);                /*              R0=0x0xfffffc15(-1003) */

0x00c463aa <ipnet_init+34>:     [FP -0x10] = R0;

0x00c463ac <ipnet_init+36>:     JUMP.S 0x0xc467b8 <ipnet_init+1072>;

0x00c463ae <ipnet_init+38>:     P2.H = 0xc9;            /* (201)        P2=0x0xc91f28 <ipnet_conf_max_sockets> */

0x00c463b2 <ipnet_init+42>:     P2.L = 0x1f28;          /* (7976)       P2=0x0xc91f28 <ipnet_conf_max_sockets> */

0x00c463b6 <ipnet_init+46>:     R0 = [P2];

0x00c463b8 <ipnet_init+48>:     R1 = R0 << 0x2;

0x00c463bc <ipnet_init+52>:     R0 = [FP -0x4];

0x00c463be <ipnet_init+54>:     R0 = R0 + R1;

0x00c463c0 <ipnet_init+56>:     [FP -0x4] = R0;

0x00c463c2 <ipnet_init+58>:     P2.H = 0xcb;            /* (203)        P2=0x0xcb1f28 <ipcom_lkm_sys_net_ipv4_neigh_default+76> */

---Type <return> to continue, or q <return> to quit---

0x00c463c6 <ipnet_init+62>:     P2.L = 0x4b4;           /* (1204)       P2=0x0xcb04b4 <ipnet_conf_cache_bufsiz> */

0x00c463ca <ipnet_init+66>:     R0 = W[P2] (X);

0x00c463cc <ipnet_init+68>:     R1 = R0.L (Z);

0x00c463ce <ipnet_init+70>:     R0 = [FP -0x4];

0x00c463d0 <ipnet_init+72>:     CALL 0x0x1a02060;

I hacked module.c to print the sections during module load:

-s .text 0xc00000 \

-s .init.text 0x7dce030 \

-s .rodata 0xc88678 \

-s .rodata.str1.4 0xc9c6ec \

-s __ksymtab_strings 0xc9cee0 \

-s __ksymtab 0xc9cf7c \

-s .data 0xcb01d0 \

-s .gnu.linkonce.this_module 0xcb20a0 \

-s .bss 0xcb2220 \

-s .symtab 0xc9cfbc \

-s .strtab 0xca4c8c \

So final CALL looks to be to a crazy address, and the crash trace confirms this as causing the problem with the last jump being from ipnet_init+72 and the PC ending up at 0x1a02060:

Undefined instruction

- May be used to emulate instructions that are not defined for

   a particular processor implementation.

Kernel OOPS in progress

Defered Exception context

CURRENT PROCESS:

COMM=insmod PID=31

TEXT = 0x07980040-0x079c5c00        DATA = 0x079c5c04-0x079d2704

BSS = 0x079d2704-0x079d87d4  USER-STACK = 0x079dff74

return address: [0x01a02060]; contents of:

0x01a02040:  3fff  ffff  ffff  ffff  ffff  bfff  ffb7  bfff

0x01a02050:  feff  ffff  ffff  ffff  ffaf  ffff  ffff  9f7f

0x01a02060: [ffbf] ffff  fffe  eff7  ffff  fff7  7fbf  e7ff

0x01a02070:  ffdf  ffff  fdff  ffff  f7f7  f7bf  bfff  fbff

SEQUENCER STATUS:               Tainted: P

SEQSTAT: 00000021  IPEND: 8030  SYSCFG: 0006

  EXCAUSE   : 0x21

  physical IVG15 asserted : <0xffa01288> /* unknown address */

  logical irq   6 mapped  : <0xffa0037c> /* unknown address */

  logical irq  18 mapped  : <0x000a5dc4> { _bfin_serial_rx_int + 0x0 }

  logical irq  19 mapped  : <0x000a5ff8> { _bfin_serial_tx_int + 0x0 }

  logical irq  24 mapped  : <0x000ae360> { _bf537mac_interrupt + 0x0 }

RETE: <0x00000000> /* Maybe null pointer? */

RETN: <0x00bf9da4> /* unknown address */

RETX: <0x01a02060> /* unknown address */

RETS: <0x00c463d4> { :ipnet:_ipnet_init + 0x4c }

PC  : <0x01a02060> /* unknown address */

DCPLB_FAULT_ADDR: <0x00bf9968> /* unknown address */

ICPLB_FAULT_ADDR: <0x00092ef4> { _sprintf + 0x0 }

PROCESSOR STATE:

R0 : 00007704    R1 : 00000020    R2 : 06052340    R3 : 00000000

R4 : 07ba0b18    R5 : 00000015    R6 : 00bcb2d0    R7 : 00cb20a0

P0 : 00bf8000    P1 : 00bf8000    P2 : 00cb04b4    P3 : 00cb20a0

P4 : 00bcb0e0    P5 : 00bcb2a4    FP : 00bf9dc4    SP : 00bf9cc8

LB0: ffa01e10    LT0: ffa01e10    LC0: 00000000

LB1: 00092d2c    LT1: 00092d22    LC1: 00000000

B0 : 00000000    L0 : 00000000    M0 : 00000000    I0 : 00136880

B1 : 00000000    L1 : 00000000    M1 : 00000000    I1 : 00000000

B2 : 00000000    L2 : 00000000    M2 : 00000000    I2 : fffc39ed

B3 : 00000000    L3 : 00000000    M3 : 00000000    I3 : 00000000

A0.w: 00000000   A0.x: 00000000   A1.w: 00000000   A1.x: 00000000

USP : 079dfe84  ASTAT: 02002060

Hardware Trace:

   0 Target : <0xffa00c2c> /* unknown address */

     Source : <0xffa0090c> /* unknown address */

   1 Target : <0xffa00c2c> /* unknown address */  <- trap

     Source : <0x00c463d0> { :ipnet:_ipnet_init + 0x48 }

   2 Target : <0x00c463ca> { :ipnet:_ipnet_init + 0x42 }

     Source : <0xffa0090c> /* unknown address */

   3 Target : <0xffa00c2c> /* unknown address */

     Source : <0x00c463c6> { :ipnet:_ipnet_init + 0x3e }

   4 Target : <0x00c463ae> { :ipnet:_ipnet_init + 0x26 }

     Source : <0x00c463a4> { :ipnet:_ipnet_init + 0x1c }

   5 Target : <0x00c4639c> { :ipnet:_ipnet_init + 0x14 }

     Source : <0xffa0090c> /* unknown address */

   6 Target : <0xffa00c2c> /* unknown address */

     Source : <0x00c46398> { :ipnet:_ipnet_init + 0x10 }

   7 Target : <0x00c46388> { :ipnet:_ipnet_init + 0x0 }

So I loaded the module debug file into bfin-uclinux-gdb on my PC  to have a look at the same function prior:

(gdb) disassemble ipnet_init

Dump of assembler code for function ipnet_init:

0x00046388 <ipnet_init+0>:      [--SP] = (R7:7, P5:5);

0x0004638a <ipnet_init+2>:      LINK 0x20;              /* (32) */

0x0004638e <ipnet_init+6>:      R0 = 0x6704 (X);                /*             R0=0x0x6704 <CAST_set_key+3320>(26372) */

0x00046392 <ipnet_init+10>:     [FP -0x4] = R0;

0x00046394 <ipnet_init+12>:     P2.H = 0x0;             /* (  0)        P2=0x0x0 <buf.1956> */

0x00046398 <ipnet_init+16>:     P2.L = 0x0;             /* (  0)        P2=0x0x0 <buf.1956> */

0x0004639c <ipnet_init+20>:     R0 = [P2];

0x0004639e <ipnet_init+22>:     R1 = 0x1 (X);           /*              R1=0x1(  1) */

0x000463a0 <ipnet_init+24>:     R1 <<= 0x14;

0x000463a2 <ipnet_init+26>:     CC = R0 <= R1;

0x000463a4 <ipnet_init+28>:     IF CC JUMP 0x0x463ae <ipnet_init+38>;

0x000463a6 <ipnet_init+30>:     R0 = -0x3eb (X);                /*             R0=0x0xfffffc15(-1003) */

0x000463aa <ipnet_init+34>:     [FP -0x10] = R0;

0x000463ac <ipnet_init+36>:     JUMP.S 0x0x467b8 <ipnet_init+1072>;

0x000463ae <ipnet_init+38>:     P2.H = 0x0;             /* (  0)        P2=0x0x0 <buf.1956> */

0x000463b2 <ipnet_init+42>:     P2.L = 0x0;             /* (  0)        P2=0x0x0---Type <return> to continue, or q <return> to quit---

<buf.1956> */

0x000463b6 <ipnet_init+46>:     R0 = [P2];

0x000463b8 <ipnet_init+48>:     R1 = R0 << 0x2;

0x000463bc <ipnet_init+52>:     R0 = [FP -0x4];

0x000463be <ipnet_init+54>:     R0 = R0 + R1;

0x000463c0 <ipnet_init+56>:     [FP -0x4] = R0;

0x000463c2 <ipnet_init+58>:     P2.H = 0x0;             /* (  0)        P2=0x0x0 <buf.1956> */

0x000463c6 <ipnet_init+62>:     P2.L = 0x0;             /* (  0)        P2=0x0x0 <buf.1956> */

0x000463ca <ipnet_init+66>:     R0 = W[P2] (X);

0x000463cc <ipnet_init+68>:     R1 = R0.L (Z);

0x000463ce <ipnet_init+70>:     R0 = [FP -0x4];

0x000463d0 <ipnet_init+72>:     CALL 0x0x45bd0 <ipnet_kioevent_softirq>;

Here the function looks okay and the call is to the correct unre-located address.  So I'm wondering how after module loading the CALL instruction got the wrong address.  I'm thinking that relocation must have changed the instruction, but incorrectly, pointing to either a bug in the toolchain, compiler, or quite possibly the way the module is built.

Unfortunately the module is alien and uses it's own build process, but I added the following to it's build:

CFLAGS="-mno-fdpic -mcpu=bf537-0.3 -fno-omit-frame-pointer -fno-optimize-sibling-calls -fno-common"

Still no luck.  Do I need more?

I also tried enabling the pr_debug lines in apply_relocate_add(), as this is the relocation function that is being called as opposed to apply_relocate().  I get a lot of output, but don't really understand it e.g.

location is cb1514, value is c84654 type is 18

before b90 after c84654

Is location the instruction to be patched?  If so, I would expect to see a line patching the CALL at 0xc463d0 - but I don't, maybe the bug, but then I don't know how the address in the CALL statement changed from that observed in gdb on PC to after module load. 

Note, there are a bunch of CALL instructions going to this address, so I don't think this is a single corruption of the instruction memory - it's more systematic than that.

So... is there any good info on how Blackfin relocation works, or Linux relocation in general if Blackfin isn't very different?  Am I right that it patches the individual instructions and as such will have modified the CALL statement I'm seeing?

Any help gratefully received.

QuoteReplyEditDelete

2008-11-20 08:11:27     Re: How does module relocation work

Bernd Schmidt (GERMANY)

Message: 65597   

As a shot in the dark, does the appended patch help?

module-cache.diff

QuoteReplyEditDelete

2008-11-20 08:35:54     Re: How does module relocation work

Michael McTernan (UNITED KINGDOM)

Message: 65602   

I'm getting a "File not found" when trying to download the patch - can you repost?

QuoteReplyEditDelete

2008-11-20 08:37:48     Re: How does module relocation work

Mike Frysinger (UNITED STATES)

Message: 65603   

try again.  files posted do not immediatly show up on the server.

QuoteReplyEditDelete

2008-11-20 09:11:39     Re: How does module relocation work

Michael McTernan (UNITED KINGDOM)

Message: 65608   

Got the patch - looked interesting, but it hasn't changed the behaviour   I may goto write through cache as an experiment though.

I've got a little more debug now too.  The CALL is updated once during relocation, after which the value is set the the incorrect CALL seen in the disassembly.  I found the relevant relocation record with bfin-uclinux-objdump:

000463d2 R_pcrel24         ___umodsi3

The address is the instruction +2, hence why my earlier grep failed.  The application of the relocation produces the following output:

location is c463d2, value is ffa02060 type is 10

value is 7f6dde48, before e3ff-fc00 after e36d-de48

The module is still going in at .text 0xc00000.  I'm just trying to understand this bit of code now to see if it makes sense...

QuoteReplyEditDelete

2008-11-20 09:26:23     Re: How does module relocation work

Bernd Schmidt (GERMANY)

Message: 65609   

00463d2 R_pcrel24         ___umodsi3

That shouldn't happen.  Modules must be compiled with -mlong-calls.

QuoteReplyEditDelete

2008-11-20 09:35:02     Re: How does module relocation work

Michael McTernan (UNITED KINGDOM)

Message: 65611   

Awesome - that does it!  The module's now loaded.

I suspected the alien build environment for this module was dodgy - I already added a bunch of stuff but didn't see the -mlong-calls option first time around.  Thankyou for pointing this out!

Kind Regards, Mike

QuoteReplyEditDelete

2008-11-20 09:35:50     Re: How does module relocation work

Mike Frysinger (UNITED STATES)

Message: 65612   

i wonder if we can detect & reject PCREL relocations to symbols inside of the kernel ...

QuoteReplyEditDelete

2008-11-20 11:39:59     Re: How does module relocation work

Michael McTernan (UNITED KINGDOM)

Message: 65620   

Trapping and rejecting the module would sure be nice if it doesn't add much overhead to module loading...

QuoteReplyEditDelete

2008-11-20 19:49:17     Re: How does module relocation work

Robin Getz (UNITED STATES)

Message: 65640   

Mike:

It's a good idea - Bernd would need to comment on the practicality.

-Robin

Attachments:
  • Created
Was this helpful?

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.