2008-11-07 03:38:07     There may be BUG in bfin_5xx.c DMA mode.

2008-11-07 03:38:07     There may be BUG in bfin_5xx.c DMA mode.

DAVID ZHOU (CHINA)

Message: 64793   

Hi,

There may be some problem with serial driver in DMA mode. My version is 2008R1-RC8 and I have fix bug #4459 and #4460.

And if there is little data to transfer, this problem may not come out, but if you send lot of data continuously to bf536,this problem may happen a lot during the test procedure.

My test case:

      1. send big bin file (maybe more than 200KB )to blackfin through PC  serial port to bf536 uclinux ttyBF1(working in DMA mode).

      2. after get this file in blackfin uclinux then send out through network back to PC

      3. compare these two file and you can find error.

I have check the source code and find it is most problely in

void bfin_serial_rx_dma_timeout(struct bfin_serial_port *uart)

{

... ...

uart->rx_dma_nrows = get_dma_curr_ycount(uart->rx_dma_channel);

x_pos = get_dma_curr_xcount(uart->rx_dma_channel);

... ...

}

and often happens in when value of  uart->rx_dma_nrows  is 7

Could any body check it, thanks !

QuoteReplyEditDelete

2008-11-07 04:32:15     Re: There may be BUG in bfin_5xx.c DMA mode.

Mike Frysinger (UNITED STATES)

Message: 64817   

there has been a bunch of fixes since 2008R1.  you could try the version in the branch or trunk.

QuoteReplyEditDelete

2008-11-07 04:55:39     Re: There may be BUG in bfin_5xx.c DMA mode.

Sonic Zhang (CHINA)

Message: 64818   

A bug has been fixed on 2008R1 branch. Please use the serial source on the branch head.

QuoteReplyEditDelete

2008-11-09 21:04:44     Re: There may be BUG in bfin_5xx.c DMA mode.

DAVID ZHOU (CHINA)

Message: 64893   

Thanks Sonic and Mike,in the trunk version the bug I mentioned have been fixed.

  • Created
Was this helpful?

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.