2008-10-21 10:44:20     Problems with BlueTechnix CM-BF537E

2008-10-21 10:44:20     Problems with BlueTechnix CM-BF537E

Patrick Hotz (GERMANY)

Message: 63992   

Please Help me,

i have big problems with my CM-BF537E on a FireCracker Board...

at the moment there is the BlueSheep bootloader installed

I connect to the board using the minicom terminal software under Debian.

I have connection to the board.

but i can not send the u-boot .hex file to the CM-BF537E...

i have read the FAQ from BlueTechnix but it doesent work..

(http://bluetechnix.at/rainbow2006/site/support/faq/350/faq.aspx)

i start the transfer with "xmr u-boot.hex" ==> that is OK

then i start the file transfer using xmodem config ==> the CM-BF537E Module hangs up and do nothing until i press the reset button...

is there anyone who can help me?

TranslateQuoteReplyEditDelete

2008-10-21 13:51:52     Re: Problems with BlueTechnix CM-BF537E

Mike Frysinger (UNITED STATES)

Message: 63997   

we dont use/know/support the Blue/Black Sheep bootloaders.  you'll have to contact the BlueTechnix guys for assistance.

QuoteReplyEditDelete

2008-10-21 15:45:36     Re: Problems with BlueTechnix CM-BF537E

Robin Getz (UNITED STATES)

Message: 64001   

Patrick:

We don't support the Firecracker board either. As Mike said - ask your place of purchase for support.

-Robin

  • Created
Was this helpful?

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.