2008-10-20 15:33:26     use timer

2008-10-20 15:33:26     use timer

damien OLLIVE (UNITED STATES)

Message: 63952   

I don't understand how use the timer.

I have the driver timer_test.c (http://docs.blackfin.uclinux.org/doku.php?id=linux-kernel:timers), i have added it in the kernel.

But how use it, how use the timer who are setting in this driver they are never launch and i don't understand how launch it.

if you can explain me hox that working thanks

QuoteReplyEditDelete

2008-10-20 16:04:33     Re: use timer

Mike Frysinger (UNITED STATES)

Message: 63953   

assuming you have not modified the example driver, what exactly do you see in the kernel log ?  i just tested it again and it still works fine for me ...

QuoteReplyEditDelete

2008-10-20 16:43:53     Re: use timer

damien OLLIVE (UNITED STATES)

Message: 63954   

sorry for the question which is certanly stupid but how can i see if the modul works fine. i have load and install it but i don't receive any printk from the timer.

(I have load the exemple of the wiki without modification)

thanks

QuoteReplyEditDelete

2008-10-20 16:46:54     Re: use timer

Mike Frysinger (UNITED STATES)

Message: 63955   

if you want to read the kernel log buffer, then you use `dmesg` like normal

QuoteReplyEditDelete

2008-10-20 17:03:57     Re: use timer

damien OLLIVE (UNITED STATES)

Message: 63956   

ok...

thanks that working.

Sorry for the question of beginner, but that explain a lot of my problem.

thanks

  • Created
Was this helpful?

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.