2008-08-11 09:32:57     with sd card on ADSP-BF548 EZ-KIT

2008-08-11 09:32:57     with sd card on ADSP-BF548 EZ-KIT

Jingwei Cheng (CHINA)

Message: 60248   

hello,every one!

I can't config SD card on  ADSP-BF548 EZ-KIT .

Because I can't find /proc/spi_mmc.

How to config?

Thanks!!!

TranslateQuoteReplyEditDelete

2008-08-11 09:44:30     Re: with sd card on ADSP-BF548 EZ-KIT

Mike Frysinger (UNITED STATES)

Message: 60249   

that doesnt really make sense ... the SD card interface on the BF548 is an on-chip peripheral.  it is not a SPI-bitbanging device like the "spi_mmc" driver that is used on BF53x parts.

QuoteReplyEditDelete

2008-08-11 09:51:46     Re: with sd card on ADSP-BF548 EZ-KIT

Jingwei Cheng (CHINA)

Message: 60250   

Thank you Mike,if I want to to use sd card on ADSP-BF548 EZ-KIT,it should be how to configure?

TranslateQuoteReplyEditDelete

2008-08-11 10:19:28     Re: with sd card on ADSP-BF548 EZ-KIT

Mike Frysinger (UNITED STATES)

Message: 60251   

just enable the BF548 SD driver and the MMC block layer, then use /dev/mmcblk* like any other system

QuoteReplyEditDelete

2008-08-11 22:25:43     Re: with sd card on ADSP-BF548 EZ-KIT

Jingwei Cheng (CHINA)

Message: 60265   

mount faile!

My kernel configuration is as follows: Other default.

Linux Kernel Configuration--->

   Device Drivers--->

  <*>MMC/SD card support--->

   --- MMC/SD card support

   []  MMC debugging

   []  Allow unsafe resume (DANGEROUS)

   --- MMC/SD Card Drivers

   <*> MMC/SD block device drivers

   --- MMC/SD Host Controller Drivers

   <M> Blackfin Secure Digital Host support

   []    Blackfin EZkit Rev 1.3 Missing SDH_CMD Pull Up Resistor Workaround

   <>  MMC/SD for SPI support (EXPERIMENTAL)

on target:

root:/dev>

root:/dev>

root:/dev> ls

audio      null       ram7       tty18      tty33      tty49      tty7

console    otp        ram8       tty19      tty34      tty5       tty8

dsp        ptmx       ram9       tty2       tty35      tty50      tty9

fb0        pts        random     tty20      tty36      tty51      ttyBF0

full       ram0       rtc0       tty21      tty37      tty52      urandom

i2c-0      ram1       snd        tty22      tty38      tty53      vcs

kmem       ram10      tty        tty23      tty39      tty54      vcs1

kmsg       ram11      tty0       tty24      tty4       tty55      vcsa

log        ram12      tty1       tty25      tty40      tty56      vcsa1

mem        ram13      tty10      tty26      tty41      tty57      watchdog

mixer      ram14      tty11      tty27      tty42      tty58      zero

mtd0       ram15      tty12      tty28      tty43      tty59

mtd0ro     ram2       tty13      tty29      tty44      tty6

mtd1       ram3       tty14      tty3       tty45      tty60

mtd1ro     ram4       tty15      tty30      tty46      tty61

mtdblock0  ram5       tty16      tty31      tty47      tty62

mtdblock1  ram6       tty17      tty32      tty48      tty63

root:/dev> mount -t vfat -o sync /dev/mmcblock0 /mnt/mmc

mount: mounting /dev/mmcblock0 on /mnt/mmc failed

root:/dev>

root:/dev>

root:/dev>

root:/dev>

TranslateQuoteReplyEditDelete

2008-08-12 21:51:21     Re: with sd card on ADSP-BF548 EZ-KIT

Mike Frysinger (UNITED STATES)

Message: 60355   

clearly if /dev/mmcblock0 doesnt exist, then it isnt going to work.  trying to run commands isnt going to change that.

mmcblock is like any other block device.  you have to debug it one step at a time to figure out what is failing.  start with the kernel boot output to see what the driver has to say about the driver and any cards.

QuoteReplyEditDelete

2008-08-12 22:26:34     Re: with sd card on ADSP-BF548 EZ-KIT

Cliff Cai (CHINA)

Message: 60356   

Hi Jingwei,

I think you should configure a built-in  sdh driver and choose the workaround ,just  as following:

<*> Blackfin Secure Digital Host support

   [*]    Blackfin EZkit Rev 1.3 Missing SDH_CMD Pull Up Resistor Workaround

Cliff

QuoteReplyEditDelete

2008-08-13 03:43:10     回复: Re: with sd card on ADSP-BF548 EZ-KIT

Jingwei Cheng (CHINA)

Message: 60366   

all kernel config is default.

I use the nandflash, will have an impact??

Cliff,I config the host,buf can't find /dev/mmc,can't mount,can't find sd card.

Thanks.

TranslateQuoteReplyEditDelete

2008-08-13 04:04:11     Re: 回复: Re: with sd card on ADSP-BF548 EZ-KIT

Cliff Cai (CHINA)

Message: 60367   

You can  run: ./build_sdiommc_kernel.exp BF548-EZKIT (under testsuites/sdiommc/)

to generate the config file for SD/MMC .

Cliff

QuoteReplyEditDelete

2008-08-13 09:59:17     回复: Re: 回复: Re: with sd card on ADSP-BF548 EZ-KIT

Jingwei Cheng (CHINA)

Message: 60401   

what's mean?

run: ./build_sdiommc_kernel.exp BF548-EZKIT (under testsuites/sdiommc/)

I don't understand,Cliff.

  • Created
Was this helpful?

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.