2008-06-16 04:22:25     what's the difference between ITU-R BT.656 and UYVY422

2008-06-16 04:22:25     what's the difference between ITU-R BT.656 and UYVY422

Matthew Wang (CHINA)

Message: 57333   

what's the difference between ITU-R BT.656 and UYVY422?

I have read the ITU-R BT.656 standard, and in ITU-R BT.656 fomat , there are some control words and UYVY422,

So, If I could understand that ITU-R BT.656 format is equal to UYVY422 format?

The data from CMOS camera sensor will be transformed to ITU-R BT.656 with TVP5150AM1, then they will be dealed with Video for Linux driver as a result of v4l.yuv. So, if there is some difference between ITU-R BT.656 and UYVY422, then we have to transform ITU-R BT.656 to UYVY422 in v4l driver, don't we ?

TranslateQuoteReplyEditDelete

2008-06-16 10:39:16     Re: what's the difference between ITU-R BT.656 and UYVY422

Robin Getz (UNITED STATES)

Message: 57346   

Matthew:

My understanding of the v4l framework is that the applicaiton asks the driver for a specific format (<code class="CONSTANT">VIDIOC_TRY_FMT</code> ioctl) If the driver can support it, it provides it.

http://www.linuxtv.org/downloads/video4linux/API/V4L2_API/spec/c830.htm

It doesn't matter what the camera supports - it matters what the application wants.

QuoteReplyEditDelete

2008-06-17 02:49:01     回复: Re: what's the difference between ITU-R BT.656 and UYVY422

Matthew Wang (CHINA)

Message: 57358   

thank you, Robin

  • Created
Was this helpful?

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.