2008-05-22 14:56:36     pppd help

2008-05-22 14:56:36     pppd help

blue hash (UNITED STATES)

Message: 56157   

I'm unable to connect via pppd betweent the dev machine and blackfin target.

All the steps in the following link were followed:

http://docs.blackfin.uclinux.org/doku.php?id=uclinux-dist:ppp&s[]=pppd

host-ip: 192.168.4.124

blackfin-ip : 192.168.1.10

File /etc/ppp/options contains:

On the blackfin:

lock

nocrtscts

lock

nocrtscts

192.168.1.10:192.168.1.124

linkname ppp0

local

nodefaultroute

/dev/ttyBF0

57600

-detach

On the Host

lock

nocrtscts

192.168.1.124:192.168.1.10

linkname ppp0

local

nodefaultroute

/dev/ttyS0

57600

-detach

When pppd is started on the host:

[root@localhost ~]# pppd

Using interface ppp0

Connect: ppp0 <--> /dev/ttyS0

LCP: timeout sending Config-Requests

Connection terminated.

Modem hangup

When pppd is started on the blackfin:

root:/> pppd

Using interface ppp0

Connect: ppp0 <--> /dev/ttyBF0

Warning - secret file /etc/ppp/pap-secrets has world and/or group access

CCP: timeout sending Config-Requests

IPCP: timeout sending Config-Requests

Connection terminated.

Modem hangup

Thanks.

QuoteReplyEditDelete

2008-05-22 21:16:15     Re: pppd help

Yi Li (CHINA)

Message: 56162   

Are you using 08R1 release or trunk?

QuoteReplyEditDelete

2008-05-23 08:42:57     Re: pppd help

blue hash (UNITED STATES)

Message: 56210   

Its the 08R1 release

Has it been fixed in trunk?

QuoteReplyEditDelete

2008-05-26 00:43:15     Re: pppd help

Yi Li (CHINA)

Message: 56261   

I need to have a try and let you know.

  • Created
Was this helpful?

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.