2008-05-15 13:04:46     Undefined or illegal instruction

2008-05-15 13:04:46     Undefined or illegal instruction

Laurent Winkler (SWITZERLAND)

Message: 55863   

I am trying to compile uclinux for a blackfin processor. Here is one problem I run into.

While running certain scripts (even simple ones with a few 'if's and 'for's) with msh I get an error : see description below.

Some errors may come from the fact that I use vfork() instead of fork() as required by the hardware. I know vfork() should not exit with 'return' on the child process (you should use 'exit' instead).

My questions are :

What exactly should I changes, so that uc-linux uses vfork() ? For now I've just switched vfork() for fork() in portmap.c ?

How does uclinux handle a call to fork(), as found in many other files ?

Do you have any other clue why this error keeps happening ?

------------------the script :

for arg in $* ; do

if [ "$arg" = "2" ]; then

echo deux

fi

if [ "$arg" = "3" ]; then

echo trois

fi

if [ "$arg" = "4" ]; then

echo quatre

fi

done

------------------------- error ---------------------------------

Jan  1 09:23:27 blackfin user.notice kernel: Undefined instruction

Jan  1 09:23:27 blackfin user.notice kernel:  - May be used to emulate instructions that are not defined for

Jan  1 09:23:27 blackfin user.notice kernel:    a particular processor implementation.

Jan  1 09:23:27 blackfin user.notice kernel: Deferred Exception context

Jan  1 09:23:27 blackfin user.notice kernel: CURRENT PROCESS:

Jan  1 09:23:27 blackfin user.notice kernel: COMM=parocrun2 PID=349

Jan  1 09:23:27 blackfin user.notice kernel: TEXT = 0x03100040-0x031494a0        DATA = 0x031494a4-0x0315c494

Jan  1 09:23:27 blackfin user.notice kernel:  BSS = 0x0315c494-0x0315df04  USER-STACK = 0x03167f40

Jan  1 09:23:27 blackfin user.notice kernel:

Jan  1 09:23:27 blackfin user.notice kernel: return address: [0x031271f4]; contents of:

Jan  1 09:23:27 blackfin user.notice kernel: 0x031271d0:  0000  0000  0005  0000  0000  0000  0018  2e04

Jan  1 09:23:27 blackfin user.notice kernel: 0x031271e0:  002e  1007  d015  000e  0000  0000  0006  0000

Jan  1 09:23:27 blackfin user.notice kernel: 0x031271f0:  0000  0000 [0018] 6504  6374  0100  d1b8  000e

Jan  1 09:23:27 blackfin user.notice kernel: 0x03127200:  0000  0000  0007  0000  0000  0000  0018  2e04

Jan  1 09:23:27 blackfin user.notice kernel:

Jan  1 09:23:27 blackfin user.notice kernel: SEQUENCER STATUS:        Not tainted

Jan  1 09:23:27 blackfin user.notice kernel:  SEQSTAT: 00060021  IPEND: 0030  SYSCFG: 0006

Jan  1 09:23:27 blackfin user.notice kernel:   HWERRCAUSE: 0x18

Jan  1 09:23:27 blackfin user.notice kernel:   EXCAUSE   : 0x21

Jan  1 09:23:27 blackfin user.notice kernel:  RETE: <0x00000000> { _run_init_process + 0xfffff000 }

Jan  1 09:23:27 blackfin user.notice kernel:  RETN: <0x004c4000> /* unknown address */

Jan  1 09:23:27 blackfin user.notice kernel:  RETX: <0x031271f4> [ parocrun2 + 0x271b4 ]

Jan  1 09:23:27 blackfin user.notice kernel:  RETS: <0x0312710e> [ parocrun2 + 0x270ce ]

Jan  1 09:23:27 blackfin user.notice kernel:  PC  : <0x031271f4> [ parocrun2 + 0x271b4 ]

Jan  1 09:23:27 blackfin user.notice kernel: D

Jan  1 09:23:27 blackfin user.info kernel: CPLB_FAULT_ADDR: <0x03167be0> [ parocrun2 + 0x67be0 ]

Jan  1 09:23:27 blackfin user.notice kernel: ICPLB_FAULT_ADDR: <0x031271f4> [ parocrun2 + 0x271b4 ]

Jan  1 09:23:27 blackfin user.notice kernel:

Jan  1 09:23:27 blackfin user.notice kernel: PROCESSOR STATE:

Jan  1 09:23:27 blackfin user.notice kernel:  R0 : 00000000    R1 : 00000000    R2 : 00000200    R3 : 40000000

Jan  1 09:23:27 blackfin user.notice kernel:  R4 : 00000000    R5 : 00000001    R6 : 00000000    R7 : 03780394

Jan  1 09:23:27 blackfin user.notice kernel:  P0 : 00000003    P1 : 037817e0    P2 : 0315bf54    P3 : 03167f48

Jan  1 09:23:27 blackfin user.notice kernel:  P4 : 0378059c    P5 : 03780390    FP : 03167c78    SP : 004c3f24

Jan  1 09:23:27 blackfin user.notice kernel:  LB0: 0310cb21    LT0: 0310cb1e    LC0: 00000000

Jan  1 09:23:27 blackfin user.notice kernel:  LB1: 03112b65    LT1: 03112b5e    LC1: 00000000

Jan  1 09:23:27 blackfin user.notice kernel:  B0 : 00000000    L0 : 00000000    M0 : 00000000    I0 : 03167f9d

Jan  1 09:23:27 blackfin user.notice kernel:  B1 : 00000000    L1 : 00000000    M1 : 00000000    I1 : 0068066d

Jan  1 09:23:27 blackfin user.notice kernel:  B2 : 00000000    L2 : 00000000    M2 : 00000000    I2 : 00000000

Jan  1 09:23:27 blackfin user.notice kernel:  B3 : 00000000    L3 : 00000000    M3 : 00000000    I3 : 00000000

Jan  1 09:23:27 blackfin user.notice kernel: A0.w: 00000000   A0.x: 00000000   A1.w: 00000000   A1.x: 00000000

Jan  1 09:23:27 blackfin user.notice kernel: USP : 03167be4  ASTAT: 02003025

Jan  1 09:23:27 blackfin user.notice kernel:

Jan  1 09:23:27 blackfin user.notice kernel: Hardware Trace:

Jan  1 09:23:27 blackfin user.notice kernel:    0 Target : <0x0000464c> { _trap_c + 0x0 }

Jan  1 09:23:27 blackfin user.notice kernel:      Source : <0xffa006c4> { _exception_to_level5 + 0

Jan  1 09:23:27 blackfin user.info kernel: xb4 }

Jan  1 09:23:27 blackfin user.notice kernel:    1 Target : <0xffa00610> { _exception_to_level5 + 0x0 }

Jan  1 09:23:27 blackfin user.notice kernel:      Source : <0xffa0056c> { _ex_trap_c + 0x5c }

Jan  1 09:23:27 blackfin user.notice kernel:    2 Target : <0xffa00510> { _ex_trap_c + 0x0 }

Jan  1 09:23:27 blackfin user.notice kernel:      Source : <0xffa00764> { _trap + 0x28 }

Jan  1 09:23:27 blackfin user.notice kernel:    3 Target : <0xffa0073c> { _trap + 0x0 }

Jan  1 09:23:27 blackfin user.notice kernel:      Source : <0x031271f2> [ parocrun2 + 0x271b2 ]

Jan  1 09:23:27 blackfin user.notice kernel:    4 Target : <0x031271f0> [ parocrun2 + 0x271b0 ]

Jan  1 09:23:27 blackfin user.notice kernel:      Source : <0x03127112> [ parocrun2 + 0x270d2 ]

Jan  1 09:23:27 blackfin user.notice kernel:    5 Target : <0x0312710e> [ parocrun2 + 0x270ce ]

Jan  1 09:23:27 blackfin user.notice kernel:      Source : <0x0311b10e> [ parocrun2 + 0x1b0ce ]

Jan  1 09:23:27 blackfin user.notice kernel:    6 Target : <0x0311b106> [ parocrun2 + 0x1b0c6 ]

Jan  1 09:23:27 blackfin user.notice kernel:      Source : <0x0311b0fc> [ parocrun2 + 0x1b0bc ]

Jan  1 09:23:27 blackfin user.notice kernel:    7 Target : <0x0311b0f8> [ parocrun2 + 0x1b0b8 ]

Jan  1 09:23:27 blackfin user.notice kernel:      Source : <0x03102888> [ parocrun2 + 0x2848 ]

Jan  1 09:23:27 blackfin user.notice kernel:    8 Target : <0x03102876> [ parocrun2 + 0x2836 ]

Jan  1 09:23:27 blackfin user.notice kernel:      Source : <0xffa00c58> { __common_int_entry + 0xd8 }

Jan  1 09:23:27 blackfin user.notice kernel:    9 Target : <0xffa00bf6> { __common_int_entry + 0x76 }

Jan  1 09:23:27 blackfin user.notice kernel:      Source : <0xffa00e1c> { _evt_system_call + 0x64 }

Jan  1 09:23:27 blackfin user.notice kernel:   10 Target : <0xffa00e1c> { _evt_system_

Jan  1 09:23:27 blackfin user.info kernel: call + 0x64 }

Jan  1 09:23:27 blackfin user.notice kernel:      Source : <0xffa008ec> { _system_call + 0xb8 }

Jan  1 09:23:27 blackfin user.notice kernel:   11 Target : <0xffa008e8> { _system_call + 0xb4 }

Jan  1 09:23:27 blackfin user.notice kernel:      Source : <0xffa008d8> { _system_call + 0xa4 }

Jan  1 09:23:27 blackfin user.notice kernel:   12 Target : <0xffa008d2> { _system_call + 0x9e }

Jan  1 09:23:27 blackfin user.notice kernel:      Source : <0xffa008c2> { _system_call + 0x8e }

Jan  1 09:23:27 blackfin user.notice kernel:   13 Target : <0xffa0089c> { _system_call + 0x68 }

Jan  1 09:23:27 blackfin user.notice kernel:      Source : <0x0003c63a> { _sys_read + 0x4e }

Jan  1 09:23:27 blackfin user.notice kernel:   14 Target : <0x0003c61e> { _sys_read + 0x32 }

Jan  1 09:23:27 blackfin user.notice kernel:      Source : <0x0003c29e> { _vfs_read + 0x22 }

Jan  1 09:23:27 blackfin user.notice kernel:   15 Target : <0x0003c296> { _vfs_read + 0x1a }

Jan  1 09:23:27 blackfin user.notice kernel:      Source : <0x0003c2fa> { _vfs_read + 0x7e }

Jan  1 09:23:27 blackfin user.notice kernel: Stack from 004c3f04:

Jan  1 09:23:27 blackfin user.notice kernel:         00000000 ffa006c8 0015dc30 0015dc30 0015dc28 40000000 00000000 03102876

Jan  1 09:23:27 blackfin user.notice kernel:         031271f4 00000030 00060021 00000000 004c4000 031271f4 031271f4 0312710e

Jan  1 09:23:27 blackfin user.notice kernel:         00000000 02003025 03112b65 0310cb21 03112b5e 0310cb1e 00000000 00000000

Jan  1 09:23:27 blackfin user.notice kernel:         00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000

Jan  1 09:23:27 blackfin user.notice kernel:         00000000 00000000 00000000 00000000 00000000 00000000 00000000

Jan  1 09:23:27 blackfin user.info kernel: 00000000

Jan  1 09:23:27 blackfin user.notice kernel:         00000000 00000000 0068066d 03167f9d 03167be4 03167c78 03780390 0378059c

Jan  1 09:23:27 blackfin user.notice kernel:

QuoteReplyEditDelete

2008-05-15 13:26:50     Re: Undefined or illegal instruction

Cameron Barfield (UNITED STATES)

Message: 55864   

This is probably one of the best explanations of fork() vs. vfork() that I've come across:

fork() and vfork(), for those unfamiliar with these system calls, allow a process to split into two processes, a parent and a child. A process can split many times to create multiple children. When a process calls fork(), the child is a duplicate of the parent in all ways, but it shares nothing with the parent and can operate independently, as can the parent. With vfork() this is not the case. First, the parent is suspended and cannot continue executing until the child exits or calls exec(), the system call used to start a new application. The child, directly after returning from vfork(), is running on the parent's stack and is using the parent's memory and data. This means the child can corrupt the data structures or the stack in the parent, resulting in failure. This is avoided by ensuring that the child never returns from the current stack frame once vfork() has been called and that it calls _exit when finishing—exit cannot be called as it changes data structures in the parent. The child also must avoid changing any information in global data structures or variables, as such changes may break the execution of the parent.

Making an application use vfork instead of fork usually falls into the absolutely simple or incredibly difficult category. Generally, if the application does not fork and then exec() almost immediately, it needs to be checked carefully before fork() can be replaced with vfork().

The uClinux flat executable format, though it doesn't directly affect applications and their operations, does allow quite a few options that the usual ELF executables under Linux do not. Flat format executables come in two basic flavors, fully relocated and a variation of position-independent code (PIC). The fully relocated version has relocations for its code and data, while the PIC version generally needs only a few relocations for its data.

http://www.linuxjournal.com/article/7221

QuoteReplyEditDelete

2008-05-16 08:15:53     Re: Undefined or illegal instruction

Laurent Winkler (SWITZERLAND)

Message: 55924   

Hi,

Thanks for your quick reply. I managed to to test fork and vfork on a small program. Actually, fork() returns a "-1" at execution if the program is run on the blackfin card. This means that it returns an error.

However, is there a patch or something to make uc-linux runs using vfork() instead of fork() ?

QuoteReplyEditDelete

2008-05-16 09:52:43     Re: Undefined or illegal instruction

Mike Frysinger (UNITED STATES)

Message: 55929   

Linux doesnt care what userspace executes.  it is up to userspace applications to execute fork() or vfork() accordingly.

  • Created
Was this helpful?

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.