2008-05-05 06:46:02     RTC

2008-05-05 06:46:02     RTC

Servaes Joordens (NETHERLANDS)

Message: 55494   

I enabled the bfin-rtc. Is this rtc automaicatlly coupled to the function: gettimeofday? If not, is there a possibility to do this?

thanks

Servaes

QuoteReplyEditDelete

2008-05-05 08:19:47     Re: RTC

Robin Getz (UNITED STATES)

Message: 55499   

Servaes:

no - the RTC is not coupled to the kernel date functions (when the kernel boots, it reads the RTC to find the date, and that is it).

Can your describe what kind of functionality you are looking for?

-Robin

QuoteReplyEditDelete

2008-05-05 08:56:11     Re: RTC

Servaes Joordens (NETHERLANDS)

Message: 55500   

Robin,

I have to give a time-stamp with a ms resolution to each image I capture with my hardware. The normal timing of the blackfin depends on the main clock (which is dependent on a crystal). This oscilator however is not very stable, especiallu with temperature changes. Our hardware will be used in a temperature range of -40 to +50 Degrees Celcius The crystal of the rtc is much more stable, so I want to use that for timing.

The best thing would be to use the rtc as the basic mechanism for all timing. Hence my question.

Servaes

QuoteReplyEditDelete

2008-05-05 09:18:31     Re: RTC

Mike Frysinger (UNITED STATES)

Message: 55506   

if you want to read the RTC, then you need to open and read it manually

refer to linux-2.6.x/Documentation/rtc.txt for more information and code samples

  • Created
Was this helpful?

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.