2008-04-30 01:03:55     video in-out

2008-04-30 01:03:55     video in-out

Pranay Upadhyay (INDIA)

Message: 55270   

Hello all,

       I have successfully tested the video in and video out separately,for ppi driver for BF 561Ezkit. Now I want  video in-out same time for 561 Ez-kit,using cora A and core B.We have checked the video out for ppi1, it showing that core B is initialized.I have seen in the menuconfig but there was only one core B initialization option.Can we used the both core at same time for video in-out or is it possible that using only one core ,we can do video in-out.Please reply soon.

                                     -Regards

                                           -Pranay 

QuoteReplyEditDelete

2008-04-30 15:42:10     Re: video in-out

Mike Frysinger (UNITED STATES)

Message: 55309    there is only an example application for loading into core b because you need to write the application that gets loaded

QuoteReplyEditDelete

2008-05-02 02:27:16     Re: video in-out

Pranay Upadhyay (INDIA)

Message: 55361   

Hello Mike,

         Sorry, I am not getting whatever u reply.If we use only one core there is possible that we can do any processing algorithm on the video and out .Because in VDSP  core A and core B is used for real time video out .Means u r saying that only application code, if we write.Please reply I am confused about this.

                 -Thanks

                               -Pranay

QuoteReplyEditDelete

2008-05-02 04:37:14     Re: video in-out

Mike Frysinger (UNITED STATES)

Message: 55362   

you can do whatever you want in core b.  but that's the point ... you have to write all the code.

QuoteReplyEditDelete

2008-05-05 05:38:24     Re: video in-out

Pranay Upadhyay (INDIA)

Message: 55491   

Hello sir,

     ppi0 and ppi1 driver is working.May I write the application code through which both driver is opened and work successfully.I have write the application code in which I try to open the both the driver and capture the video from VCR and send to the ppi1 driver.But it is not working .Is it possible?

                                                 -Thanks

                                                      Pranay

QuoteReplyEditDelete

2008-06-17 10:48:30     Re: video in-out

Justin Wetherell (UNITED STATES)

Message: 57411   

Hello Pranay,

Could you let me know how you got the ppi0 and ppi1 drivers compiled for the 561? I am trying to accomplish the same thing.

QuoteReplyEditDelete

2008-06-19 08:32:13     Re: video in-out

Pranay Upadhyay (INDIA)

Message: 57583   

Hello Justin,

   First write the code for ppi0 and ppi1 driver. I have given the different major no. 241 and 242 respectively for these two driver.In vendor I register the driver with respective major no and give the name as you want. i have copied the both code in two different  file. One in the ppi driver code(ppi0) and another one in the bfin 7179fb code. And during menuconfig select the both  driver from respective position.

           If you want separate ppi0 and ppi1 then select any one of them.And compile the code using make command.Then after uImage.ext2 file will be created in the image folder.

-Regards

Pranay

  • Created
Was this helpful?

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.