2008-04-21 14:40:45     SDIO Wifi Mess

2008-04-21 14:40:45     SDIO Wifi Mess

Nick Moszer (UNITED STATES)

Message: 54636    Hello,

I'm working on getting a 88W8686 Marvell SDIO Wifi  card to play nice on a BF548-EZKIT.   I've run into a potential bug in the SDH driver for the bfin and thought if you guys could make heads of tails of it.

After loading the libertas module then the libertas_sdio module then loading the firmware onto the card, There is about a half second pause and the console spits:

BUG: failure at drivers/mmc/host/bfin_sdh.c:121/sdh_setup_data()!             

Kernel panic - not syncing: BUG! 

The most I can manage out of dmesg right before this happens is:  (i've got mmc debug off and libertas debug on)

     

libertas enter: libertas_init_module():1515

libertas leave: libertas_init_module():1517

libertas enter: if_sdio_init_module():1126

libertas_sdio: Libertas SDIO driver

libertas_sdio: Copyright Pierre Ossman

libertas enter: if_sdio_probe():919

libertas thread: class = 0x7, vendor = 0x2DF, device = 0x9103, model = 0xB, iopo        rt = 0x10000

libertas enter: if_sdio_prog_firmware():695

libertas enter: if_sdio_prog_helper():447

libertas thread: sending 60 bytes chunk

....(about 30 of these "sending 60 bytes chunk")

libertas thread: sending 60 bytes chunk

libertas thread: sending 56 bytes chunk

libertas thread: waiting for helper to boot...

libertas leave: if_sdio_prog_helper():549, ret 0

libertas enter: if_sdio_prog_real():565

This same behavior occurs with mmc debug off and libertas debug off.

Looking through bfin_sdh.c.. well.. anyone have any thoughts on where to go with this?

Thanks!

QuoteReplyEditDelete

2008-04-21 14:55:07     Re: SDIO Wifi Mess

Nick Moszer (UNITED STATES)

Message: 54637    Sorry, forgot to mention:

I'm using a svn kernel, 2.6.24.4-ADI-2008R2-pre-svn to be exact.  This is in a 2008R1-RC8 distribution.

The libertas driver is from the kernel with no modifications.

QuoteReplyEditDelete

2008-04-21 18:16:41     Re: SDIO Wifi Mess

Nick Moszer (UNITED STATES)

Message: 54656    After digging into this more, I changed the sdh_setup_data() function in bfin_sdh.c as follows:

//      pr_debug("%s enter flags:0x%x\n", __FUNCTION__, data->flags);

        printk("%s enter flags:0x%x numblocks:%d blksize:%d\n", __FUNCTION__, data->flags, data->blocks, data->blksz );

The output from this shows:

...(a bunch of these before this)               

sdh_setup_data enter flags:0x100 numblocks:16 blksize:32                      

sdh_setup_data enter flags:0x100 numblocks:1 blksize:32                       

sdh_setup_data enter flags:0x100 numblocks:16 blksize:32                      

sdh_setup_data enter flags:0x100 numblocks:1 blksize:32                       

sdh_setup_data enter flags:0x100 numblocks:16 blksize:32                      

sdh_setup_data enter flags:0x100 numblocks:1 blksize:32                       

sdh_setup_data enter flags:0x100 numblocks:3 blksize:32                       

sdh_setup_data enter flags:0x100 numblocks:1 blksize:32                       

sdh_setup_data enter flags:0x100 numblocks:1 blksize:50                       

BUG: failure at drivers/mmc/host/bfin_sdh.c:122/sdh_setup_data()!             

Kernel panic - not syncing: BUG!     

I read something in the libertas driver about SDH controllers puking on data chunks that aren't a multiple of 4.

Could this be the case here?

QuoteReplyEditDelete

2008-04-21 19:57:46     Re: SDIO Wifi Mess

Nick Moszer (UNITED STATES)

Message: 54657    Sorry about the numerous posts here..

The bug it's throwing, let me see if I've got this right.  It's saying you can only have block sizes that are a power of 2?

from sdh_setup_data() in bfin_sdh.c:121

BUG_ON(data->blksz & (data->blksz -1));

Adding padding code to the libertas driver to make transfers a multiple of 4 doesn't seem to help as the size would be 52 and not 64.

  • Created
Was this helpful?

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.