2008-04-10 10:51:55     scp (dropbear) didn't apply patch to dropbear-0.51

2008-04-10 10:51:55     scp (dropbear) didn't apply patch to dropbear-0.51

Andrea Federico Grisotto (ITALY)

Message: 54036    in svn trunk not all the patches applied to dropbear-0.49 have benn applied to dropbear-0.51.

When in the board scp starts, it looks where is the dbclient application.

This information is in the "options.h" file and in particular in the _PATH_SSH_PROGRAM macro.

trunk/user/dropbear/dropbear-0.49/options.h (line 206)

http://blackfin.uclinux.org/gf/project/uclinux-dist/scmsvn/?action=browse&path=%2Ftrunk%2Fuser%2Fdropbear%2Fdropbear-0.49%2Foptions.h&annotate=6092

trunk/user/dropbear/dropbear-0.51/options.h (line 212)

http://blackfin.uclinux.org/gf/project/uclinux-dist/scmsvn/?action=browse&path=%2Ftrunk%2Fuser%2Fdropbear%2Fdropbear-0.51%2Foptions.h&annotate=6488

uClinux install dbclient in "/bin" so it's necessary to rewrite the _PATH_SSH_PROGRAM macro in dropbear-0.51 in this way:

#define _PATH_SSH_PROGRAM "/bin/dbclient"

ciao Andrea.

QuoteReplyEditDelete

2008-04-10 17:00:53     Re: scp (dropbear) didn't apply patch to dropbear-0.51

Mike Frysinger (UNITED STATES)

Message: 54048    ive updated the Makefile to install the binaries into /usr/bin rather than /bin ... thanks for pointing this out

  • Created
Was this helpful?

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.