2008-04-08 11:37:11     compiler error with ISP1760 usb host

2008-04-08 11:37:11     compiler error with ISP1760 usb host

Michiel Verschueren (BELGIUM)

Message: 53850    Hi,

I've tried to compile uClinux with support for the ISP 1760 enabled, but I run into the following errors when compiling:

In file included from drivers/usb/host/pehcd/host/pehci.c:118:

drivers/usb/host/pehcd/host/qtdptd.c: In function ‘phci_hcd_qh_link_async’:

drivers/usb/host/pehcd/host/qtdptd.c:590: warning: unused variable ‘td_ptd_map’

drivers/usb/host/pehcd/host/qtdptd.c:589: warning: unused variable ‘ptd_map_buff’

drivers/usb/host/pehcd/host/qtdptd.c: In function ‘phci_hcd_qha_from_qtd’:

drivers/usb/host/pehcd/host/qtdptd.c:1212: warning: unused variable ‘cerr’

drivers/usb/host/pehcd/host/pehci.c: In function ‘pehci_hcd_td_ptd_submit_urb’:

drivers/usb/host/pehcd/host/pehci.c:293: warning: passing argument 4 of ‘isp1761_mem_write’ makes pointer from integer without a cast

drivers/usb/host/pehcd/host/pehci.c: In function ‘pehci_hcd_urb_complete’:

drivers/usb/host/pehcd/host/pehci.c:773: error: too few arguments to function ‘usb_hcd_giveback_urb’

drivers/usb/host/pehcd/host/pehci.c: In function ‘pehci_hcd_atl_worker’:

drivers/usb/host/pehcd/host/pehci.c:1998: warning: label ‘schedule’ defined but not used

drivers/usb/host/pehcd/host/pehci.c: At top level:

drivers/usb/host/pehcd/host/pehci.c:3139: warning: initialization from incompatible pointer type

drivers/usb/host/pehcd/host/pehci.c:3140: warning: initialization from incompatible pointer type

make[6]: *** [drivers/usb/host/pehcd/host/pehci.o] Error 1

make[5]: *** [drivers/usb/host/pehcd/host] Error 2

make[4]: *** [drivers/usb/host/pehcd] Error 2

make[3]: *** [drivers/usb/host] Error 2

make[2]: *** [drivers/usb] Error 2

make[1]: *** [drivers] Error 2

I'm using uClinux 2008R1-RC8 (revision 6419), and version 2008R1-RC7 of the Toolchain.

Thanks in advance

QuoteReplyEditDelete

2008-04-08 12:17:33     Re: compiler error with ISP1760 usb host

Michael Hennerich (GERMANY)

Message: 53853    Are you really sure that you use the 2008R1 release?

For me 2008R1 compiles and works.

This failure is a known issue only on svn trunk.

http://blackfin.uclinux.org/gf/project/uclinux-dist/tracker/?action=TrackerItemEdit&tracker_id=141&tracker_item_id=3973

-Michael

QuoteReplyEditDelete

2008-04-09 03:12:11     Re: compiler error with ISP1760 usb host

Michiel Verschueren (BELGIUM)

Message: 53877    Hi,

thanks for your quick reply.

I am sure I'm using 2008R1; I've checked out revision 6419 yesterday. Can you let me know which revision (or which RC) you are using?

Just to make sure: do I need anything else than the Toolchain and the uclinux-dist?

QuoteReplyEditDelete

2008-04-09 03:29:15     Re: compiler error with ISP1760 usb host

Michiel Verschueren (BELGIUM)

Message: 53879    Also, to make sure, what exactly should I use at the command line to check out the 2008R1 release?

I've been using the following:

svn checkout svn://firewall-sources.blackfin.uclinux.org:80/svn/uclinux-dist/trunk -r 6419 2008R1-RC8

Is this correct?

QuoteReplyEditDelete

2008-04-09 03:34:17     Re: compiler error with ISP1760 usb host

Michael Hennerich (GERMANY)

Message: 53880    No - you checkout trunk ...

USE:

svn checkout svn://firewall-sources.blackfin.uclinux.org:80/svn/uclinux-dist/branches/2008R1 2008R1-RC8

-Michael

QuoteReplyEditDelete

2008-04-09 03:38:25     Re: compiler error with ISP1760 usb host

Michael Hennerich (GERMANY)

Message: 53881    See also here:

http://docs.blackfin.uclinux.org/doku.php?id=developing_with_blackfin_live_sources&s[]=branches

-Michael

QuoteReplyEditDelete

2008-04-10 03:31:04     Re: compiler error with ISP1760 usb host

Michiel Verschueren (BELGIUM)

Message: 53984    I've been able to compile without any problems now.

Apparently I've been checking out the wrong versions of U-Boot and the Toolchain too, so thanks for your help.

QuoteReplyEditDelete

2008-04-15 09:06:20     Re: compiler error with ISP1760 usb host

Michiel Verschueren (BELGIUM)

Message: 54274    Hi,

now that I can compile uClinux with isp1760 support, I'm having trouble loading the driver when booting uClinux.

I get the following messages:

drivers/usb/host/pehcd/hal/hal_pxa.c: isp1761_register_driver(drv=0014bd18)

drivers/usb/host/pehcd/host/pehci.c: Host Driver has not been Registered with errors : -19

drivers/usb/host/pehcd/hal/hal_pxa.c: pid 8210, vid 8210

drivers/usb/host/pehcd/hal/hal_pxa.c: controller address 00144774

I have been altering the options in the build configuration, but that didn't help me. My current configuration looks like this (in the config menu):

<*> Support for Host-side USB

[*]   USB verbose debug messages

---   Miscellaneous USB options

[ ]   USB device filesystem

[ ]   USB device class-devices (DEPRECATED)

[ ]   Dynamic USB minor allocation (EXPERIMENTAL)

[*]   Rely on OTG Targeted Peripherals List

[ ]   Disable external hubs

---   USB Host Controller Drivers                                                                                      │ │

< >   ISP116X HCD support

< >   ISP1362 HCD support

<*>   ISP1760 HCD support

< >   SL811HS HCD support

(options below this are left blank).

I have enabled 16-bit packing for the asynchronous interface that the isp1760 is connected to. I think this explains the "pid 8210, vid 8210" output, but from the driver I have understood that bit packing should be enabled. Also, without bit packing, I get a "scratch register mismatch" warning from the driver.

I don't think this is a hardware problem, as I can access the chip properly from U-Boot.

Also, if this were a hardware problem, I think the driver would report a "scratch register mismatch" and not the "controller address" (see the isp1761_probe function in hal_pxa.c).

Any help would be welcome.

QuoteReplyEditDelete

2008-04-15 10:00:05     Re: compiler error with ISP1760 usb host

Michael Hennerich (GERMANY)

Message: 54276    The driver only works when build as a module:

Then do:

#modprobe hal_pxa

#modprobe pehci

-Michael

QuoteReplyEditDelete

2008-04-15 11:41:41     Re: compiler error with ISP1760 usb host

Michiel Verschueren (BELGIUM)

Message: 54283    Hi Michael,

thanks for your reply, but I'm afraid I don't know how to build this driver as a module. I've been looking in the documentation, but I have not found anything useful.

I have executed "make modules" and "make modules_install", after which I expected to find a hal_pxa.ko and a pehci.ko file somewhere, but obviously I didn't.

What am I forgetting here?

QuoteReplyEditDelete

2008-04-15 11:53:59     Re: compiler error with ISP1760 usb host

Michael Hennerich (GERMANY)

Message: 54285    <M> Support for Host-side USB

[*]   USB verbose debug messages

---   Miscellaneous USB options

[ ]   USB device filesystem

[ ]   USB device class-devices (DEPRECATED)

[ ]   Dynamic USB minor allocation (EXPERIMENTAL)

[*]   Rely on OTG Targeted Peripherals List

[ ]   Disable external hubs

---   USB Host Controller Drivers                                                                                      │ │

< >   ISP116X HCD support

< >   ISP1362 HCD support

<M>   ISP1760 HCD support

< >   SL811HS HCD support

Simply make your that you change <*> to <M>.

(hit space bar twice)

-Michael

  • Created
Was this helpful?

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.