2008-03-24 19:51:26     Kernel panic - not syncing: No init found when builiding as FDPIC

2008-03-24 19:51:26     Kernel panic - not syncing: No init found when builiding as FDPIC

Javier Herrero (SPAIN)

Message: 52981    Hello,

I've changed the application/library settings from FLAT to FDPIC, and now I obtain a 'Kernel panic - not syncing: No init found. Try passing init= option to kernel.' message.

After changing from FLAT to FDPIC I've done a make clean to assure that all is build ok, and the init is under /bin. The board is BF532 based, and the filesystem is jffs2 in flash memory.

Perhaps I'm forgetting something obvious...

Regards,

Javier

QuoteReplyEditDelete

2008-03-24 21:11:01     Re: Kernel panic - not syncing: No init found when builiding as FDPIC

David Rowe (AUSTRALIA)

Message: 52982    Hi Javier,

Had a very similar bug recently.  It could be that init can't run as uClibc isnt present on your file system.  Check your uClinux-dist/romfs/lib and see if ld-uClibc* are present.  If not, do a make config_menuconfig and in Blackfin build options make sure FDPIC is selected as the Binary Format.

Cheers,

David

QuoteReplyEditDelete

2008-03-24 23:09:30     Re: Kernel panic - not syncing: No init found when builiding as FDPIC

Yi Li (CHINA)

Message: 52985    Please attach the kernel boot message here for debug. Also please tell us what is your toolchain and kernel version.

-Yi

QuoteReplyEditDelete

2008-03-25 05:47:01     Re: Kernel panic - not syncing: No init found when builiding as FDPIC

Javier Herrero (SPAIN)

Message: 53002    Hi, David,

Thank you very much for your answer. You're, I've found that the shared libraries were not properly being included under /lib. Now it works OK.

Yi, I'm using latest SVN uclinux-dist and toolchain.

Thanks! Regards,

Javier

  • Created
Was this helpful?

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.