2008-02-07 03:44:52     Modbus in uclinux/Kernel

2008-02-07 03:44:52     Modbus in uclinux/Kernel

klaus hauer (AFGHANISTAN)

Message: 50797    Hi,

has anybody experience in using Modbus protocol for uclinux????

Kind regards Klaus

TranslateQuoteReplyEditDelete

2008-02-07 06:28:51     Re: Modbus in uclinux/Kernel

Javier Herrero (SPAIN)

Message: 50815    Hello, Klaus,

We have a customer who is currently using our HV Sistemas H8606 board with a 16550-class UART programmed into the FPGA and a RS485 interface who is running an application for data acquisition and control of several distributed control modules using Modbus protocol. I think that he is using a public domain Modbus library, and as far as I know he had not found any problem in implementing the library and the application under uClinux. I will try to know which library he is currently using if you are interested.

Best regards,

Javier

QuoteReplyEditDelete

2008-02-07 09:21:26     Re: Modbus in uclinux/Kernel

klaus hauer (AFGHANISTAN)

Message: 50820    Hi Javier,

yes I´m very interested which library it is an where I could get this library.

Thank you and kind regards

Klaus

TranslateQuoteReplyEditDelete

2008-02-07 10:34:31     Re: Modbus in uclinux/Kernel

Javier Herrero (SPAIN)

Message: 50823    Hi,

I've asked my customer, and told me that he found that code here:

http://www.geocities.com/pbmcrae42/index2.html

http://www.geocities.com/pbmcrae42/linuxmbus.ZIP

He however has warned me that he had to modify the code because packet CRC calculation was not right and he had to do a slight modification of the code. I hope anyway that this can be of some help to you.

Best regards,

Javier

QuoteReplyEditDelete

2008-02-08 03:31:19     Re: Modbus in uclinux/Kernel

klaus hauer (AFGHANISTAN)

Message: 50844    Thank you very much, Javier.

Have you some additional Information how to implement this library to my kernel???

Regards Klaus

  • Created
Was this helpful?

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.