2008-02-06 18:35:13     NO GDB-File in FDPIC Format

2008-02-06 18:35:13     NO GDB-File in FDPIC Format

Herbert Weinfurter (AUSTRIA)

Message: 50781    I switched to alsa-sound system and therefore I had to use FDPIC-format

currently there are no more gdb-files generated!

what's the general way to debug? (there is also a uclibc_gdb available)

QuoteReplyEditDelete

2008-02-06 19:00:48     Re: NO GDB-File in FDPIC Format

Mike Frysinger (UNITED STATES)

Message: 50783    you dont need a .gdb file.  simply use the ELF in question.  that's all a .gdb file is.

QuoteReplyEditDelete

2008-02-06 19:02:24     Re: NO GDB-File in FDPIC Format

Herbert Weinfurter (AUSTRIA)

Message: 50785    thanks,   I suggest to add this information at the debugging-documenation

QuoteReplyEditDelete

2008-02-13 04:21:35     Re: NO GDB-File in FDPIC Format

Yi Li (CHINA)

Message: 50976    This is mentioned here: http://docs.blackfin.uclinux.org/doku.php?id=debuggers#debugging_single_applications

  • Created
Was this helpful?

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.