2008-02-04 13:58:39     bfin_spi_adc.c and copy_from_user()

2008-02-04 13:58:39     bfin_spi_adc.c and copy_from_user()

murti iki (GERMANY)

Message: 50644    hello all,

I would like to ask the reason why there is not a copy_from_user() function in the write function of file operations.

The read function has the copy_to_user() but as far as I see the write() function directly dereferences the buffer

from the kernel space.

I would be most happy if somebody can explain me the idea behind this.

thanks alot

tos

QuoteReplyEditDelete

2008-02-04 16:54:41     Re: bfin_spi_adc.c and copy_from_user()

Michael Hennerich (GERMANY)

Message: 50653   

I guess this is just bad code, which tends to work on noMMU.

From an efficiency point of view it’s not a bad idea, however it violates various security aspects.

In case you’re a system designer – and know what you are doing…

However we are going to remove this driver soon, please use the spidev interface for user space access.

-Michael

QuoteReplyEditDelete

2008-02-05 05:49:29     Re: bfin_spi_adc.c and copy_from_user()

murti iki (GERMANY)

Message: 50674    Hello Michael,

  Thank you for your answer. Actually I am a little bit confused about the spi documentation.

  I would appreciate if you can also help me with the below questions of mine.

    1) http://docs.blackfin.uclinux.org/doku.php?id=adsp-spiadc_documentation

    tells that there are 2 spi drivers namely linux-2.6.x/drivers/char/spi.c (interrupt driven)

                                       and  linux-2.6.x/drivers/char/adsp-spiadc.c (dma driven)

    however in the linux-2.6.x/drivers/char/ folder there is only bfin_spi_adc.c

    I have double checked but couldn't find them, I have found one driver named spi.c but it's

    located in linux-2.6.x/drivers/spi/spi.c (also it doesn't have any ioctl commands)

    Where can I find these two drivers? ***

    I also cannot find the /linux-2.6.x/documentation/spi/spidev file.

        

    2) I have tried to go through the source files to understand the relation between these source codes to little success. Can you please explain me the connection between below files.

      

          linux-2.6.x/drivers/spi/spi_bfin5xx.c

          linux-2.6.x/drivers/spi/spi.c

     (Probably I am wrong but) To me these files tend to provide kernel functions so that higher layer drivers can utilize them. In my opinion bfin_spi_adc.c is a higher layer driver than these two however it doesn't seem to utilize them. Maybe these two drivers that I couldn't find  utilizes them in a way that a linux-uClinux newbie like me can see it easily.

Mit freundlichen Grüssen

tos

*** I have only downloaded the uClinux-dist-2007R1.1-RC3.

QuoteReplyEditDelete

2008-02-05 06:16:16     Re: bfin_spi_adc.c and copy_from_user()

Michael Hennerich (GERMANY)

Message: 50676    Tos,

the ADSP-SPIADC was obsoleted  and removed  some time ago, while we introduced the generic SPI bus driver.

It does not longer exist - I therefore removed the documentation o the wiki.

The spidev driver will be in our next release coming soon.

You can check out the 2008R1release using svn.

Gruss,

-Michael

QuoteReplyEditDelete

2008-02-05 14:21:22     Re: bfin_spi_adc.c and copy_from_user()

murti iki (GERMANY)

Message: 50711    Thanks Michael.

Maybe it's a stupid question but can you also tell me how to find this spidev driver in the svn.

I have searched for some time looked under these places

/branches/2008R1

/tags/2008R1-RC1

but couldn't find it.

QuoteReplyEditDelete

2008-02-06 10:35:20     Re: bfin_spi_adc.c and copy_from_user()

Myrick Monroe (UNITED STATES)

Message: 50765   

I just looked also and I have the same question...

Myrick

QuoteReplyEditDelete

2008-02-12 04:27:59     Re: bfin_spi_adc.c and copy_from_user()

murti iki (GERMANY)

Message: 50921    After having some time off with other subjects.

I have looked into this svn issue. As a user new to linux, I have found out that you need the subversion software to access this

trunk.  There is an online book in the "svn references" section to the left. It has a good deal of information.

Anyway probably, use of this svn is already mentioned in the wiki but for careless readers like me, maybe a bigger typed notice would help

  • Created
Was this helpful?

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.