2008-01-25 18:51:52     Starting daemon from /etc/rc messes up stdin?

2008-01-25 18:51:52     Starting daemon from /etc/rc messes up stdin?

Steve Strobel (UNITED STATES)

Message: 50172    I am trying to start a long-running background process (daemon) from /etc/rc using a command like "/sleep_and_echo &" (I am using the simple script shown below for testing).  When I run that command manually after booting, I can continue to enter commands at the "root~>" prompt and see the responses (intermingled with the "Sleeping..." output from the background task).  When I run that task from the /etc/rc file, it seems to prevent me doing anything else from the console, both while it is running and even after it has completed.  What am I missing?

#! /bin/sh

echo "This is /mnt/permanent/startup/sleep_and_echo"

sleep 1

echo "Sleeping..."

sleep 1

echo "Sleeping..."

sleep 1

echo "Sleeping..."

sleep 1

echo "Sleeping..."

sleep 1

echo "Sleeping..."

sleep 1

Thanks for any suggestions,

Steve

QuoteReplyEditDelete

2008-02-06 10:41:10     Re: Starting daemon from /etc/rc messes up stdin?

Mike Frysinger (UNITED STATES)

Message: 50766    seems to work for me ... anything running in /etc/rc should not affect the login shell launched on the console ...

what are your console / simpleinit settings ?

..............

Have a lot of fun...

jThis is /mnt/permanent/startup/sleep_and_echo

BusyBox v1.9.0 (2008-02-05 20:09:28 EST) built-in shell (msh)

Enter 'help' for a list of built-in commands.

root:/> PHY: 0:01 - Link is Up - 100/Full

Sleeping...

uptime

14:20:13 up 0 min, load average: 0.00, 0.00, 0.00

root:/> Sleeping...

root:/> uptime

14:20:14 up 0 min, load average: 0.08, 0.01, 0.00

root:/> Sleeping...

root:/> uptime

14:20:15 up 0 min, load average: 0.08, 0.01, 0.00

root:/> Sleeping...

date

Thu Jan  1 14:20:16 UTC 1970

root:/> daSleeping...

te

Thu Jan  1 14:20:17 UTC 1970

root:/>

QuoteReplyEditDelete

2008-02-15 18:42:00     Re: Starting daemon from /etc/rc messes up stdin?

Steve Strobel (UNITED STATES)

Message: 51132    It started working for me too.  I must have had something set up incorrectly, but I never figured out what it was.  Thanks for the help.

  • Created
Was this helpful?

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.