2008-01-11 05:57:18     Any options or methods in uclinux to reduce latency

2008-01-11 05:57:18     Any options or methods in uclinux to reduce latency

sneha lal (INDIA)

Message: 49476    hi all

We are working with mpeg codec applications and the target is bf561.

As the project is in final stage,we have started the optimization and looking to reduce the latency occured by our application.

Is there any specific method or option in uclinux kernel to do this task?

It would be great help for us if you provide any ideas regarding this..

thanks

QuoteReplyEditDelete

2008-01-11 08:06:13     Re: Any options or methods in uclinux to reduce latency

Robin Getz (UNITED STATES)

Message: 49501    Sneha:

I'm not sure what you mean by latency. Latency == delay. How is there delay in your application?

-Robin

QuoteReplyEditDelete

2008-01-21 01:14:15     Re: Any options or methods in uclinux to reduce latency

sneha lal (INDIA)

Message: 49876   

hi

Actually our need is to reduce the execution time of application.The latency i mean was the time taken by the board to produce the output.So what are the kernel optimization methods available in uclinux?

thanks

QuoteReplyEditDelete

2008-01-21 01:56:59     Re: Any options or methods in uclinux to reduce latency

Yi Li (CHINA)

Message: 49877    > The latency i mean was the time taken by the board to produce the output.

This is still very unclear. There are things you need to do before optimization:

1. measure your current "latency"

2. identify bottle neck

3. optimize

  • Created
Was this helpful?

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.