2007-11-26 03:31:31     adeos patch (xenomai)

2007-11-26 03:31:31     adeos patch (xenomai)

Filip Van Rillaer (BELGIUM)

Message: 47505   

Hello,

The latest update of the xenomai patch is 7 months old.  It's clear that a lot of files that are touched by this patch have changed a lot in those 7 months.

I found a more recent patch : adeos-ipipe-2.6.23-bf5xx-1.7-00.patch (r3090 | rpm | 2007-10-17 18:57:24 +0200 (Wed, 17 Oct 2007) | 1 line Upgrade Adeos/blackfin support)

URL: http://svn.gna.org/svn/xenomai/trunk/ksrc/arch/blackfin/patches

Unfortunately I cannot find the SVN version on which this patch was applied.  Who know's which version I should check out to apply this patch?

When can we expect an updated patch on blackfin.uclinux.org?

Best regards,

Filip

TranslateQuoteReplyEditDelete

2007-11-26 22:36:42     Re: adeos patch (xenomai)

Yi Li (CHINA)

Message: 47532    Hi,

This "adeos-ipipe-2.6.23-bf5xx-1.7-00.patch" confusing me too. The SVN trunk blackfin uclinux kernel is still 2.6.22. You may try to apply the patch to SVN checkout around 2007-10-17. But I will spend some time to update the patch to current SVN.

-Yi

QuoteReplyEditDelete

2007-11-28 03:59:22     Re: adeos patch (xenomai)

Filip Van Rillaer (BELGIUM)

Message: 47693   

Hello Yi,

Thank you for your answer and sorry for my late reply (I was not in the office for 1 1/2 day).

I got some info from Philippe Gerum about the 2.6.23 patch : <<This patch is against v2.6.23 vanilla. GIT commit bbf25010f1a6b761914430f5fca081ec8c7accd1.>>

Can you tell me (or where I can find a some info about it) how such an updated patch for Blackfin uClinux is made, or otherwise stated "where can I find the SVN repositories that are merged to create the patch-file that can be found in uclinux-dist/bfin_patch/adeos_patch"?

Many thanks in advance,

Filip

TranslateQuoteReplyEditDelete

2007-11-28 05:01:26     Re: adeos patch (xenomai)

Yi Li (CHINA)

Message: 47700    Filip,

The blackfin uclinux kernel development is based on this svn: see here: https://blackfin.uclinux.org/gf/project/linux-kernel/scmsvn

We sync the blackfin arch code (and related common code) with the vanilla linux-kernel git tree frequently (a week or so).  When we do a release, we sync the whole linux-kernel in our svn with vanilla tree (including all common code and other arch), e.g, from 2.6.22 to 2.6.23. So there is a little difference between our SVN trunk and the upstream linux git tree.

It is suggested to do blackfin uclinux development based on our svn since we will do the synchronize with upstream.

Adeos is an out-of-tree kernel patch. It affects both blackfin arch and common code. The maintainer can choose to use either upstream vanilla tree or ours. But I will ask if he could make patch based on our SVN.

Also since there is a time difference between Xenomai release and the blackfin uclinux release,  I keep a patch in uclinux-dist/bfin_patch/adeos_patch, which will be updated when people asking for an adeos patch for latest SVN trunk or latest release. But the patch from Xenomai project should be the main source.

So if you want to use adeos/xenomain, you can use "adeos-ipipe-bf53x-R07R1RC3-1.6-02.patch"  and "uclinux-dist-2007r1-rc3" release.

-Yi

QuoteReplyEditDelete

2007-11-28 12:13:12     Re: adeos patch (xenomai)

Filip Van Rillaer (BELGIUM)

Message: 47779   

Hello Yi,

Thank you for your explanation.

I will wait for the updated patch in SVN.

Best regards,

Filip

TranslateQuoteReplyEditDelete

2007-11-30 03:29:08     Re: adeos patch (xenomai)

Filip Van Rillaer (BELGIUM)

Message: 47879   

Hello Yi,

You wrote : << But I will ask if he could make patch based on our SVN.>>

When do you think that the updated patch will be available?

Many thanks in advance,

Filip

TranslateQuoteReplyEditDelete

2007-11-30 04:14:23     Re: adeos patch (xenomai)

Yi Li (CHINA)

Message: 47880    Hi,

I got the answer from Philippe that he "<tt>don't track the Blackfin SVN</tt>

<tt>repo anymore since 2.6.23, but rather the mainline tree</tt> ". So I think we will need to update the patch to the SVN trunk. I need to finish things at hand before working on this (a week or so). I'd suggest to use 07r1 patch if you cannot wait.

-Yi

QuoteReplyEditDelete

2007-11-30 04:49:02     Re: adeos patch (xenomai)

Filip Van Rillaer (BELGIUM)

Message: 47884   

OK, thank you for your effort,

Filip

TranslateQuoteReplyEditDelete

2008-04-04 06:14:49     Re: adeos patch (xenomai)

Mattias K (SWEDEN)

Message: 53636    Hi,

I would like to try xenomai for the 2007RC3.1 release. I can find the adeos patch but which version of xenomai shall I use?

regards,

/Mattias

QuoteReplyEditDelete

2008-04-07 00:15:56     Re: adeos patch (xenomai)

Yi Li (CHINA)

Message: 53724    please use: xenomai-2.4-rc4/ksrc/arch/blackfin/patches/adeos-ipipe-bf53x-R07R1RC3-1.6-02.patch

QuoteReplyEditDelete

2008-04-07 03:30:30     Re: adeos patch (xenomai)

Mattias K (SWEDEN)

Message: 53731    Ok,

I just tested, this patch does not work with the 2007RC3.1 rc.

I will test with 2008 release.

/Mattias

  • Created
Was this helpful?

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.