[#4186] Test of scratchpad_app_stack failed in SMP kernel
Submitted By: Vivi Li
Open Date
2008-06-23 04:46:33 Close Date
2008-10-17 00:29:46
Priority:
Medium Assignee:
Vivi Li
Status:
Closed Fixed In Release:
N/A
Found In Release:
N/A Release:
Category:
N/A Board:
Processor:
N/A Silicon Revision:
Is this bug repeatable?:
Yes Resolution:
Rejected
Uboot version or rev.:
Toolchain version or rev.:
08r1.5-11
App binary format:
Summary: Test of scratchpad_app_stack failed in SMP kernel
Details:
Test of scratchpad_app_stack failed in SMP kernel.
Below is the log.
Test script, build script and test source code are located at uclinux-dist/testsuites/scratchpad_app_stack.
--
root:/> ./helloworld
BINFMT_FLAT: L1 stack support disabled - will continue anyway
Hello world!, 0x4c4f20
TEST FAIL
root:/> version
kernel: Linux release 2.6.22.19-ADI-2008R1-svn4872, build #98 SMP Mon Jun 23 04:09:27 CST 2008
toolchain: bfin-uclinux-gcc release gcc version 4.1.2 (ADI svn)
user-dist: release svn-6801, build #802 Mon Jun 23 04:08:39 CST 2008
root:/>
Follow-ups
--- Graf Yang 2008-06-25 02:32:15
This APP will fail when it run on CoreB, because it check the stack high/low
boundaries of CoreA.
--- Mike Frysinger 2008-06-25 07:55:59
then we need to update the test so that it only runs on core a
--- Graf Yang 2008-10-16 06:01:03
SMP kernel have closed supporting user app stack in L1 scratchpad, so this test
have been meaningless.
--- Vivi Li 2008-10-17 00:29:46
So don't run this test case for SMP test.
And close this bug.
Thanks!
Files
Changes
Commits
Dependencies
Duplicates
Associations
Tags
File Name File Type File Size Posted By
No Files Were Found