[#4565] eth0 device on bf537 fails to be started.
Submitted By: Mingquan Pan
Open Date
2008-10-27 03:33:59 Close Date
2008-10-27 22:32:55
Priority:
Medium Assignee:
Mike Frysinger
Status:
Closed Fixed In Release:
N/A
Found In Release:
N/A Release:
Category:
N/A Board:
Processor:
N/A Silicon Revision:
Is this bug repeatable?:
Yes Resolution:
Fixed
Uboot version or rev.:
Toolchain version or rev.:
svn head
App binary format:
Summary: eth0 device on bf537 fails to be started.
Details:
eth0 device on bf537 fails to be started on trunk now.
root:/> dmesg
Linux version 2.6.26.5-ADI-2009R1-pre-svn5484-dirty (test@40-bf537-toolchain) (gcc version 4.1.2 (ADI svn)) #14 Mon Oct 27 16:47:54 CST 2008
console [early_BFuart0] enabled
early printk enabled on early_BFuart0
Warning: limiting memory to 56MB due to hardware anomaly 05000263
Board Memory: 64MB
Kernel Managed Memory: 64MB
Memory map:
fixedcode = 0x00000400-0x00000490
text = 0x00001000-0x00109150
rodata = 0x00109160-0x0015bc74
bss = 0x0015bc80-0x0016afd8
data = 0x0016afd8-0x0017a000
stack = 0x00178000-0x0017a000
init = 0x0017a000-0x004fa000
available = 0x004fa000-0x037ff000
DMA Zone = 0x03f00000-0x04000000
Hardware Trace Active and Enabled
Reset caused by Software reset
Blackfin support (C) 2004-2008 Analog Devices, Inc.
Compiled for ADSP-BF537 Rev 0.2
Blackfin Linux support by blackfin.uclinux.org/
Processor Speed: 500 MHz core clock and 100 MHz System Clock
boot memmap: 00000000004fa000 - 00000000037ff000 (usable)
On node 0 totalpages: 14335
DMA zone: 112 pages used for memmap
DMA zone: 0 pages reserved
DMA zone: 14223 pages, LIFO batch:3
Normal zone: 0 pages used for memmap
Movable zone: 0 pages used for memmap
NOMPU: setting up cplb tables for global access
Instruction Cache Enabled
Data Cache Enabled (write-through)
Built 1 zonelists in Zone order, mobility grouping off. Total pages: 14223
Kernel command line: root=/dev/mtdblock0 rw earlyprintk=serial,uart0,57600 panic=3
Configuring Blackfin Priority Driven Interrupts
PID hash table entries: 256 (order: 8, 1024 bytes)
console handover: boot [early_BFuart0] -> real [ttyBF0]
Dentry cache hash table entries: 8192 (order: 3, 32768 bytes)
Inode-cache hash table entries: 4096 (order: 2, 16384 bytes)
Kernel managed physical pages: 14335
Memory available: 51664k/65536k RAM, (3584k init code, 1056k kernel code, 452k data, 1024k dma, 7756k reserved)
Calibrating delay loop... 997.37 BogoMIPS (lpj=1994752)
Security Framework initialized
Mount-cache hash table entries: 512
Blackfin Scratchpad data SRAM: 4 KB
Blackfin L1 Data A SRAM: 16 KB (15 KB free)
Blackfin L1 Data B SRAM: 16 KB (16 KB free)
Blackfin L1 Instruction SRAM: 48 KB (41 KB free)
net_namespace: 192 bytes
NET: Registered protocol family 16
Blackfin GPIO Controller
Blackfin DMA Controller
stamp_init(): registering device resources
NET: Registered protocol family 2
IP route cache hash table entries: 1024 (order: 0, 4096 bytes)
TCP established hash table entries: 2048 (order: 2, 16384 bytes)
TCP bind hash table entries: 2048 (order: 1, 8192 bytes)
TCP: Hash tables configured (established 2048 bind 2048)
TCP reno registered
NET: Registered protocol family 1
Setting up Blackfin MMR debugfs
msgmni has been set to 100
io scheduler noop registered
io scheduler anticipatory registered (default)
io scheduler cfq registered
Serial: Blackfin serial driver
bfin-uart.1: ttyBF0 at MMIO 0xffc00400 (irq = 18) is a BFIN-UART
brd: module loaded
bfin_mac bfin_mac.0: Requesting peripherals failed!
bfin_mac: probe of bfin_mac.0 failed with error -14
bfin-spi bfin-spi.0: Blackfin BF5xx on-chip SPI Controller Driver, Version 1.0, regs_base@ffc00500, dma channel@7
rtc-bfin rtc-bfin: rtc core: registered rtc-bfin as rtc0
bfin-wdt: initialized: timeout=20 sec (nowayout=0)
TCP cubic registered
NET: Registered protocol family 17
rtc-bfin rtc-bfin: setting system clock to 1970-01-01 19:17:38 UTC (69458)
Freeing unused kernel memory: 3584k freed
dma_alloc_init: dma_page @ 0x004f6000 - 256 pages at 0x03f00000
root:/> ifconfig
lo Link encap:Local Loopback
inet addr:127.0.0.1 Mask:255.0.0.0
UP LOOPBACK RUNNING MTU:16436 Metric:1
RX packets:0 errors:0 dropped:0 overruns:0 frame:0
TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:0
RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)
root:/> ifconfig eth0 10.100.4.50
ifconfig: SIOCSIFADDR: No such device
Follow-ups
--- Mike Frysinger 2008-10-27 05:05:40
hmm, looks like i may have broken it with my gpio cleanups ...
--- Mike Frysinger 2008-10-27 15:31:10
should be fixed now ... the BF54x code had a bug where it would reject
peripheral-only pins and when i merged, it leaked into the BF53x code ... but it
should be fixed now
--- Mingquan Pan 2008-10-27 22:32:55
Yes,close.
Files
Changes
Commits
Dependencies
Duplicates
Associations
Tags
File Name File Type File Size Posted By
No Files Were Found