[#4749] Boot kernel in BF533-EZKIT without set ip during boot, it stops at initial console
Submitted By: Vivi Li
Open Date
2008-12-23 04:47:44 Close Date
2008-12-30 01:42:14
Priority:
Medium High Assignee:
Sonic Zhang
Status:
Closed Fixed In Release:
N/A
Found In Release:
N/A Release:
Category:
N/A Board:
EZKIT Lite
Processor:
BF533 Silicon Revision:
Is this bug repeatable?:
Yes Resolution:
Fixed
Uboot version or rev.:
Toolchain version or rev.:
toolchain 4.1-2008_Dec_03
App binary format:
Summary: Boot kernel in BF533-EZKIT without set ip during boot, it stops at initial console
Details:
BF533-EZKIT fails to boot up when initial console.
It's default config, and ip is not set during kernel boot.
Config file is attached. Bellow is the log:
--
(tftpboot 0x1000000 linux; bootelf)
Linux version 2.6.28-rc2-ADI-2009R1-pre-svn5909 (test@uclinux67-533ezkit) (gcc version 4.1.2 (ADI s8
Warning: limiting memory to 31MB due to hardware anomaly 05000263
Board Memory: 32MB
Kernel Managed Memory: 32MB
Memory map:
fixedcode = 0x00000400-0x00000490
text = 0x00001000-0x001056a0
rodata = 0x001056a0-0x00151648
bss = 0x00151650-0x0015fc9c
data = 0x0015fc9c-0x0016e000
stack = 0x0016c000-0x0016e000
init = 0x0016e000-0x003dd000
available = 0x003dd000-0x01eff000
DMA Zone = 0x01f00000-0x02000000
Hardware Trace Active and Enabled
Blackfin support (C) 2004-2008 Analog Devices, Inc.
Compiled for ADSP-BF533 Rev 0.3
Warning: Compiled for Rev 3, but running on Rev 4
Blackfin Linux support by blackfin.uclinux.org/
Processor Speed: 594 MHz core clock and 118 MHz System Clock
NOMPU: setting up cplb tables
Instruction Cache Enabled for CPU0
Data Cache Enabled for CPU0 (write-through)
Built 1 zonelists in Zone order, mobility grouping off. Total pages: 7873
Kernel command line: root=/dev/mtdblock0 rw
Configuring Blackfin Priority Driven Interrupts
PID hash table entries: 128 (order: 7, 512 bytes)
console [ttyBF0] enabled
Dentry cache hash table entries: 4096 (order: 2, 16384 bytes)
Inode-cache hash table entries: 2048 (order: 1, 8192 bytes)
Memory available: 27484k/32768k RAM, (2492k init code, 1041k kernel code, 419k data, 1024k dma, 308)
Calibrating delay loop... 1183.74 BogoMIPS (lpj=2367488)
Security Framework initialized
Mount-cache hash table entries: 512
Blackfin Scratchpad data SRAM: 4 KB
Blackfin L1 Data A SRAM: 16 KB (15 KB free)
Blackfin L1 Data B SRAM: 16 KB (16 KB free)
Blackfin L1 Instruction SRAM: 64 KB (57 KB free)
PDA for CPU0 reserved at 00152598
net_namespace: 288 bytes
NET: Registered protocol family 16
Blackfin GPIO Controller
Blackfin DMA Controller
ezkit_init(): registering device resources
NET: Registered protocol family 2
IP route cache hash table entries: 1024 (order: 0, 4096 bytes)
TCP established hash table entries: 1024 (order: 1, 8192 bytes)
TCP bind hash table entries: 1024 (order: 0, 4096 bytes)
TCP: Hash tables configured (established 1024 bind 1024)
TCP reno registered
NET: Registered protocol family 1
msgmni has been set to 53
io scheduler noop registered
io scheduler anticipatory registered (default)
io scheduler cfq registered
Serial: Blackfin serial driver
brd: module loaded
smc91x.c: v1.1, sep 22 2004 by Nicolas Pitre <nico@cam.org>
eth0: SMC91C11xFD (rev 1) at 20310300 IRQ 42 [nowait]
eth0: Ethernet addr: 00:e0:22:fe:b1:2e
bfin-spi bfin-spi.0: Blackfin on-chip SPI Controller Driver, Version 1.0, regs_base@ffc00500, dma c5
rtc-bfin rtc-bfin: rtc core: registered rtc-bfin as rtc0
bfin-wdt: initialized: timeout=20 sec (nowayout=0)
TCP cubic registered
NET: Registered protocol family 17
rtc-bfin rtc-bfin: setting system clock to 1970-02-09 00:53:53 UTC (3372833)
Freeing unused kernel memory: 2492k freed
Warning: unable to open an initial console.
Follow-ups
--- Sonic Zhang 2008-12-29 02:42:51
Someone removed bfin_uart_device from platform_device data.
Fixed.
--- Mike Frysinger 2008-12-29 07:04:51
it's easy enough to lookup the history
blackfin.uclinux.org/gf/project/linux-kernel/scmsvn/?action=browse&path=%2Ftrunk%2Farch%2Fblackfin%2Fmach-bf533%2Fboards%2Fezkit.c&r1=5626&r2=5839&pathrev=5917
--- Vivi Li 2008-12-30 01:42:14
OK now. Close it.
Thanks!
Files
Changes
Commits
Dependencies
Duplicates
Associations
Tags
File Name File Type File Size Posted By
config.bf533-ezkit application/octet-stream 27160 Vivi Li