[#4842] multiple insmod of bf5xx_nand.ko panics
Submitted By: John DeHority
Open Date
2009-01-27 15:24:13
Priority:
Medium Assignee:
Nobody
Status:
Open Fixed In Release:
N/A
Found In Release:
N/A Release:
Category:
Drivers Board:
STAMP
Processor:
BF527 Silicon Revision:
Is this bug repeatable?:
Yes Resolution:
Uboot version or rev.:
Toolchain version or rev.:
GCC 4.1.2 2008R1
App binary format:
Summary: multiple insmod of bf5xx_nand.ko panics
Details:
It is only possible to insmod the nand flash driver two times:
#insmod bf5xx_nand.ko
other steps that utilize driver (mount, write file, umount)
#rmmod bf5xx_nand.ko
KERNEL PANIC
It used to panic on the second insmod. This was "fixed" in #4463...now it works twice, but no more than twice! This bug appears to have been tested against bfin_nand module. We are using the bf5xx_nand module.
Kernel was built with 2.6.22.19-ADI-2008R1.5, we sync with this branch each night. We are in sync as of 27 Jan 09.
Follow-ups
--- Robin Getz 2009-01-27 18:25:45
John:
Thanks for the report - it will be a week or so before anyone can look at this
-- as most of our developers are off for Chinese New Year.
-Robin
--- Cliff Cai 2009-02-04 22:48:53
it seems the workaround from mainline doesn't work in this case,Bryan know
the details.
Cliff
Files
Changes
Commits
Dependencies
Duplicates
Associations
Tags
File Name File Type File Size Posted By
No Files Were Found