[#4847] build e2fsprogs failed after update to version 1.41.4
Submitted By: Vivi Li
Open Date
2009-02-02 05:21:02 Close Date
2009-04-28 00:16:49
Priority:
Medium Assignee:
Mike Frysinger
Status:
Closed Fixed In Release:
N/A
Found In Release:
N/A Release:
Category:
Make Errors Board:
Processor:
ALL Silicon Revision:
Is this bug repeatable?:
Yes Resolution:
Fixed
Uboot version or rev.:
Toolchain version or rev.:
gcc4.1_2009-01-19
App binary format:
Summary: build e2fsprogs failed after update to version 1.41.4
Details:
Build e2fsprogs failed after update e2fsprogs to version 1.41.4.
Enable some apps such as mke2fs and e2fsck, e2fsprogs will be built.
Bellow is the log:
--
make[5]: Entering directory `/home/test/work/cruise/checkouts/uclinux-dist/user/e2fsprogs/build-e2fsprogs-1.41.4'^M
cd .; CONFIG_FILES=./lib/uuid/uuid_types.h ./config.status^M
../../../e2fsprogs-1.41.4/lib/ss/get_readline.c:24: warning: ‘ss_release_readline’ defined but not used^M
GEN_LIB libss.a^M
make[5]: Leaving directory `/home/test/work/cruise/checkouts/uclinux-dist/user/e2fsprogs/build-e2fsprogs-1.41.4/lib/ss'^M
making all in lib/e2p^M
make[5]: Entering directory `/home/test/work/cruise/checkouts/uclinux-dist/user/e2fsprogs/build-e2fsprogs-1.41.4/lib/e2p'^M
make[5]: *** No rule to make target `../../lib/ext2fs/ext2_err.h', needed by `feature.o'. Stop.^M
make[5]: *** Waiting for unfinished jobs....^M
make[5]: Leaving directory `/home/test/work/cruise/checkouts/uclinux-dist/user/e2fsprogs/build-e2fsprogs-1.41.4/lib/e2p'^M
make[4]: *** [all-libs-recursive] Error 1^M
make[4]: *** Waiting for unfinished jobs....^M
config.status: creating ./lib/uuid/uuid_types.h^M
config.status: executing default-1 commands^M
make[5]: Leaving directory `/home/test/work/cruise/checkouts/uclinux-dist/user/e2fsprogs/build-e2fsprogs-1.41.4'^M
make[5]: Entering directory `/home/test/work/cruise/checkouts/uclinux-dist/user/e2fsprogs/build-e2fsprogs-1.41.4/lib/et'^M
make[5]: `compile_et' is up to date.^M
make[5]: Leaving directory `/home/test/work/cruise/checkouts/uclinux-dist/user/e2fsprogs/build-e2fsprogs-1.41.4/lib/et'^M
make[5]: Entering directory `/home/test/work/cruise/checkouts/uclinux-dist/user/e2fsprogs/build-e2fsprogs-1.41.4/lib/ext2fs'^M
SUBST ext2_err.et^M
COMPILE_ET ext2_err.et^M
make[5]: Leaving directory `/home/test/work/cruise/checkouts/uclinux-dist/user/e2fsprogs/build-e2fsprogs-1.41.4/lib/ext2fs'^M
make[4]: Leaving directory `/home/test/work/cruise/checkouts/uclinux-dist/user/e2fsprogs/build-e2fsprogs-1.41.4'^M
make[3]: *** [all] Error 2^M
make[3]: Leaving directory `/home/test/work/cruise/checkouts/uclinux-dist/user/e2fsprogs'^M
make[2]: *** [e2fsprogs] Error 2^M
make[2]: Leaving directory `/home/test/work/cruise/checkouts/uclinux-dist/user'^M
make[1]: *** [all] Error 2^M
make[1]: Leaving directory `/home/test/work/cruise/checkouts/uclinux-dist/user'^M
make: *** [subdirs] Error 1^M
Follow-ups
--- Vivi Li 2009-03-12 05:51:21
This bug doesn't happen every time. It seems that it has something to do with
the order of compiling.
Kernel can always be built with NON_SMP_BUILD=1.
--- Mike Frysinger 2009-04-23 23:15:03
should be all set now by updating e2fsprogs dependencies
--- Vivi Li 2009-04-28 00:16:49
OK, close it.
Files
Changes
Commits
Dependencies
Duplicates
Associations
Tags
File Name File Type File Size Posted By
No Files Were Found