[#4924] usb gadget zero bulk test NO. 1/3/5/7 fails on 527
Submitted By: Vivi Li
Open Date
2009-02-20 05:43:53 Close Date
2009-06-18 03:29:27
Priority:
Medium High Assignee:
Cliff Cai
Status:
Closed Fixed In Release:
N/A
Found In Release:
N/A Release:
Category:
N/A Board:
EZKIT Lite
Processor:
BF527 Silicon Revision:
Is this bug repeatable?:
Yes Resolution:
Fixed
Uboot version or rev.:
Toolchain version or rev.:
gcc4.1_2009-01-19
App binary format:
Summary: usb gadget zero bulk test NO. 1/3/5/7 fails on 527
Details:
For usb gadget zero bulk test NO. 1/3/5/7, they easily fail for BF527-EZKIT on latest trunk.
* bf527-ezkit image on trunk (musb_hdrc: version 6.0, pio)
* silicon rev 0.2, board rev 1.4
* latest gadget zero bulk test script
--
sudo ./src/testusb -D /proc/bus/usb/005/112 -t1
unknown speed /proc/bus/usb/005/112
/proc/bus/usb/005/112 test 1 --> 32 (Broken pipe)
sudo ./src/testusb -D /proc/bus/usb/005/112 -t3
/proc/bus/usb/005/112 test 3 --> 32 (Broken pipe)
sudo ./src/testusb -D /proc/bus/usb/005/112 -t5
/proc/bus/usb/005/112 test 5 --> 32 (Broken pipe)
sudo ./src/testusb -D /proc/bus/usb/005/112 -t7
/proc/bus/usb/005/112 test 7 --> 32 (Broken pipe)
Follow-ups
--- Vivi Li 2009-03-18 05:47:11
I re-test bf527-ezkit with the following configuration:
* bf527-ezkit image of 08r1.5 (musb_hdrc: version 6.0, pio mode)
At first t5 test pass, after several test cycles, it breaks. Continue to run
t7, it fails to return and kernel reboots automatically. t1 and t3 always pass
before kernel reboots.
Bellow is the error log:
sudo ./src/testusb -D /proc/bus/usb/002/011 -t5
unknown speed /proc/bus/usb/002/011
/proc/bus/usb/002/011 test 5 --> 32 (Broken pipe)
uclinux63-527-usbdev:/home/test/work/cruise/checkouts/uclinux-dist/testsuites/usbdev
#
sudo ./src/testusb -D /proc/bus/usb/002/011 -t7
(kernel reboot automatically)
--- Cliff Cai 2009-05-13 02:06:04
All the Broken pipe failures on peripheral bulk out tests (-t1,3,5,7...)are
caused by receiving wrong data.the test driver(f_sourcesink.c in /usb/garget/)
will check the reveived data manually,to see if the data is correct or not,if
not,it halts the device,and returns ERROR.
In current test,the host issues all "0" data packets to device in
pattern 0,and the test driver will check if the buffer which store the data read
from Rx FIFO is all filled with zero,a failure is detected when non-zero data is
checked.see check_read_data() in f_sourcesink.c.
In peripheral BULK mode,this problem occurs in both DMA and PIO mode, I guess
that the corrupt data is wrongly sent to Rx FIFO,since I didn't see any CRC or
bit-stuff error check for the mode in the HRM.
Any thoughts?
Cliff
--- Sonic Zhang 2009-05-13 02:19:42
In peripheral bulk transfer mode, when data received in RX fifo is corrupt, no
hardware CRC check or error status bit is set by the MUSB controller according
to the HRM. Either this is allowed by USB spec and the test cases are incorrect
or there is a hardware issue in MUSB controller to receive corrupt data without
error check.
--- Cliff Cai 2009-05-13 05:05:46
According to the usb2.0 spec,if the data packet has CRC or bit stuff error,it
should be discarded.see 8.7.1 of usb2.0 spec.
--- Cliff Cai 2009-06-11 23:55:30
fixed by disabling double buffer mode.
--- Vivi Li 2009-06-18 03:29:27
OK now. Close it.
Files
Changes
Commits
Dependencies
Duplicates
Associations
Tags
File Name File Type File Size Posted By
No Files Were Found