[#5114] build kernel fails at setup.c for bf537-stamp
Submitted By: Vivi Li
Open Date
2009-05-08 00:45:05 Close Date
2009-05-08 03:43:14
Priority:
Medium Assignee:
Sonic Zhang
Status:
Closed Fixed In Release:
N/A
Found In Release:
N/A Release:
Category:
N/A Board:
N/A
Processor:
ALL Silicon Revision:
Is this bug repeatable?:
Yes Resolution:
Fixed
Uboot version or rev.:
Toolchain version or rev.:
toolchain4.1-09r1_rc6
App binary format:
N/A
Summary: build kernel fails at setup.c for bf537-stamp
Details:
build kernel for bf537-stamp, it fails at arch/blackfin/kernel/setup.c
--
CC arch/blackfin/kernel/setup.o^M
arch/blackfin/kernel/setup.c: In function ‘setup_arch’:^M
arch/blackfin/kernel/setup.c:804: error: ‘ANOMALY_05000274’ undeclared (first use in this function)^M
arch/blackfin/kernel/setup.c:804: error: (Each undeclared identifier is reported only once^M
arch/blackfin/kernel/setup.c:804: error: for each function it appears in.)^M
make[2]: *** [arch/blackfin/kernel/setup.o] Error 1^M
--
Follow-ups
--- Sonic Zhang 2009-05-08 00:55:03
Add ANOMALY_05000274 in head file.
--- Vivi Li 2009-05-08 03:43:14
OK now. Close it.
Files
Changes
Commits
Dependencies
Duplicates
Associations
Tags
File Name File Type File Size Posted By
No Files Were Found