[#5135] error info shows when reboot kernel after run oprofile test
Submitted By: Vivi Li
Open Date
2009-05-15 07:28:39 Close Date
2009-07-02 03:34:06
Priority:
Medium Assignee:
Graf Yang
Status:
Closed Fixed In Release:
N/A
Found In Release:
N/A Release:
Category:
Tests Board:
Processor:
ALL Silicon Revision:
Is this bug repeatable?:
Yes Resolution:
Fixed
Uboot version or rev.:
Toolchain version or rev.:
gcc4.1-09r1_rc6
App binary format:
Summary: error info shows when reboot kernel after run oprofile test
Details:
Reboot kernel after run oprofile test, there will be error info.
Run following for oprofile test:
--
root:/> /usr/bin/bfin_opcontrol --init
root:/> /usr/bin/bfin_opcontrol --start-daemon &^M
KSDBG:get cputype=4,counts=1^M
Using 2.6+ OProfile kernel interface.^M
Reading module info.^M
Using log file /var/lib/oprofile/oprofiled.log^M
147^M
root:/> /usr/bin/bfin_opcontrol --start^M
root:/> /usr/bin/bfin_opcontrol --dump^M
root:/> /usr/bin/opreport -l^M
CPU: CPU with timer interrupt, speed 600 MHz (estimated)^M
Profiling through timer interrupt^M
warning: could not check that the binary file /vmlinux has not been modified since the profile was taken. Results may be inaccurate.^M
samples % app name symbol name^M
1 50.0000 ld-uClibc.so.0 (no symbols)^M
1 50.0000 vmlinux _getname^M
root:/>
Then reboot kernel, there will be error info.
root:/> reboot
Illegal use of supervisor resource
- Attempted to use a Supervisor register or instruction from User mode.
Supervisor resources are registers and instructions that are reserved
for Supervisor use: Supervisor only registers, all MMRs, and Supervisor
only instructions.
Deferred Exception context
CURRENT PROCESS:
COMM=oprofiled PID=148
CPU = 0
TEXT = 0x03120000-0x03129358 DATA = 0x03130358-0x03139210
BSS = 0x03139210-0x03140000 USER-STACK = 0x0315fe70
return address: [0x0312242e]; contents of:
0x03122400: e51b ff9b 0051 e519 ff98 e51b ff99 0051
0x03122410: e519 ff96 e51b ff97 0051 e519 ff94 e51b
0x03122420: ff95 0051 e519 ff92 e51b ff93 0051 [e519]
0x03122430: ff90 e51b ff91 0051 e519 ff8e e51b ff8f
SEQUENCER STATUS: Not tainted
SEQSTAT: 0006202e IPEND: 0030 SYSCFG: 0006
EXCAUSE : 0x2e
interrupts disabled
physical IVG5 asserted : <0xffa00b8c> { _evt_ivhw + 0x0 }
RETE: <0x00000000> /* Maybe null pointer? */
RETN: <0x03110000> [ /usr/lib/libpopt.so.0 + 0x0 ]
RETX: <0x00000480> /* Maybe fixed code section */
RETS: <0x03122d7c> [ /usr/bin/oprofiled + 0x2d7c ]
PC : <0x0312242e> [ /usr/bin/oprofiled + 0x242e ]
DCPLB_FAULT_ADDR: <0xfffffe40> /* kernel dynamic memory */
ICPLB_FAULT_ADDR: <0x0312242e> [ /usr/bin/oprofiled + 0x242e ]
PROCESSOR STATE:
R0 : 00000000 R1 : 00000001 R2 : 00880008 R3 : 00000002
R4 : 0315fe74 R5 : 030d0004 R6 : 00000000 R7 : 0315fd04
P0 : 000000be P1 : 00a8c120 P2 : 030d13f8 P3 : 00000000
P4 : 03130b20 P5 : 03130fd0 FP : 0315fce4 SP : 0310ff24
LB0: 00ae6351 LT0: 00ae6344 LC0: 00000000
LB1: 00a9d68b LT1: 00a9d68a LC1: 00000000
B0 : 00000000 L0 : 00000000 M0 : 00000000 I0 : 0315eb91
B1 : 00000000 L1 : 00000000 M1 : 00000000 I1 : 00000000
B2 : 00000000 L2 : 00000000 M2 : 00000000 I2 : 00000000
B3 : 00000000 L3 : 00000000 M3 : 00000000 I3 : 00000000
A0.w: 00000000 A0.x: 00000000 A1.w: 00000000 A1.x: 00000000
USP : 0315fcd4 ASTAT: 02003004
Hardware Trace:
0 Target : <0x000049e8> { _trap_c + 0x0 }
Source : <0xffa0062a> { _exception_to_level5 + 0x9e } CALL pcrel
1 Target : <0xffa0058c> { _exception_to_level5 + 0x0 }
Source : <0xffa0045e> { _bfin_return_from_exception + 0x6 } RTX
2 Target : <0xffa00458> { _bfin_return_from_exception + 0x0 }
Source : <0xffa004e6> { _ex_trap_c + 0x66 } JUMP.S
3 Target : <0xffa00480> { _ex_trap_c + 0x0 }
Source : <0xffa006c4> { _trap + 0x38 } JUMP (P4)
4 Target : <0xffa006aa> { _trap + 0x1e }
Source : <0xffa006a6> { _trap + 0x1a } IF !CC JUMP
5 Target : <0xffa0068c> { _trap + 0x0 }
Source : <0x03122d78> [ /usr/bin/oprofiled + 0x2d78 ] CALL pcrel
6 Target : <0x03122d74> [ /usr/bin/oprofiled + 0x2d74 ]
Source : <0x03122d6c> [ /usr/bin/oprofiled + 0x2d6c ] IF CC JUMP
7 Target : <0x03122d66> [ /usr/bin/oprofiled + 0x2d66 ]
Source : <0x00a8c126> [ /lib/libc.so.0 + 0xc126 ] RTS
8 Target : <0x00a8c126> [ /lib/libc.so.0 + 0xc126 ]
Source : <0xffa00b88> { __common_int_entry + 0xd8 } RTI
9 Target : <0xffa00b26> { __common_int_entry + 0x76 }
Source : <0xffa00d50> { _evt_system_call + 0x64 } JUMP.S
10 Target : <0xffa00d50> { _evt_system_call + 0x64 }
Source : <0xffa0084c> { _system_call + 0xb8 } RTS
11 Target : <0xffa00848> { _system_call + 0xb4 }
Source : <0xffa00838> { _system_call + 0xa4 } IF !CC JUMP
12 Target : <0xffa00832> { _system_call + 0x9e }
Source : <0xffa00822> { _system_call + 0x8e } IF !CC JUMP
13 Target : <0xffa007fc> { _system_call + 0x68 }
Source : <0xffa00118> { _sys_rt_sigreturn + 0x10 } RTS
14 Target : <0xffa00114> { _sys_rt_sigreturn + 0xc }
Source : <0x00002354> { _do_rt_sigreturn + 0x48 } RTS
15 Target : <0x00002348> { _do_rt_sigreturn + 0x3c }
Source : <0x00002a10> { _do_rt_sigreturn + 0x704 } JUMP.S
Userspace Stack
Stack info:
SP: [0x0315fcd4] <0x0315fcd4> [ oprofiled + 0x1fcd4 ]
FP: (0x0315fd94)
Memory from 0x0315fcd0 to 03160000
0315fcd0: 00000000 [03130fd0] 03130b20 0315fd04 00000000 030d0004 0315fe74 0315fd2c
0315fcf0: 00000004 00000001 03130690 00000000 03130880 00004000 00000000 00000000
0315fd10: 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
0315fd30: 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
0315fd50: 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
0315fd70: 00000000 00000000 00000000 00000000 00000000 00000000 031618f0 00000800
0315fd90: 00000800 (0315fe34)<00ab36cc> 0315ff18 031618f0 0315ff6b 0315ff20 03163adc
0315fdb0: 00ae68a4 030d1144 0dfd935e 00000000 00000000 00000000 00000000 00000000
0315fdd0: 00000000 00000003 03120034 00000004 00000020 00000005 00000006 00000006
0315fdf0: 00001000 00000007 00ae0000 00000008 00000000 00000009 031224f8 00000000
0315fe10: 00000000 0000000b 00000000 0000000c 00000000 0000000d 00000000 0000000e
0315fe30: 00000000 (00000000)<03122526> 030d1178 031224f8 030d1170 0315ff20 0315ff40
0315fe50:<031224fc> 0310286c 00000005 0315ff40 0310285c 03102864 030d1170 0315ff4c
0315fe70: 00000005 0315ff6b <0315ff7e> 0315ff81 0315ff82 0315ff8f 00000000 <0315ffa6>
0315fe90: 0315ffad 0315ffbb 0315ffde 00000000 00000010 00000000 00000006 00001000
0315feb0: 00000011 00000064 00000003 03120034 00000004 00000020 00000005 00000006
0315fed0: 00000007 00ae0000 00000008 00000000 00000009 031224f8 0000000b 00000000
0315fef0: 0000000c 00000000 0000000d 00000000 0000000e 00000000 00000017 00000000
0315ff10: 0000001f 0001ffe9 00000000 00000000 <00020000> 00ae0000 00000000 0000701c
0315ff30: 030d101c 0000b01c 00000450 00000000 <00020000> 03120000 00000000 00009358
0315ff50: 03130358 0000d358 00008eb8 00000000 00000000 00000000 2f000000 2f727375
0315ff70: 2f6e6962 6f72706f 656c6966 652d0064 2d2d0000 762d6f6e 6e696c6d 2d007875
0315ff90: 616d692d 2f3d6567 2f6e6962 74656877 6e6f7473 4f480065 2f3d454d 45485300
0315ffb0: 2f3d4c4c 2f6e6962 50006873 3d485441 6e69622f 73752f3a 69622f72 732f3a6e
0315ffd0: 3a6e6962 7273752f 6962732f 4554006e 6c3d4d52 78756e69 73752f00 69622f72
0315fff0: 706f2f6e 69666f72 0064656c 00000000 00000000
Return addresses in stack:
frame 1 : <0x00ab36cc> [ /lib/libc.so.0 + 0x336cc ]
frame 2 : <0x03122526> [ /usr/bin/oprofiled + 0x2526 ]
address : <0x031224fc> [ /usr/bin/oprofiled + 0x24fc ]
address : <0x0315ff7e> [ oprofiled + 0x1ff7e ]
address : <0x0315ffa6> [ oprofiled + 0x1ffa6 ]
address : <0x00020000> { _check_clock + 0x28 }
COMM=oprofiled PID=147
RETN: <0x030d8000> [ watchdogd + 0x0 ]
P4 : 03130b20 P5 : 03130fd0 FP : 0315fce4 SP : 030d7f24
Restarting system..
U-Boot 2008.10-svn1847 (ADI-2009R1-rc1) (Apr 17 2009 - 18:25:58)
CPU: ADSP bf561-0.3 (Detected Rev: 0.5) (bypass boot)
Board: ADI BF561 EZ-Kit Lite board
Support: http://blackfin.uclinux.org/
Clock: VCO: 600 MHz, Core: 600 MHz, System: 100 MHz
RAM: 64 MB
Flash: 8 MB
In: serial
Out: serial
Err: serial
Net: MAC: 00:E0:22:FE:B1:3C
Hit any key to stop autoboot: 0
bfin>
Jump to NULL address
TEXT = 0x03130000-0x03139358 DATA = 0x03160358-0x03169210
BSS = 0x03169210-0x03180000 USER-STACK = 0x0319fe50
return address: [0x00000000]; contents of:
SEQSTAT: 0006202d IPEND: 0030 SYSCFG: 0006
EXCAUSE : 0x2d
RETN: <0x031a4000> /* kernel dynamic memory */
RETS: <0x03132d7c> [ /usr/bin/oprofiled + 0x2d7c ]
PC : <0x00000000> /* Maybe null pointer? */
DCPLB_FAULT_ADDR: <0x0319fd44> [ oprofiled + 0x1fd44 ]
ICPLB_FAULT_ADDR: <0x00000000> /* Maybe null pointer? */
R4 : 0319fe54 R5 : 030d1004 R6 : 0319ff00 R7 : 0319fce4
P0 : 000000be P1 : 00000000 P2 : 00aef3f8 P3 : 00000000
P4 : 03160b20 P5 : 03160fd0 FP : 0319fcc4 SP : 031a3f24
LB1: 00a9fa39 LT1: 00a9f9f2 LC1: 00000000
B0 : 00000000 L0 : 00000000 M0 : 00000000 I0 : 0319ea05
USP : 0319fcb4 ASTAT: 02003004
Source : <0x03132436> [ /usr/bin/oprofiled + 0x2436 ] JUMP (P1)
6 Target : <0x0313242e> [ /usr/bin/oprofiled + 0x242e ]
Source : <0x03132d78> [ /usr/bin/oprofiled + 0x2d78 ] CALL pcrel
7 Target : <0x03132d74> [ /usr/bin/oprofiled + 0x2d74 ]
Source : <0x03132d6c> [ /usr/bin/oprofiled + 0x2d6c ] IF CC JUMP
8 Target : <0x03132d66> [ /usr/bin/oprofiled + 0x2d66 ]
9 Target : <0x00a8c126> [ /lib/libc.so.0 + 0xc126 ]
10 Target : <0xffa00b26> { __common_int_entry + 0x76 }
11 Target : <0xffa00d50> { _evt_system_call + 0x64 }
12 Target : <0xffa00848> { _system_call + 0xb4 }
13 Target : <0xffa00832> { _system_call + 0x9e }
14 Target : <0xffa007fc> { _system_call + 0x68 }
15 Target : <0xffa00114> { _sys_rt_sigreturn + 0xc }
SP: [0x0319fcb4] <0x0319fcb4> [ oprofiled + 0x1fcb4 ]
FP: (0x0319fd74)
Memory from 0x0319fcb0 to 031a0000
0319fcb0: 00000000 [03160fd0] 03160b20 0319fce4 0319ff00 030d1004 0319fe54 0319fd0c
0319fcd0: 00000000 00000001 03160690 00000000 03160880 00004000 00000000 00000000
0319fcf0: 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
0319fd10: 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
0319fd30: 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
0319fd50: 00000000 00000000 00000000 00000000 00000000 00000000 031798f0 00000800
0319fd70: 00000800 (0319fe14)<00ab36cc> 0319fef4 031798f0 0319ff43 0319ff00 0317badc
0319fd90: 00ae68a4 00aef144 0dfd935e 00000000 00000000 00000000 00000000 00000000
0319fdb0: 00000000 00000003 03130034 00000004 00000020 00000005 00000006 00000006
0319fdd0: 00001000 00000007 00ae0000 00000008 00000000 00000009 031324f8 00000000
0319fdf0: 00000000 0000000b 00000000 0000000c 00000000 0000000d 00000000 0000000e
0319fe10: 00000000 (00000000)<03132526> 00aef178 031324f8 00aef170 0319ff00 0319ff20
0319fe30:<031324fc> 03ecf864 00000004 0319ff20 03ecf854 03ecf85c 00aef170 0319ff2c
0319fe50: 00000004 0319ff43 0319ff4f 0319ff78 0319ff8c 00000000 0319ffad 0319ffb8
0319fe70: 0319ffdb 0319ffe9 00000000 00000010 00000000 00000006 00001000 00000011
0319fe90: 00000064 00000003 03130034 00000004 00000020 00000005 00000006 00000007
0319feb0: 00ae0000 00000008 00000000 00000009 031324f8 0000000b 00000000 0000000c
0319fed0: 00000000 0000000d 00000000 0000000e 00000000 00000017 00000000 0000001f
0319fef0: 0001fff0 00000000 00000000 00000000 <00020000> 00ae0000 00000000 0000701c
0319ff10: 00aef01c 0000b01c 00000450 00000000 <00020000> 03130000 00000000 00009358
0319ff30: 03160358 0000d358 00008eb8 00000000 2e000000 72706f2f 6c69666f 2d006465
0319ff50: 6576652d 3d73746e 41544f54 52425f4c 48434e41 3978303a 313a303a 30303030
0319ff70: 3a313a30 00313a31 6d762d2d 756e696c 2f2e3d78 696c6d76 0078756e 656b2d2d
0319ff90: 6c656e72 6e61722d 303d6567 31303030 2c303030 66303030 30646531 52455400
0319ffb0: 696c3d4d 0078756e 48544150 69622f3d 752f3a6e 622f7273 2f3a6e69 6e696273
0319ffd0: 73752f3a 62732f72 53006e69 4c4c4548 69622f3d 68732f6e 4d4f4800 002f3d45
0319fff0: 706f2f2e 69666f72 0064656c 00000000 00001004
frame 2 : <0x03132526> [ /usr/bin/oprofiled + 0x2526 ]
address : <0x031324fc> [ /usr/bin/oprofiled + 0x24fc ]
P4 : 03160b20 P5 : 03160fd0 FP : 0319fcc4 SP : 030d7f24
14 Target : <0xffa00810> { _system_call + 0x7c }
Source : <0xffa00830> { _system_call + 0x9c } JUMP.S
15 Target : <0xffa0082e> { _system_call + 0x9a }
Source : <0xffa01836> { _schedule + 0x1aa } RTS
Follow-ups
--- Graf Yang 2009-06-25 07:30:51
It will encounter null pointer or instruction misalign when oprofile is going
into _exit(EXIT_SUCCESS).
Old toolchain(svn3087) have not this problem.
--- Graf Yang 2009-06-26 08:58:43
Since toolchain commit svn3171, an uClibc bug is exposed for fdpic format.
Some stack may be destroyed by functions in ld-uClibc.so.0.
I need digging in...
Attach the application file for Jie to look on it.
--- Jie Zhang 2009-06-27 00:21:35
I think I know what happens. It's not a regression of toolchain. It's an
application bug.
static void opd_fork(void)
{
switch(vfork()){
//switch (fork()) {
case -1:
perror("oprofiled: fork() failed: ");
exit(EXIT_FAILURE);
break;
case 0:
default:
/* parent */
_exit(EXIT_SUCCESS);
}
vfork does not make a copy of address space for child process. Both child and
parent share the same one. In opd_fork (), the child will ruin the stack when it
returns from main and calls exit. The GOT pointer saved on stack when entering
main is destroyed. When parent resumes, an incorrect value is restored for GOT
pointer, which further causes the dump shows in the bug report.
The child should call an exec function or _exit after vfork. The oprofile have
to be fixed in this way.
--- Graf Yang 2009-06-29 05:50:58
In opd_fork(), the child go down, the parent just do _exit(), so I think we need
not call this function.
I have commit it to trunk and branch.
--- Mike Frysinger 2009-06-29 11:48:52
then why not change opd_fork() to call daemon(1,1)
--- Graf Yang 2009-06-29 22:05:20
Need to make things be more clear.
--- Graf Yang 2009-06-30 04:19:29
Mike,
daemon() also works.
The following patch would be committed if no one object.
static void opd_go_daemon(void)
+#ifdef __uClinux__
+ daemon (0, 1);
+#else
opd_fork();
if (chdir(OP_BASE_DIR)) {
@@ -141,9 +142,9 @@
+#endif
--- Mike Frysinger 2009-06-30 12:50:56
you should use daemon(1,1) and then do the chdir() manually to match behavior
daemon() will chdir("/"), not chdir(OP_BASE_DIR)
--- Graf Yang 2009-06-30 22:34:14
Thanks, I will commit patch like the following.
- /*opd_fork();*/
+ daemon (1, 1);
fprintf(stderr, "oprofiled: opd_go_daemon: couldn't chdir to "
OP_BASE_DIR ": %s", strerror(errno));
+ opd_fork();
+ if (chdir(OP_BASE_DIR)) {
+ fprintf(stderr, "oprofiled: opd_go_daemon: couldn't chdir to "
+ OP_BASE_DIR ": %s", strerror(errno));
+ exit(EXIT_FAILURE);
+ }
+
if (setsid() < 0) {
perror("oprofiled: opd_go_daemon: couldn't setsid: ");
--- Graf Yang 2009-07-01 03:26:23
Commited to trunk and branch.
--- Vivi Li 2009-07-02 03:34:06
OK now. Close it.
Files
Changes
Commits
Dependencies
Duplicates
Associations
Tags
File Name File Type File Size Posted By
oprofiled3170 application/octet-stream 46016 Graf Yang
opdump3171 application/octet-stream 782384 Graf Yang