[#5408] sometimes underrun happens for audio on bf527-ezkit
Submitted By: Vivi Li
Open Date
2009-07-29 05:23:33
Priority:
Medium Assignee:
Cliff Cai
Status:
Open Fixed In Release:
N/A
Found In Release:
2009R1-RC6 Release:
Category:
Audio Board:
Processor:
BF527 Silicon Revision:
Is this bug repeatable?:
Yes Resolution:
Not reproducible
Uboot version or rev.:
Toolchain version or rev.:
gcc4.1_2009r1-rc9
App binary format:
Summary: sometimes underrun happens for audio on bf527-ezkit
Details:
When vrec|vplay for ssm2602 on bf527-ezkit, sometimes underrun happens.
I see this twice in recent test but haven\\\\\\\'t got a method to reproduce it.
--
Linux version 2.6.28.10-ADI-2009R1-svn7084 (test@uboot30-527ezkit) (gcc version 4.1.2 (ADI svn)) #85 Wed Jul 29 10:09:56 GMT 2009
bootconsole [early_shadow0] enabled
bootconsole [early_BFuart0] enabled
early printk enabled on early_BFuart0
Board Memory: 64MB
Kernel Managed Memory: 64MB
Memory map:
fixedcode = 0x00000400-0x00000490
text = 0x00001000-0x0012d3d0
rodata = 0x0012d3d0-0x0018a36c
bss = 0x0018b000-0x0019c2a4
data = 0x0019c2a4-0x001ae000
stack = 0x001ac000-0x001ae000
init = 0x001ae000-0x007bc000
available = 0x007bc000-0x03dff000
DMA Zone = 0x03e00000-0x04000000
Hardware Trace Active and Enabled
Boot Mode: 9
Blackfin support (C) 2004-2009 Analog Devices, Inc.
Compiled for ADSP-BF527 Rev 0.0
Blackfin Linux support by http://blackfin.uclinux.org/
Processor Speed: 525 MHz core clock and 131 MHz System Clock
NOMPU: setting up cplb tables
Instruction Cache Enabled for CPU0
Data Cache Enabled for CPU0 (write-back)
Built 1 zonelists in Zone order, mobility grouping off. Total pages: 15747
Kernel command line: root=/dev/mtdblock0 rw earlyprintk=serial,uart0,57600, console=ttyBF0,57600 ip=10.100.4.50:10.100.4.174:10.100.4.174:255.255.255.0:bf527-ezkit:eth0:off
Configuring Blackfin Priority Driven Interrupts
PID hash table entries: 256 (order: 8, 1024 bytes)
console handover:boot [early_BFuart0] boot [early_shadow0] -> real [ttyBF0]
Dentry cache hash table entries: 8192 (order: 3, 32768 bytes)
Inode-cache hash table entries: 4096 (order: 2, 16384 bytes)
Memory available: 54996k/65536k RAM, (6200k init code, 1200k kernel code, 516k data, 2048k dma, 572k reserved)
Calibrating delay loop... 1046.52 BogoMIPS (lpj=2093056)
Security Framework initialized
Mount-cache hash table entries: 512
Blackfin Scratchpad data SRAM: 4 KB
Blackfin L1 Data A SRAM: 16 KB (15 KB free)
Blackfin L1 Data B SRAM: 16 KB (16 KB free)
Blackfin L1 Instruction SRAM: 48 KB (42 KB free)
net_namespace: 288 bytes
NET: Registered protocol family 16
Blackfin DMA Controller
ezkit_init(): registering device resources
SCSI subsystem initialized
NET: Registered protocol family 2
IP route cache hash table entries: 1024 (order: 0, 4096 bytes)
TCP established hash table entries: 2048 (order: 2, 16384 bytes)
TCP bind hash table entries: 2048 (order: 1, 8192 bytes)
TCP: Hash tables configured (established 2048 bind 2048)
TCP reno registered
NET: Registered protocol family 1
msgmni has been set to 107
io scheduler noop registered
io scheduler anticipatory registered (default)
io scheduler cfq registered
bfin-t350mcqb: 320x240 24-bit RGB FrameBuffer initializing...
dma_alloc_init: dma_page @ 0x03a3c000 - 512 pages at 0x03e00000
bfin-otp: initialized
Serial: Blackfin serial driver
bfin-uart.1: ttyBF0 at MMIO 0xffc02000 (irq = 31) is a BFIN-UART
brd: module loaded
bfin_mii_bus: probed
bfin_mac: attached PHY driver [Generic PHY] (mii_bus:phy_addr=0:03, irq=-1, mdc_clk=2500000Hz(mdc_div=25)@sclk=131MHz)
bfin_mac bfin_mac.0: Blackfin on-chip Ethernet MAC driver, Version 1.1
Driver \\\\\\\'sd\\\\\\\' needs updating - please use bus_type methods
rtc-bfin rtc-bfin: rtc core: registered rtc-bfin as rtc0
bfin-wdt: initialized: timeout=20 sec (nowayout=0)
Advanced Linux Sound Architecture Driver Version 1.0.18rc3.
ALSA device list:
No soundcards found.
TCP cubic registered
NET: Registered protocol family 17
rtc-bfin rtc-bfin: setting system clock to 1970-01-01 09:59:36 UTC (35976)
IP-Config: Complete:
device=eth0, addr=10.100.4.50, mask=255.255.255.0, gw=10.100.4.174,
host=bf527-ezkit, domain=, nis-domain=(none),
bootserver=10.100.4.174, rootserver=10.100.4.174, rootpath=
Freeing unused kernel memory: 6200k freed
_____________________________________
a8888b. / Welcome to the uClinux distribution \\\\\\\\
d888888b. / _ _ \\\\\\\\
8P\\\\\\\"YP\\\\\\\"Y88 / | | |_| __ __ (TM) |
8|o||o|88 _____/ | | _ ____ _ _ \\\\\\\\ \\\\\\\\/ / |
8\\\\\\\' .88 \\\\\\\\ | | | | _ \\\\\\\\| | | | \\\\\\\\ / |
8`._.\\\\\\\' Y8. \\\\\\\\ | |__ | | | | | |_| | / \\\\\\\\ |
d/ `8b. \\\\\\\\ \\\\\\\\____||_|_| |_|\\\\\\\\____|/_/\\\\\\\\_\\\\\\\\ |
dP . Y8b. \\\\\\\\ For embedded processors including |
d8:\\\\\\\' \\\\\\\" `::88b \\\\\\\\ the Analog Devices Blackfin /
d8\\\\\\\" \\\\\\\'Y88b \\\\\\\\___________________________________/
:8P \\\\\\\' :888
8a. : _a88P For further information, check out:
._/\\\\\\\"Yaa_: .| 88P| - http://blackfin.uclinux.org/
\\\\\\\\ YP\\\\\\\" `| 8P `. - http://docs.blackfin.uclinux.org/
/ \\\\\\\\.___.d| .\\\\\\\' - http://www.uclinux.org/
`--..__)8888P`._.\\\\\\\' jgs/a:f - http://www.analog.com/blackfin
Have a lot of fun...
BusyBox v1.13.4 (2009-07-28 16:02:41 GMT) built-in shell (msh)
Enter \\\\\\\'help\\\\\\\' for a list of built-in commands.
root:/> versiPHY: 0:03 - Link is Up - 100/Full
on
kernel: Linux release 2.6.28.10-ADI-2009R1-svn7084, build #85 Wed Jul 29 10:09:56 GMT 2009
toolchain: bfin-linux-uclibc-gcc release gcc version 4.1.2 (ADI svn)
user-dist: release svn-8591, build #19 Wed Jul 29 10:09:19 GMT 2009
root:/>
root:/> modprobe i2c-bfin-twi; modprobe snd-ssm2602
i2c-bfin-twi i2c-bfin-twi.0: Blackfin BF5xx on-chip I2C TWI Contoller, regs_base@ffc01400
ASoC version 0.13.2
dma rx:3 tx:4, err irq:15, regs:ffc00800
ssm2602 Audio Codec 0.1<6>asoc: SSM2602 <-> bf5xx-i2s mapping ok
root:/> lsmod
Module Size Used by
snd_ssm2602 1292 0
snd_soc_bf5xx_i2s 2128 1 snd_ssm2602
snd_bf5xx_i2s 2668 1 snd_ssm2602
snd_soc_bf5xx_sport 10480 3 snd_ssm2602,snd_soc_bf5xx_i2s,snd_bf5xx_i2s
snd_soc_ssm2602 8160 1 snd_ssm2602
snd_soc_core 22060 2 snd_bf5xx_i2s,snd_soc_ssm2602
ac97_bus 832 1 snd_soc_core
i2c_bfin_twi 5248 0
root:/> vrec -w -S -b 16 -s 48000 -t 5|vplay
Recording WAVE : 16 bit, Speed 48000 Hz Stereo ...
Playing WAVE : 16 bit, Speed 48000 Hz Stereo ...
sport status error: TUVF
Follow-ups
--- Vivi Li 2009-07-30 05:06:08
When I test ad1981 on bf527-ezkit, I also see underrun.
arecord -t wav -c 1 -f S16_LE -r 48000 -d 5 |aplay
Recording WAVE 'stdin' : Signed 16 bit Little Endian, Rate 48000 Hz, Mono
Playing WAVE 'stdin' : Signed 16 bit Little Endian, Rate 48000 Hz, Mono
--- Cliff Cai 2009-08-11 03:01:22
it\'s hard to reproduce it.
Cliff
Files
Changes
Commits
Dependencies
Duplicates
Associations
Tags
File Name File Type File Size Posted By
config.power_ssm2602 application/octet-stream 34280 Vivi Li
config.audio_ad1981b application/octet-stream 32148 Vivi Li