[#5632] Blackfin MUSB might use ep uninitialized
Submitted By: Mike Frysinger
Open Date
2009-10-20 14:43:04 Close Date
2009-12-04 01:07:30
Priority:
Medium Assignee:
Cliff Cai
Status:
Closed Fixed In Release:
N/A
Found In Release:
2009R1-RC6 Release:
Category:
N/A Board:
Processor:
BF548 Silicon Revision:
Is this bug repeatable?:
Yes Resolution:
Fixed
Uboot version or rev.:
Toolchain version or rev.:
trunk
App binary format:
Summary: Blackfin MUSB might use ep uninitialized
Details:
when using BF548-EZKIT_defconfig, we get:
drivers/usb/gadget/epautoconf.c: In function ‘usb_ep_autoconfig’:
drivers/usb/gadget/epautoconf.c:237: warning: ‘ep’ may be used uninitialized in this function
and indeed the code does:
} else if (gadget_is_musbhsfc(gadget) || gadget_is_musbhdrc(gadget)) {
if ((USB_ENDPOINT_XFER_BULK == type)
|| (USB_ENDPOINT_XFER_ISOC == type)) {
if (USB_DIR_IN & desc->bEndpointAddress)
ep = find_ep (gadget, "ep5in");
else
ep = find_ep (gadget, "ep6out");
}
if (ep && ep_matches (gadget, ep, desc))
return ep;
so for non bulk/isoc types, ep is not initialized
Follow-ups
--- Cliff Cai 2009-10-30 06:01:06
it's not a problem of not initializing non bulk/iso eps,just struct usb_ep *ep
is not initialized.
Anyway,we should add INT ep support.
Files
Changes
Commits
Dependencies
Duplicates
Associations
Tags
File Name File Type File Size Posted By
No Files Were Found