[#5735] A SMP sync problem may lead to timers on core B not working
Submitted By: Yi Li
Open Date
2009-12-02 02:45:33 Close Date
2009-12-13 22:34:23
Priority:
Medium Assignee:
Yi Li
Status:
Closed Fixed In Release:
N/A
Found In Release:
2010R1 Release:
Category:
N/A Board:
Processor:
ALL Silicon Revision:
Is this bug repeatable?:
Yes Resolution:
Fixed
Uboot version or rev.:
Toolchain version or rev.:
2009R1 gcc 4.1
App binary format:
Summary: A SMP sync problem may lead to timers on core B not working
Details:
When I am testing PREEMPT_RT kernel on BF561-ezkit, the kernel blocks while booting. When kernel initialize ethernet driver, it sleeps and never wakes up.
The issue happens when kernel waits for a timer for Core B (the timers are per-cpu based: static DEFINE_PER_CPU(struct tvec_base *, tvec_bases) = &boot_tvec_bases) to timeout.
However, the ksoftirqd thread for core B (note, the ksoftirqd thread is also per-cpu based) cannot work properly, and the timers for Core B never times out.
In kernel/softirq.c:
ksoftirqd()
{
...
while (local_softirq_pending()) {
/* Preempt disable stops cpu going offline.
If already offline, we'll be on wrong CPU:
don't process */
if (cpu_is_offline((long)__bind_cpu))
goto wait_to_die;
wait_to_die:
preempt_enable();
/* Wait for kthread_stop */
set_current_state(TASK_INTERRUPTIBLE);
while (!kthread_should_stop()) {
schedule();
}
__set_current_state(TASK_RUNNING);
return 0;
When ksoftirqd() for the first time run on core B, it is possile core A is still initializing core B (see smp_init() -> cpu_up() -> __cpu_up() ). So the "cpu_is_offline()" check may returns true and ksoftirqd moves to "wait_to_die".
We need to fix bf561 smp code to make sure core B stays idle until core B is considered online.
Follow-ups
--- Mike Frysinger 2009-12-12 23:39:30
so is this issue fixed now ? can we close the bug ?
--- Yi Li 2009-12-13 22:34:23
Yes. We can close this bug. (I was testing this fix with the another SMP patch
to use static array for inter-processor message queue, so delayed for a while).
Files
Changes
Commits
Dependencies
Duplicates
Associations
Tags
File Name File Type File Size Posted By
No Files Were Found