[#5739] Blackfin serial dma is wonky after 2.6.32 upgrade
Submitted By: Mike Frysinger
Open Date
2009-12-03 19:42:21 Close Date
2010-01-19 01:21:16
Priority:
Medium Assignee:
Sonic Zhang
Status:
Closed Fixed In Release:
N/A
Found In Release:
2010R1 Release:
Category:
N/A Board:
Processor:
ALL Silicon Revision:
Is this bug repeatable?:
Yes Resolution:
Fixed
Uboot version or rev.:
Toolchain version or rev.:
trunk 3760
App binary format:
Summary: Blackfin serial dma is wonky after 2.6.32 upgrade
Details:
the serial core under went some changes that seems to have made our dma mode angry. boot up a BF537-STAMP_defconfig and see the misbehavior. RX seems to work fine, but TX lags way behind.
Follow-ups
--- Mike Frysinger 2009-12-15 15:27:24
as a data point, vanilla 2.6.32 and current master (2.6.33-rc0) dont suffer this
problem. but i havent picked through the big pile of serial changes we have
locally to find out which one is causing the problem exactly.
--- Sonic Zhang 2009-12-15 23:07:44
Just figure out the cacheflush against the tx dma buffer should not be punt,
because it is allocated in cacheable memory region by kernel. Only the rx dma
buffer is allocated in uncacheable DMA region in bfin serial driver.
Fixed.
Files
Changes
Commits
Dependencies
Duplicates
Associations
Tags
File Name File Type File Size Posted By
No Files Were Found